Other Parts Discussed in Thread: OMAP3530, TPS65950
We are noticing hangs with USB and other subsystems on Linux 2.6.32, 3.0 and 3.2 with OMAP3530 and when these hangs occur, we see processes stuck waiting for high resolution timers that have huge negative expiry endpoints.
Investigation reveals that sometimes two successive calls to the function omap34xx_32k_read() in .../arch/arm/plat-omap will return the second value less than the previous-- meaning time moved backwards or sometimes the register moves forward is a huge, non-linear jump. The 32K Sync Timer register is supposed to be a monotonically increasing, read-only register clocked at 32KHz.
The TRM for the OMAP3530 states in section 16.6.1.1 that the 32K Sync Timer count register needs to be read with three separate 16-bit transfers, first reading the 16-bit LSB and then two 16-bit reads of the MSB. None of the Linux kernels I listed do it this way. They all do a single 32-bit read of this register.
Can someone confirm if the requirement to read the 32K Sync Timer with three separate 16-bit transfers is a real requirement and if so, comment on why most of the Linux kernels with OMAP support are not doing it correctly. Or, can someone confirm that the requirement is not real and that performing a single 32-bit read should be OK and then suggest why we see the register move backwards and/or make huge jumps??
Chris Elmquist
LogicPD