Tool/software:
Hello,linjun,brijesh
We have a project here where the output images of the probabilistic csirx initialization are all in the not_complte state. It has been confirmed that most of the output images have a few black lines, while the normal situation does not. You can see the comparison of different images in the attachment.
The image resolution is 3840 * 1909, and raw12 is unpacked into raw16 data, with the first row and the last 20 rows being ebd data
We have made several attempts based on this issue:
1.des re-disable and enable output, while csirx still outputs not_complte images
2. When the sensor is re-disabled or enabled for output, csirx still outputs the not_complte image
3. csirx deinit, init, csirx returns to normal output
For the main sdk calls of the corresponding csirx, please refer to the attached code screenshot.
In conclusion, it is highly likely that there is some kind of bug in csirx. Please assist in analyzing it, brijesh. Thank you.
releate log :