Tool/software:
Hi,expert
Our thermal management requirement is to reset after it is higher than 123℃ and lower than 116 degrees, so we made the following changes:
After setting it to 116 ℃, some chips reset immediately when they reach 123 ℃, without obvious pauses waiting for it to drop below 116 ℃
When we reset it back to 105 ℃, this problem no longer occurs. Is this problem caused by the difference between the upper and lower thresholds being too small?
We don't see anything in the register below.