This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCSTUDIO: linux debian ccs 12.8.1 can not load libminidump.so

Part Number: CCSTUDIO

Tool/software:

Hi,

I installed the latest ccs a few weeks ago and have been using it without issues.

Now I upgraded my debian testing distribution to the latest version and after that ccs failed to load

with : There was a problem loading /opt/ti/ccs1281/ccs/eclipse/../ccs_base/common/bin/libMiniDump.so

I have tried to figure out why but have not found a cause other then the obvious

distribution upgrade I did.

If I try to see what libraries are needed by ccs it does not show up :

rth@castle:~$ ldd /opt/ti/ccs1281/ccs/eclipse/ccstudio
    linux-vdso.so.1 (0x00007f551af0f000)
    libpthread.so.0 => /lib/x86_64-linux-gnu/libpthread.so.0 (0x00007f551aee9000)
    libdl.so.2 => /lib/x86_64-linux-gnu/libdl.so.2 (0x00007f551aee4000)
    libc.so.6 => /lib/x86_64-linux-gnu/libc.so.6 (0x00007f551acee000)
    /lib64/ld-linux-x86-64.so.2 (0x00007f551af11000)

rth@castle:~$ objdump -p /opt/ti/ccs1281/ccs/eclipse/ccstudio | grep -i needed
NEEDED libpthread.so.0
NEEDED libdl.so.2
NEEDED libc.so.6

Is this a known new issue ?

Is there a way to fix this ?

I also installed ccs v20 (theia) which does load and if I can figure out how to setup a new

project without using the wizard it might be usable.

ccs v20 will still load when I rename libminidump.so

Roelof