Tool/software:
Hi,TI expert
1.The sending method I use is Tx buffer.
2.Can one dedicated Tx Buffer be configured with multiple message IDs?
3.If multiple message IDs can be assigned, what are the advantages and disadvantages.
4.Based on your experience, should one tx buffer be paired with one message ID or multiple message IDs.
5.int32_t MCAN_txBufTransIntrEnable(uint32_t baseAddr,uint32_t bufNum,uint32_t enable),this API interface is called only once during initialization or once after sending a message
Above, thank you