Tool/software:
Dear TI Support Team,
I am using the following setup to read microphone data:
-
Processor Board: TMS320C5517 EVM
-
Audio Front-End: PCM1864CMBEVM (TIDA-01454B)
-
Demo Used:
BF_rt_bios
fromC:\ti\c55_lp\c55_csl_3.08.01\demos\audio-preprocessing\c5517
-
Mic Input: 6 microphones currently interfaced
-
Reference: TI video and documentation — Voice Processing Tools Software Slides
Currently, I am successfully reading 6 microphone channels via the I2S interface. I would like to extend this to read 8 microphone channels.
My queries are:
-
Is it possible to capture all 8 microphone channels from the PCM1864CMBEVM using the TMS320C5517 EVM?
-
If yes:
-
What hardware or jumper changes are required?
-
What modifications are needed in the existing
BF_rt_bios
demo (e.g., DMA buffer settings, McASP/I2S configuration)? -
Is there a way to use the internal ADC peripheral to read additional channels?
-
-
If not directly possible:
-
Can you recommend any method to achieve 8 mic input using this setup (e.g., cascading devices or alternate signal routing)?
-
Looking forward to your response.
Best regards,
Eswar Badri