This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA4VH-Q1: issue with G-streamer pipeline setup command to access Ethernet and USB Camera data

Part Number: TDA4VH-Q1
Other Parts Discussed in Thread: AM62P, TDA4VH

Tool/software:

Hi I am using 2 TI EVM's one TDA4VH Q1 and AM62P.

I have two different camera sources 1. Logitech USB camera and 2nd our company's Ethernet camera, I am trying to display both of the streams on a display live using TI EVM

I am using SDK 9.2.0.5 in TDA4 and SDK 10.01.10.04 in AM62p

I understand there are differences in the SDK and HW because of which we need to setup g-streamer pipeline differently in AM62P vs TDA4VH, below are my commands which worked in AM62P and failing in TDA4VH can you help me to root causing this problem.

Working command in AM62P:

USB Camera: gst-launch-1.0 -v v4l2src device=/dev/video0 ! video/x-raw, width=640, height=480, format=YUY2 ! videoconvert ! autovideosink sync=false


Ethernet Camera: gst-launch-1.0 -v udpsrc multicast-group=224.0.40.116 multicast-iface="eth0" port=5004 caps="application/x-rtp, media=(string)video, clock-rate=(int)90000, encoding-name=(string)H264, payload=(int)96" auto-multicast=true ! rtph264depay ! decodebin ! videoconvert ! videoscale ! video/x-raw,width=1280,height=720 ! autovideosink sync=false

Command used in TDA4VH not working.

USB Camera: root@j784s4-evm:~# gst-launch-1.0 -v v4l2src device=/dev/video0 ! video/mpeg ! jpegdec ! videoconvert ! autovideosink sync=false
WARNING: erroneous pipeline: could not link v4l2src0 to jpegdec0, jpegdec0 can't handle caps video/mpeg

Ethernet Camera: gst-launch-1.0 -v udpsrc multicast-group=224.0.40.116 multicast-iface="eth0" port=5004 caps="application/x-rtp, media=(string)video, clock-rate=(int)90000, encoding-name=(string)H264, payload=(int)96" auto-multicast=true ! rtph264depay ! decodebin ! videoconvert ! videoscale ! video/x-raw,width=1280,height=720 ! autovideosink sync=false

  • Hello, could you try specifying the correct caps in the pipeline. There is a mismatch with using video/mpeg and jpegdec. If your camera is capturing in JPEG images then you should use image/jpeg. Try using the below pipeline:

    • gst-launch-1.0 -v v4l2src device=/dev/video0 ! image/jpeg, width=640, height=480, framerate=30/1 ! jpegdec ! videoconvert ! autovideosink sync=false

    Thank you,
    Sarabesh S.

  • Hi Sarabesh Srinivasan,

    I Got into this error message with the above command


    root@j784s4-evm:~# gst-launch-1.0 -v v4l2src device=/dev/video0 ! image/jpeg, width=640, height=480, framerate=30/1 ! jpegdec ! videoconvert ! autovideosink sync=false


    Setting pipeline to PAUSED ...
    ERROR: from element /GstPipeline:pipeline0/GstV4l2Src:v4l2src0: Device '/dev/video0' is not a capture device.
    Additional debug info:
    ../gst-plugins-good-1.20.7/sys/v4l2/v4l2_calls.c(629): gst_v4l2_open (): /GstPipeline:pipeline0/GstV4l2Src:v4l2src0:
    Capabilities: 0x4204000
    ERROR: pipeline doesn't want to preroll.
    Failed to set pipeline to PAUSED.
    Setting pipeline to NULL ...
    Freeing pipeline ...
    root@j784s4-evm:~#

  •  Hello,

    Are you sure that /dev/video0 is a camera input? Also, can you confirm whether it captures in JPEG format?

    The J784s4 has the same Wav521CL CODEC driver as the AM62P so your pipelines should translate across devices fine. The only difference is that the J784s4 has two VPU cores for greater throughput.

    Thank you,
    Sarabesh S.

    1. It turns out that USB A on the TDA4Vh evm is not enabled, when I switched to USB-C I could get Video. Thanks you for USB camera pipelie Srinivasan.

    2. Can you Confirm if this Pipeline is setup correctly for TDA4vh to access Ethernet camera, below command has the camera details

    1. root@j784s4-evm:/dev# gst-launch-1.0 -v udpsrc multicast-group=224.0.40.116 multicast-iface="eth1" port=5006 caps="application/x-rtp, media=(string)video, clock-rate=(int)90000, encoding-name=(string)H264, payload=(int)96" auto-multicast=true ! rtph264depay ! decodebin ! videoconvert ! videoscale ! video/x-raw,width=640,height=480 ! autovideosink sync=false
      Setting pipeline to PAUSED ...
      Pipeline is live and does not need PREROLL ...
      Got context from element 'autovideosink0': gst.gl.GLDisplay=context, gst.gl.GLDisplay=(GstGLDisplay)"\(GstGLDisplayWayland\)\ gldisplaywayland0";
      Pipeline is PREROLLED ...
      Setting pipeline to PLAYING ...
      /GstPipeline:pipeline0/GstUDPSrc:udpsrc0.GstPad:src: caps = application/x-rtp, media=(string)video, clock-rate=(int)90000, encoding-name=(string)H2                      64, payload=(int)96
      /GstPipeline:pipeline0/GstRtpH264Depay:rtph264depay0.GstPad:sink: caps = application/x-rtp, media=(string)video, clock-rate=(int)90000, encoding-na                      me=(string)H264, payload=(int)96
      New clock: GstSystemClock
    2. not sure if this helps but I can see video out properly with same pipeline when tested on AM62p EVM. 
  • Thanks you for USB camera pipelie Srinivasan

    No problem!

    Can you Confirm if this Pipeline is setup correctly for TDA4vh to access Ethernet camera, below command has the camera details

    1. Yes I can confirm that this pipeline looks correct and functioning as long as eth1 is active and joined the multicast group. ]

    2. Like mentioned earlier, if your pipeline is functional on AM62P then it will translate to TDA4VH.

    I hope this resolves your issue.

    Thank you,
    Sarabesh S.

  • Hi Srinivasan, 
    I still facing issue setting up Ethernet camera pipeline on TDA4VH getting this below error

    1. root@j784s4-evm:/dev# gst-launch-1.0 -v udpsrc multicast-group=224.0.40.116 multicast-iface="eth1" port=5006 caps="application/x-rtp, media=(string)video, clock-rate=(int)90000, encoding-name=(string)H264, payload=(int)96" auto-multicast=true ! rtph264depay ! decodebin ! videoconvert ! videoscale ! video/x-raw,width=640,height=480 ! autovideosink sync=false
      Setting pipeline to PAUSED ...
      Pipeline is live and does not need PREROLL ...
      Got context from element 'autovideosink0': gst.gl.GLDisplay=context, gst.gl.GLDisplay=(GstGLDisplay)"\(GstGLDisplayWayland\)\ gldisplaywayland0";
      Pipeline is PREROLLED ...
      Setting pipeline to PLAYING ...
      /GstPipeline:pipeline0/GstUDPSrc:udpsrc0.GstPad:src: caps = application/x-rtp, media=(string)video, clock-rate=(int)90000, encoding-name=(string)H264, payload=(int)96
      /GstPipeline:pipeline0/GstRtpH264Depay:rtph264depay0.GstPad:sink: caps = application/x-rtp, media=(string)video, clock-rate=(int)90000, encoding-name=(string)H264, payload=(int)96
      New clock: GstSystemClock


      is there something I can do to understand this problem? 
  • Hello, 

    Can you add GST_DEBUG=3 to the beginning of the pipeline: "GST_DEBUG=3 gst-launch-1.0 ..."

    Please share logs once you do this.

    Thanks,
    Sarabesh S.

  • hi srinivasan, 
    I tried to resolve this issue in few different ways none of which worked.
    First thing I tried is to make sure data is available with this command > sudo tcpdump -i eth0 udp port 5006 observed lot of packet drops, below is the response

    05:08:22.667563 IP 192.168.40.111.5004 > 224.0.40.116.5006: UDP, length 346
    05:08:22.668181 IP 192.168.40.111.5004 > 224.0.40.116.5006: UDP, length 1454
    05:08:22.668302 IP 192.168.40.111.5004 > 224.0.40.116.5006: UDP, length 1454
    05:08:22.668424 IP 192.168.40.111.5004^C

    1085 packets captured
    4249 packets received by filter
    2372 packets dropped by kernel

    I tried to increase buffer which did not work below is the command 

    GST_DEBUG=3 gst-launch-1.0 -v udpsrc multicast-group=224.0.40.116 multicast-iface=eth0 port=5006 buffer-size=26214400 caps="application/x-rtp, media=video, clock-rate=90000, encoding-name=H264, payload=96" auto-multicast=true ! rtph264depay ! h264parse ! avdec_h264 ! videoconvert ! autovideosink sync=false

    Response is: but no video out on display

    root@j784s4-evm:~# GST_DEBUG=3 gst-launch-1.0 -v udpsrc multicast-group=224.0.40.116 multicast-iface=eth0 port=5006 buffer-size=26214400 caps="application/x-rtp, media=video, clock-rate=90000, encoding-name=H264, payload=96" auto-multicast=true ! rtph264depay ! h264parse ! avdec_h264 ! videoconvert ! autovideosink sync=false
    Setting pipeline to PAUSED ...
    0:00:00.140075125  1356     0x3c278350 WARN               glcontext gstglcontext_egl.c:552:gst_gl_context_egl_dump_config:<glcontextegl0> unknown EGL_COLOR_BUFFER_TYPE value 3300
    0:00:00.140164575  1356     0x3c278350 WARN               glcontext gstglcontext_egl.c:552:gst_gl_context_egl_dump_config:<glcontextegl0> unknown EGL_COLOR_BUFFER_TYPE value 3300
    0:00:00.140183065  1356     0x3c278350 WARN               glcontext gstglcontext_egl.c:552:gst_gl_context_egl_dump_config:<glcontextegl0> unknown EGL_COLOR_BUFFER_TYPE value 3300
    0:00:00.140211245  1356     0x3c278350 WARN               glcontext gstglcontext_egl.c:552:gst_gl_context_egl_dump_config:<glcontextegl0> unknown EGL_COLOR_BUFFER_TYPE value 3300
    0:00:00.140230145  1356     0x3c278350 WARN               glcontext gstglcontext_egl.c:552:gst_gl_context_egl_dump_config:<glcontextegl0> unknown EGL_COLOR_BUFFER_TYPE value 3300
    0:00:00.140246360  1356     0x3c278350 WARN               glcontext gstglcontext_egl.c:552:gst_gl_context_egl_dump_config:<glcontextegl0> unknown EGL_COLOR_BUFFER_TYPE value 3300
    0:00:00.140262570  1356     0x3c278350 WARN               glcontext gstglcontext_egl.c:552:gst_gl_context_egl_dump_config:<glcontextegl0> unknown EGL_COLOR_BUFFER_TYPE value 3300
    0:00:00.140279105  1356     0x3c278350 WARN               glcontext gstglcontext_egl.c:552:gst_gl_context_egl_dump_config:<glcontextegl0> unknown EGL_COLOR_BUFFER_TYPE value 3300
    0:00:00.140295095  1356     0x3c278350 WARN               glcontext gstglcontext_egl.c:552:gst_gl_context_egl_dump_config:<glcontextegl0> unknown EGL_COLOR_BUFFER_TYPE value 3300
    0:00:00.140311190  1356     0x3c278350 WARN               glcontext gstglcontext_egl.c:552:gst_gl_context_egl_dump_config:<glcontextegl0> unknown EGL_COLOR_BUFFER_TYPE value 3300
    0:00:00.140327520  1356     0x3c278350 WARN               glcontext gstglcontext_egl.c:552:gst_gl_context_egl_dump_config:<glcontextegl0> unknown EGL_COLOR_BUFFER_TYPE value 3300
    0:00:00.140343685  1356     0x3c278350 WARN               glcontext gstglcontext_egl.c:552:gst_gl_context_egl_dump_config:<glcontextegl0> unknown EGL_COLOR_BUFFER_TYPE value 3300
    0:00:00.140359885  1356     0x3c278350 WARN               glcontext gstglcontext_egl.c:552:gst_gl_context_egl_dump_config:<glcontextegl0> unknown EGL_COLOR_BUFFER_TYPE value 3300
    0:00:00.140376170  1356     0x3c278350 WARN               glcontext gstglcontext_egl.c:552:gst_gl_context_egl_dump_config:<glcontextegl0> unknown EGL_COLOR_BUFFER_TYPE value 3300
    0:00:00.140392070  1356     0x3c278350 WARN               glcontext gstglcontext_egl.c:552:gst_gl_context_egl_dump_config:<glcontextegl0> unknown EGL_COLOR_BUFFER_TYPE value 3300
    0:00:00.140408290  1356     0x3c278350 WARN               glcontext gstglcontext_egl.c:552:gst_gl_context_egl_dump_config:<glcontextegl0> unknown EGL_COLOR_BUFFER_TYPE value 3300
    0:00:00.140424255  1356     0x3c278350 WARN               glcontext gstglcontext_egl.c:552:gst_gl_context_egl_dump_config:<glcontextegl0> unknown EGL_COLOR_BUFFER_TYPE value 3300
    0:00:00.140440195  1356     0x3c278350 WARN               glcontext gstglcontext_egl.c:552:gst_gl_context_egl_dump_config:<glcontextegl0> unknown EGL_COLOR_BUFFER_TYPE value 3300
    0:00:00.140457145  1356     0x3c278350 WARN               glcontext gstglcontext_egl.c:552:gst_gl_context_egl_dump_config:<glcontextegl0> unknown EGL_COLOR_BUFFER_TYPE value 3300
    0:00:00.140473735  1356     0x3c278350 WARN               glcontext gstglcontext_egl.c:552:gst_gl_context_egl_dump_config:<glcontextegl0> unknown EGL_COLOR_BUFFER_TYPE value 3300
    0:00:00.473278085  1356     0x3c278350 WARN               glcontext gstglcontext_egl.c:552:gst_gl_context_egl_dump_config:<glcontextegl0> unknown EGL_COLOR_BUFFER_TYPE value 3300
    0:00:00.473297010  1356     0x3c278350 WARN               glcontext gstglcontext_egl.c:552:gst_gl_context_egl_dump_config:<glcontextegl0> unknown EGL_COLOR_BUFFER_TYPE value 3300
    0:00:00.473313095  1356     0x3c278350 WARN               glcontext gstglcontext_egl.c:552:gst_gl_context_egl_dump_config:<glcontextegl0> unknown EGL_COLOR_BUFFER_TYPE value 3300
    0:00:00.473329260  1356     0x3c278350 WARN               glcontext gstglcontext_egl.c:552:gst_gl_context_egl_dump_config:<glcontextegl0> unknown EGL_COLOR_BUFFER_TYPE value 3300
    0:00:00.473345260  1356     0x3c278350 WARN               glcontext gstglcontext_egl.c:552:gst_gl_context_egl_dump_config:<glcontextegl0> unknown EGL_COLOR_BUFFER_TYPE value 3300
    0:00:00.473361270  1356     0x3c278350 WARN               glcontext gstglcontext_egl.c:552:gst_gl_context_egl_dump_config:<glcontextegl0> unknown EGL_COLOR_BUFFER_TYPE value 3300
    0:00:00.473377175  1356     0x3c278350 WARN               glcontext gstglcontext_egl.c:552:gst_gl_context_egl_dump_config:<glcontextegl0> unknown EGL_COLOR_BUFFER_TYPE value 3300
    0:00:00.473393685  1356     0x3c278350 WARN               glcontext gstglcontext_egl.c:552:gst_gl_context_egl_dump_config:<glcontextegl0> unknown EGL_COLOR_BUFFER_TYPE value 3300
    0:00:00.473409910  1356     0x3c278350 WARN               glcontext gstglcontext_egl.c:552:gst_gl_context_egl_dump_config:<glcontextegl0> unknown EGL_COLOR_BUFFER_TYPE value 3300
    0:00:00.473425835  1356     0x3c278350 WARN               glcontext gstglcontext_egl.c:552:gst_gl_context_egl_dump_config:<glcontextegl0> unknown EGL_COLOR_BUFFER_TYPE value 3300
    0:00:00.473441895  1356     0x3c278350 WARN               glcontext gstglcontext_egl.c:552:gst_gl_context_egl_dump_config:<glcontextegl0> unknown EGL_COLOR_BUFFER_TYPE value 3300
    0:00:00.473457875  1356     0x3c278350 WARN               glcontext gstglcontext_egl.c:552:gst_gl_context_egl_dump_config:<glcontextegl0> unknown EGL_COLOR_BUFFER_TYPE value 3300
    0:00:00.473474005  1356     0x3c278350 WARN               glcontext gstglcontext_egl.c:552:gst_gl_context_egl_dump_config:<glcontextegl0> unknown EGL_COLOR_BUFFER_TYPE value 3300
    0:00:00.473489920  1356     0x3c278350 WARN               glcontext gstglcontext_egl.c:552:gst_gl_context_egl_dump_config:<glcontextegl0> unknown EGL_COLOR_BUFFER_TYPE value 3300
    0:00:00.473505920  1356     0x3c278350 WARN               glcontext gstglcontext_egl.c:552:gst_gl_context_egl_dump_config:<glcontextegl0> unknown EGL_COLOR_BUFFER_TYPE value 3300
    0:00:00.473521880  1356     0x3c278350 WARN               glcontext gstglcontext_egl.c:552:gst_gl_context_egl_dump_config:<glcontextegl0> unknown EGL_COLOR_BUFFER_TYPE value 3300
    0:00:00.473537935  1356     0x3c278350 WARN               glcontext gstglcontext_egl.c:552:gst_gl_context_egl_dump_config:<glcontextegl0> unknown EGL_COLOR_BUFFER_TYPE value 3300
    0:00:00.473553925  1356     0x3c278350 WARN               glcontext gstglcontext_egl.c:552:gst_gl_context_egl_dump_config:<glcontextegl0> unknown EGL_COLOR_BUFFER_TYPE value 3300
    0:00:00.806379640  1356     0x3c278350 WARN               glcontext gstglcontext_egl.c:552:gst_gl_context_egl_dump_config:<glcontextegl0> unknown EGL_COLOR_BUFFER_TYPE value 3300
    0:00:00.806397260  1356     0x3c278350 WARN               glcontext gstglcontext_egl.c:552:gst_gl_context_egl_dump_config:<glcontextegl0> unknown EGL_COLOR_BUFFER_TYPE value 3300
    0:00:00.806413450  1356     0x3c278350 WARN               glcontext gstglcontext_egl.c:552:gst_gl_context_egl_dump_config:<glcontextegl0> unknown EGL_COLOR_BUFFER_TYPE value 3300
    0:00:00.806429810  1356     0x3c278350 WARN               glcontext gstglcontext_egl.c:552:gst_gl_context_egl_dump_config:<glcontextegl0> unknown EGL_COLOR_BUFFER_TYPE value 3300
    0:00:00.806446045  1356     0x3c278350 WARN               glcontext gstglcontext_egl.c:552:gst_gl_context_egl_dump_config:<glcontextegl0> unknown EGL_COLOR_BUFFER_TYPE value 3300
    0:00:00.806462110  1356     0x3c278350 WARN               glcontext gstglcontext_egl.c:552:gst_gl_context_egl_dump_config:<glcontextegl0> unknown EGL_COLOR_BUFFER_TYPE value 3300
    0:00:00.806478175  1356     0x3c278350 WARN               glcontext gstglcontext_egl.c:552:gst_gl_context_egl_dump_config:<glcontextegl0> unknown EGL_COLOR_BUFFER_TYPE value 3300
    0:00:00.806494290  1356     0x3c278350 WARN               glcontext gstglcontext_egl.c:552:gst_gl_context_egl_dump_config:<glcontextegl0> unknown EGL_COLOR_BUFFER_TYPE value 3300
    0:00:00.806510310  1356     0x3c278350 WARN               glcontext gstglcontext_egl.c:552:gst_gl_context_egl_dump_config:<glcontextegl0> unknown EGL_COLOR_BUFFER_TYPE value 3300
    0:00:00.806526380  1356     0x3c278350 WARN               glcontext gstglcontext_egl.c:552:gst_gl_context_egl_dump_config:<glcontextegl0> unknown EGL_COLOR_BUFFER_TYPE value 3300
    warning: queue 0xffff8c000be0 destroyed while proxies still attached:
      xdg_wm_base@6 still attached
      wl_subcompositor@5 still attached
      wl_compositor@4 still attached
      wl_registry@2 still attached
    0:00:00.822166240  1356     0x3c278350 WARN               glcontext gstglcontext_egl.c:552:gst_gl_context_egl_dump_config:<glcontextegl1> unknown EGL_COLOR_BUFFER_TYPE value 3300
    0:00:00.822202955  1356     0x3c278350 WARN               glcontext gstglcontext_egl.c:552:gst_gl_context_egl_dump_config:<glcontextegl1> unknown EGL_COLOR_BUFFER_TYPE value 3300
    0:00:00.822220790  1356     0x3c278350 WARN               glcontext gstglcontext_egl.c:552:gst_gl_context_egl_dump_config:<glcontextegl1> unknown EGL_COLOR_BUFFER_TYPE value 3300
    0:00:00.822237710  1356     0x3c278350 WARN               glcontext gstglcontext_egl.c:552:gst_gl_context_egl_dump_config:<glcontextegl1> unknown EGL_COLOR_BUFFER_TYPE value 3300
    0:00:00.822254245  1356     0x3c278350 WARN               glcontext gstglcontext_egl.c:552:gst_gl_context_egl_dump_config:<glcontextegl1> unknown EGL_COLOR_BUFFER_TYPE value 3300
    0:00:00.822271040  1356     0x3c278350 WARN               glcontext gstglcontext_egl.c:552:gst_gl_context_egl_dump_config:<glcontextegl1> unknown EGL_COLOR_BUFFER_TYPE value 3300
    0:00:00.822287095  1356     0x3c278350 WARN               glcontext gstglcontext_egl.c:552:gst_gl_context_egl_dump_config:<glcontextegl1> unknown EGL_COLOR_BUFFER_TYPE value 3300
    0:00:00.822303385  1356     0x3c278350 WARN               glcontext gstglcontext_egl.c:552:gst_gl_context_egl_dump_config:<glcontextegl1> unknown EGL_COLOR_BUFFER_TYPE value 3300
    0:00:01.150611545  1356     0x3c278350 WARN               glcontext gstglcontext_egl.c:552:gst_gl_context_egl_dump_config:<glcontextegl1> unknown EGL_COLOR_BUFFER_TYPE value 3300
    0:00:01.150631220  1356     0x3c278350 WARN               glcontext gstglcontext_egl.c:552:gst_gl_context_egl_dump_config:<glcontextegl1> unknown EGL_COLOR_BUFFER_TYPE value 3300
    0:00:01.150647465  1356     0x3c278350 WARN               glcontext gstglcontext_egl.c:552:gst_gl_context_egl_dump_config:<glcontextegl1> unknown EGL_COLOR_BUFFER_TYPE value 3300
    0:00:01.150664155  1356     0x3c278350 WARN               glcontext gstglcontext_egl.c:552:gst_gl_context_egl_dump_config:<glcontextegl1> unknown EGL_COLOR_BUFFER_TYPE value 3300
    0:00:01.150680205  1356     0x3c278350 WARN               glcontext gstglcontext_egl.c:552:gst_gl_context_egl_dump_config:<glcontextegl1> unknown EGL_COLOR_BUFFER_TYPE value 3300
    0:00:01.150695965  1356     0x3c278350 WARN               glcontext gstglcontext_egl.c:552:gst_gl_context_egl_dump_config:<glcontextegl1> unknown EGL_COLOR_BUFFER_TYPE value 3300
    0:00:01.150711610  1356     0x3c278350 WARN               glcontext gstglcontext_egl.c:552:gst_gl_context_egl_dump_config:<glcontextegl1> unknown EGL_COLOR_BUFFER_TYPE value 3300
    0:00:01.150727020  1356     0x3c278350 WARN               glcontext gstglcontext_egl.c:552:gst_gl_context_egl_dump_config:<glcontextegl1> unknown EGL_COLOR_BUFFER_TYPE value 3300
    0:00:01.150742440  1356     0x3c278350 WARN               glcontext gstglcontext_egl.c:552:gst_gl_context_egl_dump_config:<glcontextegl1> unknown EGL_COLOR_BUFFER_TYPE value 3300
    0:00:01.150758410  1356     0x3c278350 WARN               glcontext gstglcontext_egl.c:552:gst_gl_context_egl_dump_config:<glcontextegl1> unknown EGL_COLOR_BUFFER_TYPE value 3300
    0:00:01.150773990  1356     0x3c278350 WARN               glcontext gstglcontext_egl.c:552:gst_gl_context_egl_dump_config:<glcontextegl1> unknown EGL_COLOR_BUFFER_TYPE value 3300
    0:00:01.150789425  1356     0x3c278350 WARN               glcontext gstglcontext_egl.c:552:gst_gl_context_egl_dump_config:<glcontextegl1> unknown EGL_COLOR_BUFFER_TYPE value 3300
    0:00:01.150805075  1356     0x3c278350 WARN               glcontext gstglcontext_egl.c:552:gst_gl_context_egl_dump_config:<glcontextegl1> unknown EGL_COLOR_BUFFER_TYPE value 3300
    0:00:01.150820745  1356     0x3c278350 WARN               glcontext gstglcontext_egl.c:552:gst_gl_context_egl_dump_config:<glcontextegl1> unknown EGL_COLOR_BUFFER_TYPE value 3300
    0:00:01.150836400  1356     0x3c278350 WARN               glcontext gstglcontext_egl.c:552:gst_gl_context_egl_dump_config:<glcontextegl1> unknown EGL_COLOR_BUFFER_TYPE value 3300
    0:00:01.150851790  1356     0x3c278350 WARN               glcontext gstglcontext_egl.c:552:gst_gl_context_egl_dump_config:<glcontextegl1> unknown EGL_COLOR_BUFFER_TYPE value 3300
    0:00:01.150867735  1356     0x3c278350 WARN               glcontext gstglcontext_egl.c:552:gst_gl_context_egl_dump_config:<glcontextegl1> unknown EGL_COLOR_BUFFER_TYPE value 3300
    0:00:01.150883415  1356     0x3c278350 WARN               glcontext gstglcontext_egl.c:552:gst_gl_context_egl_dump_config:<glcontextegl1> unknown EGL_COLOR_BUFFER_TYPE value 3300
    0:00:01.483706075  1356     0x3c278350 WARN               glcontext gstglcontext_egl.c:552:gst_gl_context_egl_dump_config:<glcontextegl1> unknown EGL_COLOR_BUFFER_TYPE value 3300
    0:00:01.483726310  1356     0x3c278350 WARN               glcontext gstglcontext_egl.c:552:gst_gl_context_egl_dump_config:<glcontextegl1> unknown EGL_COLOR_BUFFER_TYPE value 3300
    0:00:01.483743705  1356     0x3c278350 WARN               glcontext gstglcontext_egl.c:552:gst_gl_context_egl_dump_config:<glcontextegl1> unknown EGL_COLOR_BUFFER_TYPE value 3300
    0:00:01.483759790  1356     0x3c278350 WARN               glcontext gstglcontext_egl.c:552:gst_gl_context_egl_dump_config:<glcontextegl1> unknown EGL_COLOR_BUFFER_TYPE value 3300
    0:00:01.483775765  1356     0x3c278350 WARN               glcontext gstglcontext_egl.c:552:gst_gl_context_egl_dump_config:<glcontextegl1> unknown EGL_COLOR_BUFFER_TYPE value 3300
    0:00:01.483791610  1356     0x3c278350 WARN               glcontext gstglcontext_egl.c:552:gst_gl_context_egl_dump_config:<glcontextegl1> unknown EGL_COLOR_BUFFER_TYPE value 3300
    0:00:01.483807285  1356     0x3c278350 WARN               glcontext gstglcontext_egl.c:552:gst_gl_context_egl_dump_config:<glcontextegl1> unknown EGL_COLOR_BUFFER_TYPE value 3300
    0:00:01.483823105  1356     0x3c278350 WARN               glcontext gstglcontext_egl.c:552:gst_gl_context_egl_dump_config:<glcontextegl1> unknown EGL_COLOR_BUFFER_TYPE value 3300
    0:00:01.483839155  1356     0x3c278350 WARN               glcontext gstglcontext_egl.c:552:gst_gl_context_egl_dump_config:<glcontextegl1> unknown EGL_COLOR_BUFFER_TYPE value 3300
    0:00:01.483854815  1356     0x3c278350 WARN               glcontext gstglcontext_egl.c:552:gst_gl_context_egl_dump_config:<glcontextegl1> unknown EGL_COLOR_BUFFER_TYPE value 3300
    0:00:01.483871165  1356     0x3c278350 WARN               glcontext gstglcontext_egl.c:552:gst_gl_context_egl_dump_config:<glcontextegl1> unknown EGL_COLOR_BUFFER_TYPE value 3300
    0:00:01.483886980  1356     0x3c278350 WARN               glcontext gstglcontext_egl.c:552:gst_gl_context_egl_dump_config:<glcontextegl1> unknown EGL_COLOR_BUFFER_TYPE value 3300
    0:00:01.483902870  1356     0x3c278350 WARN               glcontext gstglcontext_egl.c:552:gst_gl_context_egl_dump_config:<glcontextegl1> unknown EGL_COLOR_BUFFER_TYPE value 3300
    0:00:01.483918545  1356     0x3c278350 WARN               glcontext gstglcontext_egl.c:552:gst_gl_context_egl_dump_config:<glcontextegl1> unknown EGL_COLOR_BUFFER_TYPE value 3300
    0:00:01.483934445  1356     0x3c278350 WARN               glcontext gstglcontext_egl.c:552:gst_gl_context_egl_dump_config:<glcontextegl1> unknown EGL_COLOR_BUFFER_TYPE value 3300
    0:00:01.483950090  1356     0x3c278350 WARN               glcontext gstglcontext_egl.c:552:gst_gl_context_egl_dump_config:<glcontextegl1> unknown EGL_COLOR_BUFFER_TYPE value 3300
    0:00:01.483965965  1356     0x3c278350 WARN               glcontext gstglcontext_egl.c:552:gst_gl_context_egl_dump_config:<glcontextegl1> unknown EGL_COLOR_BUFFER_TYPE value 3300
    0:00:01.483982195  1356     0x3c278350 WARN               glcontext gstglcontext_egl.c:552:gst_gl_context_egl_dump_config:<glcontextegl1> unknown EGL_COLOR_BUFFER_TYPE value 3300
    0:00:01.816798605  1356     0x3c278350 WARN               glcontext gstglcontext_egl.c:552:gst_gl_context_egl_dump_config:<glcontextegl1> unknown EGL_COLOR_BUFFER_TYPE value 3300
    0:00:01.816816330  1356     0x3c278350 WARN               glcontext gstglcontext_egl.c:552:gst_gl_context_egl_dump_config:<glcontextegl1> unknown EGL_COLOR_BUFFER_TYPE value 3300
    0:00:01.816832350  1356     0x3c278350 WARN               glcontext gstglcontext_egl.c:552:gst_gl_context_egl_dump_config:<glcontextegl1> unknown EGL_COLOR_BUFFER_TYPE value 3300
    0:00:01.816848275  1356     0x3c278350 WARN               glcontext gstglcontext_egl.c:552:gst_gl_context_egl_dump_config:<glcontextegl1> unknown EGL_COLOR_BUFFER_TYPE value 3300
    Pipeline is live and does not need PREROLL ...
    Got context from element 'autovideosink0': gst.gl.GLDisplay=context, gst.gl.GLDisplay=(GstGLDisplay)"\(GstGLDisplayWayland\)\ gldisplaywayland0";
    Pipeline is PREROLLED ...
    Setting pipeline to PLAYING ...
    /GstPipeline:pipeline0/GstUDPSrc:udpsrc0.GstPad:src: caps = application/x-rtp, media=(string)video, clock-rate=(int)90000, encoding-name=(string)H264, payload=(int)96
    New clock: GstSystemClock
    /GstPipeline:pipeline0/GstRtpH264Depay:rtph264depay0.GstPad:sink: caps = application/x-rtp, media=(string)video, clock-rate=(int)90000, encoding-name=(string)H264, payload=(int)96
    

    can you assist in this

  • Hello, 

    Could you follow the examples given in this FAQ:  [FAQ] SK-AM69: How to run GStreamer pipeline with RTSP source 

    This will provide a framework for how to write your pipeline.

    Thanks,
    Sarabesh S.