This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA4VM: Unhandled Exception in EL3 for SBL boot Flow

Part Number: TDA4VM

Tool/software:

Hello,

During our SBL boot flow, we are facing Unhandled Exception in EL3( ATF).

Regards,

Veeraiyan

NOTICE:  BL31: v2.10.0(release):v2.10.0-367-g00f1ec6b8-dirty
NOTICE:  BL31: Built : 12:44:19, Jul 10 2025
Unhandled Exception in EL3.
x30            = 0x0000000070007184
x0             = 0x0000000000000001
x1             = 0x000000007000a098
x2             = 0x000000007000a000
x3             = 0x0000000000000000
x4             = 0x0000000032401000
x5             = 0x0000000000000040
x6             = 0x000000007001803e
x7             = 0x0000000000000000
x8             = 0x0000000070000000
x9             = 0x00000000700105b0
x10            = 0x0000000032e00000
x11            = 0x0000000000000000
x12            = 0x0000000070009268
x13            = 0x0000000070009268
x14            = 0x0000000000000010
x15            = 0x0000000070000044
x16            = 0xe42fa8643fd1ab82
x17            = 0xc0a22c943d904fcc
x18            = 0x1e514f7b8b0781f4
x19            = 0x000000007000b438
x20            = 0x000000007000b3d0
x21            = 0xdd9861cff5cad4f8
x22            = 0x0eef1ea5a8940973
x23            = 0x2aa1f026eff7e1a8
x24            = 0x0000000070018000
x25            = 0x8386bc6737d352fe