Part Number: TDA4VP-Q1
Tool/software:
Hello Experts
We was trying to simulate the power dissipation of TDA4VP using the "J784S4_PowerEstimationTool_v0p8" tool.
We are trying to have a loading scenario where we call its as "reduced operation mode" to have the power dissipation as less as possible.
We experimented having all the loading to 0% but we observed that the power dissipation is as below.
| 125C | |
| IP | Total Power [mW] |
| A72 | 149 |
| C7x / MMA | 113 |
| Pulsar (Main) | 19 |
| GPU | 18 |
| Wave Encoder / Decoder | 14 |
| VPAC3 | 26 |
| DMPAC | 1 |
| Rest of chip | 8330 |
At 125degC its showing 8.3W and at 105degC its showing 5.6W.
Is this expected or there are some settings in the tool.
Note: We are calculating using Strong process
regards
Ratheesh