Other Parts Discussed in Thread: TDA4VL, AB15
Tool/software:
Hi Expert,
We use TDA4VL EVB with Linux SDK 9.2 to test. Now we can run an opengl application and display to eDP-1. But its resolution is 800x600 when we use kmsprint to query it:
root@j721s2-evm:~# kmsprint
Connector 0 (40) DP-1 (disconnected)
Encoder 0 (39) NONE
Connector 1 (50) eDP-1 (connected)
Encoder 1 (49) NONE
Crtc 1 (48) 800x600@60.32 40.000 800/40/128/88/- 600/1/4/23/- 60 (60.32) 0xa 0x48
Plane 1 (41) fb-id: 66 (crtcs: 0 1) 0,0 800x600 -> 0,0 800x600 (AR12 AB12 RA12 RG16 BG16 AR15 AB15 AR24 AB24 RA24 BA24 RG24 BG24 AR30 AB30 XR12 XB12 RX12 XR15 XB15 XR24 XB24 RX24 BX24 XR30 XB30 YUYV UYVY NV12)
FB 66 800x600
But in document EVM UserGuide_spruj69, it shows: "the second DisplayPort [J36] .. supports resolutions up to 1080p". How to change resolution to 1080p?
Thanks.
BR,
Jeff