Part Number: AM62L-PROCESSOR-SDK
Other Parts Discussed in Thread: AM62L
Tool/software:
Hi team,
When i was testing the first release sdk in u-boot level i was able to properly detect the adin phy in my board.But with the same changes done in the u-boot source in the new released sdk version i was unable to get that automatic detection .Adin Phy gets detected only after i give the command dhcp.
With the 11.00.15.05 SDK 
With the 11.00.05.02 SDK
Net: ADIN1300 PHY detected at addr 4
I want this to automatically detect as it was in the old sdk.Where should i have to make the changes.
Regards,
Dheeraj K