Hi,
we have to develop a medical device which is not life critical , but is class II and therefore has considerable reliability requirements.
There are some platforms very attractive , like BeagleBoard and some others , which are low cost , powerful and with very rich connectivity.
Is there anyone who reads this forum , which has experienced the use of any of these platforms for some medical application, or any kind of application that requires a considerable level of reliability ?
which development platform is suitable for this kind of application ? Originally i was thinking about the use af Android, which in spite of being new and having some complexity, seems stable; but by reading forums and reviews on the Internet,it seems that the opinions are conflicting.
The central question is not about real time, because we will use a dedicated board with a microcontroller for low level tasks with real time requirements; so, the focus is about reliability.