I'm working on a design, with the ARM uP AM335x ZCZ package where I would like to implement two Ethernet ports with MII(GMII) interface or RMII interface, and also NAND flash. I can see that I will get a pinconflict on pin U17, which shall be used for RXERR for the second PHY and as WP for the NAND Flash. Can you advise, how this can be solved?
Kind Regards Peter