This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM 368 with ADV 7842 decoder

We are looking to interface the ADV 7842 decoder as an input to the DM 368 to convert composite, s-video and dvi signals into a digital format for further processing.

Is it possible to interface ADV 7842 with DM 368? The ADV 7842 datasheet mentions support of ITU 656, 709 and various SMPTE standards at the output side. The DM 368 datasheet mentions support of ITU 601/656 and 1120. For Standard Definition signals therefore there doesn't seem to be a problem but are the High Definition signal support of both ICs compatible? If No, then which decoder would you suggest and why? If Yes then are there drivers available for this?

Any help or pointers to help material will be deeply appreciated.

Regards

PG