Tool/software:
Hi TI expert,
We are currently using the Sony IMX728 image sensor, which adopts the RCCG pixel pattern.
However, we noticed that the default tuning tool (python build) does not provide an explicit option for the RCCG pattern.
The available COLOR_PATTERN settings in the config file are:
# 0=RGGB; 1=GRBG; 2=GBRG; 3=BGGR; 4=MONO;
# 10=RGGI, 11=GRIG, 12=BGGI, 13=GBIG, 14=GIRG, 15=IGGR, 16=GIBG, 17=IGGB
COLOR_PATTERN xxx
It seems RCCG is not directly supported here.
Could you please advise which color pattern setting would be the most compatible with RCCG?
Or is there any workaround or recommended approach for using RCCG sensors in the TI tuning workflow?
Thank you very much for your assistance.
Best regards,
YL