Part Number: PROCESSOR-SDK-AM68A
Other Parts Discussed in Thread: AM68A, SK-AM68
Tool/software:
Hello TI Team,
I'm designing a custom board based on the AM68A reference design. The original board supports only two camera connectors, but I need to integrate three cameras for my application.
For testing, I successfully connected the third camera using an Arducam V3Link board. Now I want to integrate all three cameras directly into my custom board.
I have a few questions regarding connector options:
-
Can I use a 40-pin expansion connector to directly connect the third camera? If yes, what signals and pin configuration should I consider to ensure compatibility with the AM68A CSI-2 interface and V3Link setup?
-
Alternatively, can I integrate one of the Arducam V3Link connectors directly into my custom board? Are there any reference schematics or guidelines available for this?
-
What are the best practices for routing CSI-2 signals and FPD-Link III connections on a custom board to support three cameras reliably?