This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

NAND flash interface to OMAP 3530

Hi friends
am working on Devkit8000 board which has OMAP 3530. 1 GByte is allocated for GPMC
so we can connect NAND or NOR flash. the physical address range is 0x00000000 to 0x3fffffff.  
am working on USB mass storage device project, i need to interface 4GByte nand flash to
OMAP 3530. i cant connect 4 GByte to GPMC because memory limitation, how can i interface
4 GByte MLC NAND Flash (part number is MT29F32G08CBACAWP from micron). is it possible to use
GPIO pins for interface without NAND flash controller. please suggest if you have any ideas.

thanks and regards
N Reddy
email ID:babu.dec04@gmail.co