This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA2PXEVM: [TDA2Px][VALEO][DAT 2.1]: Bypassing ISS Internal ISP When Using Camera with Onboard ISP

Part Number: TDA2PXEVM

Tool/software:

I am working with a camera module that includes an onboard ISP, and I'm interfacing it with a TDA2Px SoC, which also has an internal ISP within the ISS. Since the image is already processed by the camera's ISP, I would like to know if it's possible to bypass the internal ISP in the ISS and route the image data directly to the resizer. Could you please confirm if this is feasible and what configuration would be needed? If possible kindly share the flow diagram.

Thank you