This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SK-AM62: An SDIO device is externally connected using the SD pins on the EVB board. After adapting the driver, a power-on failure error is reported

Part Number: SK-AM62


Tool/software:

HW:Connect an SDIO device via fly wires.

SW:arch/arm64/boot/dts/ti/k3-am62x-sk-common.dtsi

Rewrite the SDIO1 device node as follows:

&sdhci1 {
- /* SD/MMC */
- bootph-all;
- status = "okay";
- pinctrl-names = "default";
- pinctrl-0 = <&main_mmc1_pins_default>;
- disable-wp;
+ /* SD/MMC */
+ bootph-all;
+ status = "okay";
+ pinctrl-names = "default";
+ pinctrl-0 = <&main_mmc1_pins_default>;
+ /* Limit frequency to 50Mhz under 3.3v */
+ max-frequency = <50000000>;
+ sd-uhs-sdr12;
+ broken-cd;
+ no-sd;
+ no-mmc;
};

check dmesg log as follows:

root@am62xx-evm:~# dmesg | grep mmc
[ 1.897508] mmc0: CQHCI version 5.10
[ 1.939803] mmc0: SDHCI controller on fa10000.mmc [fa10000.mmc] using ADMA 64-bit
[ 1.949484] mmc1: CQHCI version 5.10
[ 2.024789] mmc0: Command Queue Engine enabled
[ 2.029287] mmc0: new HS200 MMC card at address 0001
[ 2.035544] mmcblk0: mmc0:0001 G1M15L 29.6 GiB
[ 2.043552] mmcblk0: p1
[ 2.046687] mmcblk0boot0: mmc0:0001 G1M15L 31.5 MiB
[ 2.052740] mmcblk0boot1: mmc0:0001 G1M15L 31.5 MiB
[ 2.058895] mmcblk0rpmb: mmc0:0001 G1M15L 4.00 MiB, chardev (239:0)
[ 3.477348] sdhci-am654 fa00000.mmc: Power on failed
[ 3.512954] mmc1: SDHCI controller on fa00000.mmc [fa00000.mmc] using ADMA 64-bit
[ 3.637011] EXT4-fs (mmcblk0p1): recovery complete
[ 3.642471] EXT4-fs (mmcblk0p1): mounted filesystem df55c9b4-ab34-4143-af16-febd6b620543 r/w with ordered data mode. Quota mode: none.
[ 5.269331] EXT4-fs (mmcblk0p1): re-mounted df55c9b4-ab34-4143-af16-febd6b620543 r/w. Quota mode: none.

add info below:

[ 1135.316321] mmc1: Timeout waiting for hardware cmd interrupt.
[ 1135.322092] mmc1: sdhci: ============ SDHCI REGISTER DUMP ===========
[ 1135.328519] mmc1: sdhci: Sys addr: 0x00000000 | Version: 0x00001004
[ 1135.334944] mmc1: sdhci: Blk size: 0x00000000 | Blk cnt: 0x00000000
[ 1135.341369] mmc1: sdhci: Argument: 0x00000000 | Trn mode: 0x00000000
[ 1135.347795] mmc1: sdhci: Present: 0x01f00001 | Host ctl: 0x00000001
[ 1135.354221] mmc1: sdhci: Power: 0x0000000e | Blk gap: 0x00000080
[ 1135.360645] mmc1: sdhci: Wake-up: 0x00000000 | Clock: 0x0000e8c3
[ 1135.367070] mmc1: sdhci: Timeout: 0x00000000 | Int stat: 0x00000000
[ 1135.373496] mmc1: sdhci: Int enab: 0x00ff0003 | Sig enab: 0x00ff0003
[ 1135.379921] mmc1: sdhci: ACmd stat: 0x00000000 | Slot int: 0x00000000
[ 1135.386346] mmc1: sdhci: Caps: 0x3de8c801 | Caps_1: 0x18002407
[ 1135.392772] mmc1: sdhci: Cmd: 0x00000000 | Max curr: 0x00000000
[ 1135.399196] mmc1: sdhci: Resp[0]: 0x00000000 | Resp[1]: 0x00000000
[ 1135.405622] mmc1: sdhci: Resp[2]: 0x00000000 | Resp[3]: 0x00000000
[ 1135.412047] mmc1: sdhci: Host ctl2: 0x00000000
[ 1135.416478] mmc1: sdhci: ADMA Err: 0x00000000 | ADMA Ptr: 0x0000000000000000
[ 1135.423596] mmc1: sdhci: ============================================