Part Number: CCSTUDIO
Tool/software:
I am new to Code Composer Studio version 20 (Theia based). A very simple issue has been getting in my way.
Once I have opened a workspace folder, if I exit CCS then reopen it, it assumes I want to open the folder last used. That would be convenient only if I always open the same workspace.
I can see no method to close that folder so I can open a different folder.
If I open a new folder, although both folders are not shown in the project explorer, CCS 20 acts as though both the old folder and the new folder are open.
Under the File menu, there is no option to close the current folder. Such an option is desperately needed.
Either that or is there a way to set an option to NOT open a folder each time the GUI is reopened?
CCS versions through version 12 ALWAYS gave a small pop-up window asking the user to select the desired workspace folder. What a wonderful feature that was!