I have just started using the DM8168 EVM, and can't work out how to get it to boot from the host. I have followed the DM816x EZ Software Developer's guide, and installed Code Sourcery and the EZ SDK. I then used the setup.sh script to to set up the development host. The instructions then punt on what to do next (particularly as regards boot switches) and I have checked out the u-Boot and board Technical Reference Manual, and tried a variety of plausible switch settings, but to no avail. I'd appreciate any help / pointers.
As an aside (or possibly central issue) how does the EVM get its IP address? I'm using an old Dell Inspiron 6000 laptop as host, with it getting its IP address wirelessly from the DHCP server in my router. The EVM is connected to the Dell's ethernet port. Is this wrong? Do I somehow need to put my ethernet port on a different sub-net from the router?
Thanks
Pete