Tool/software:
Hello,
We are developing using the AM6422. The system has now booted from the eMMC storage. When updating the real-time core program to the /lib/firmware
path via Ethernet, the operation reports success. However, after rebooting using the reboot
command, the system fails to start. The power-on print logs have been submitted.
The same program works correctly when transferred via Ethernet to other hardware units, confirming that the real-time core program itself is not the issue.
Given this situation, how can we regain access to the system? Is our only immediate option to erase and rewrite the eMMC? This approach is highly inconvenient for field operations. We hope you can provide some assistance.
U-Boot 2021.01-00001-g7e12ed6f28-dirty (Feb 27 2025 - 16:33:34 +0800) SoC: AM64X SR2.0 HS-FS Model: Texas Instruments AM642 EVM EEPROM not available at 80, trying to read at 81 Reading on-board EEPROM at 0x51 failed -1 DRAM: 2 GiB NAND: 0 MiB MMC: mmc@fa10000: 0, mmc@fa00000: 1 Loading Environment from MMC... OK In: serial@2800000 Out: serial@2800000 Err: serial@2800000 EEPROM not available at 80, trying to read at 81 Reading on-board EEPROM at 0x51 failed -1 Net: eth0: ethernet@8000000port@1 Hit any key to stop autoboot: 0 switch to partitions #0, OK mmc0(part 0) is current device SD/MMC found on device 0 Failed to load 'boot.scr' ** Unrecognized filesystem type ** 19079680 bytes read in 106 ms (171.7 MiB/s) 39165 bytes read in 3 ms (12.5 MiB/s) ## Flattened Device Tree blob at 88000000 Booting using the fdt blob at 0x88000000 Loading Device Tree to 000000008fef3000, end 000000008fffffff ... OK Starting kernel ... [ 0.000000] Booting Linux on physical CPU 0x0000000000 [0x410fd034] [ 0.000000] Linux version 5.10.168-g2c23e6c538 (byf@byf-virtual-machine) (aarch64-none-linux-gnu-gcc (GNU Toolchain for the A-profile Architecture 9.2-2019.12 (arm-9.10)) 9.2.1 20191025, GNU ld (GNU Toolchain for the A-profile Architecture 9.2-2019.12 (arm-9.10)) 2.33.1.20191209) #6 SMP PREEMPT Tue Feb 25 14:27:36 CST 2025 [ 0.000000] Machine model: Texas Instruments AM642 EVM [ 0.000000] earlycon: ns16550a0 at MMIO32 0x0000000002800000 (options '') [ 0.000000] printk: bootconsole [ns16550a0] enabled [ 0.000000] efi: UEFI not found. [ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a0000000, size 1 MiB [ 0.000000] OF: reserved mem: initialized node r5f-dma-memory@a0000000, compatible id shared-dma-pool [ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a0100000, size 285 MiB [ 0.000000] OF: reserved mem: initialized node r5f-memory@a0100000, compatible id shared-dma-pool [ 0.000000] OF: reserved mem: initialized node apps-shared-memory, compatible id dma-heap-carveout [ 0.000000] Zone ranges: [ 0.000000] DMA [mem 0x0000000080000000-0x00000000ffffffff] [ 0.000000] DMA32 empty [ 0.000000] Normal empty [ 0.000000] Movable zone start for each node [ 0.000000] Early memory node ranges [ 0.000000] node 0: [mem 0x0000000080000000-0x000000009e7fffff] [ 0.000000] node 0: [mem 0x000000009e800000-0x00000000b1e19fff] [ 0.000000] node 0: [mem 0x00000000b1e1b000-0x00000000b1e1ffff] [ 0.000000] node 0: [mem 0x00000000b1e20000-0x00000000b3e1ffff] [ 0.000000] node 0: [mem 0x00000000b3e20000-0x00000000ffffffff] [ 0.000000] Initmem setup node 0 [mem 0x0000000080000000-0x00000000ffffffff] [ 0.000000] cma: Reserved 512 MiB at 0x00000000dd000000 [ 0.000000] psci: probing for conduit method from DT. [ 0.000000] psci: PSCIv1.1 detected in firmware. [ 0.000000] psci: Using standard PSCI v0.2 function IDs [ 0.000000] psci: Trusted OS migration not required [ 0.000000] psci: SMC Calling Convention v1.2 [ 0.000000] percpu: Embedded 22 pages/cpu s51288 r8192 d30632 u90112 [ 0.000000] Detected VIPT I-cache on CPU0 [ 0.000000] CPU features: detected: ARM erratum 845719 [ 0.000000] CPU features: detected: GIC system register CPU interface [ 0.000000] Built 1 zonelists, mobility grouping on. Total pages: 516095 [ 0.000000] Kernel command line: console=ttyS2,115200n8 earlycon=ns16550a,mmio32,0x02800000 mtdparts=fc40000.spi.0:1m(ospi.tiboot3),2m(ospi.tispl),4m(ospi.u-boot),256k(ospi.env),256k(ospi.env.backup),57088k@8m(ospi.rootfs),256k(ospi.phypattern);omap2-nand.0:2m(NAND.tiboot3),2m(NAND.tispl),2m(NAND.tiboot3.backup),4m(NAND.u-boot),256k(NAND.u-boot-env),256k(NAND.u-boot-env.backup),-(NAND.file-system) root=PARTUUID=39ce1b5e-01 rw rootfstype=ext4 rootwait [ 0.000000] Dentry cache hash table entries: 262144 (order: 9, 2097152 bytes, linear) [ 0.000000] Inode-cache hash table entries: 131072 (order: 8, 1048576 bytes, linear) [ 0.000000] mem auto-init: stack:off, heap alloc:off, heap free:off [ 0.000000] Memory: 1163748K/2097148K available (11200K kernel code, 1160K rwdata, 4304K rodata, 1856K init, 433K bss, 409112K reserved, 524288K cma-reserved) [ 0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=2, Nodes=1 [ 0.000000] rcu: Preemptible hierarchical RCU implementation. [ 0.000000] rcu: RCU event tracing is enabled. [ 0.000000] rcu: RCU restricting CPUs from NR_CPUS=256 to nr_cpu_ids=2. [ 0.000000] Trampoline variant of Tasks RCU enabled. [ 0.000000] Tracing variant of Tasks RCU enabled. [ 0.000000] rcu: RCU calculated value of scheduler-enlistment delay is 25 jiffies. [ 0.000000] rcu: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=2 [ 0.000000] NR_IRQS: 64, nr_irqs: 64, preallocated irqs: 0 [ 0.000000] GICv3: GIC: Using split EOI/Deactivate mode [ 0.000000] GICv3: 256 SPIs implemented [ 0.000000] GICv3: 0 Extended SPIs implemented [ 0.000000] GICv3: Distributor has no Range Selector support [ 0.000000] GICv3: 16 PPIs implemented [ 0.000000] GICv3: CPU0: found redistributor 0 region 0:0x0000000001840000 [ 0.000000] ITS [mem 0x01820000-0x0182ffff] [ 0.000000] GIC: enabling workaround for ITS: Socionext Synquacer pre-ITS [ 0.000000] ITS@0x0000000001820000: Devices Table too large, reduce ids 20->19 [ 0.000000] ITS@0x0000000001820000: allocated 524288 Devices @80800000 (flat, esz 8, psz 64K, shr 0) [ 0.000000] ITS: using cache flushing for cmd queue [ 0.000000] GICv3: using LPI property table @0x0000000080030000 [ 0.000000] GIC: using cache flushing for LPI property table [ 0.000000] GICv3: CPU0: using allocated LPI pending table @0x0000000080040000 [ 0.000000] arch_timer: cp15 timer(s) running at 200.00MHz (phys). [ 0.000000] clocksource: arch_sys_counter: mask: 0xffffffffffffff max_cycles: 0x2e2049d3e8, max_idle_ns: 440795210634 ns [ 0.000005] sched_clock: 56 bits at 200MHz, resolution 5ns, wraps every 4398046511102ns [ 0.008537] Console: colour dummy device 80x25 [ 0.013128] Calibrating delay loop (skipped), value calculated using timer frequency.. 400.00 BogoMIPS (lpj=800000) [ 0.023805] pid_max: default: 32768 minimum: 301 [ 0.028628] LSM: Security Framework initializing [ 0.033416] Mount-cache hash table entries: 4096 (order: 3, 32768 bytes, linear) [ 0.040993] Mountpoint-cache hash table entries: 4096 (order: 3, 32768 bytes, linear) [ 0.050963] rcu: Hierarchical SRCU implementation. [ 0.056221] Platform MSI: msi-controller@1820000 domain created [ 0.062553] PCI/MSI: /bus@f4000/interrupt-controller@1800000/msi-controller@1820000 domain created [ 0.071814] EFI services will not be available. [ 0.076698] smp: Bringing up secondary CPUs ... I/TC: Secondary CPU 1 initializing I/TC: Secondary CPU 1 switching to normal world boot [ 0.090303] Detected VIPT I-cache on CPU1 [ 0.090342] GICv3: CPU1: found redistributor 1 region 0:0x0000000001860000 [ 0.090358] GICv3: CPU1: using allocated LPI pending table @0x0000000080050000 [ 0.090424] CPU1: Booted secondary processor 0x0000000001 [0x410fd034] [ 0.090552] smp: Brought up 1 node, 2 CPUs [ 0.119937] SMP: Total of 2 processors activated. [ 0.124751] CPU features: detected: 32-bit EL0 Support [ 0.130026] CPU features: detected: CRC32 instructions [ 0.143560] CPU: All CPU(s) started at EL2 [ 0.147764] alternatives: patching kernel code [ 0.153565] devtmpfs: initialized [ 0.163608] KASLR disabled due to lack of seed [ 0.168420] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 7645041785100000 ns [ 0.178394] futex hash table entries: 512 (order: 3, 32768 bytes, linear) [ 0.202860] pinctrl core: initialized pinctrl subsystem [ 0.208934] DMI not present or invalid. [ 0.213661] NET: Registered protocol family 16 [ 0.220085] DMA: preallocated 256 KiB GFP_KERNEL pool for atomic allocations [ 0.227484] DMA: preallocated 256 KiB GFP_KERNEL|GFP_DMA pool for atomic allocations [ 0.235584] DMA: preallocated 256 KiB GFP_KERNEL|GFP_DMA32 pool for atomic allocations [ 0.244365] thermal_sys: Registered thermal governor 'step_wise' [ 0.244372] thermal_sys: Registered thermal governor 'power_allocator' [ 0.250973] cpuidle: using governor menu [ 0.261948] hw-breakpoint: found 6 breakpoint and 4 watchpoint registers. [ 0.268961] ASID allocator initialised with 65536 entries [ 0.298477] HugeTLB registered 1.00 GiB page size, pre-allocated 0 pages [ 0.305365] HugeTLB registered 32.0 MiB page size, pre-allocated 0 pages [ 0.312218] HugeTLB registered 2.00 MiB page size, pre-allocated 0 pages [ 0.319066] HugeTLB registered 64.0 KiB page size, pre-allocated 0 pages [ 0.327338] cryptd: max_cpu_qlen set to 1000 [ 0.335222] k3-chipinfo 43000014.chipid: Family:AM64X rev:SR2.0 JTAGID[0x1bb3802f] Detected [ 0.344689] iommu: Default domain type: Translated [ 0.350114] SCSI subsystem initialized [ 0.354402] mc: Linux media interface: v0.10 [ 0.358795] videodev: Linux video capture interface: v2.00 [ 0.364495] pps_core: LinuxPPS API ver. 1 registered [ 0.369566] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it> [ 0.378908] PTP clock support registered [ 0.382948] EDAC MC: Ver: 3.0.0 [ 0.386996] omap-mailbox 29020000.mailbox: omap mailbox rev 0x66fc9100 [ 0.394477] FPGA manager framework [ 0.398072] Advanced Linux Sound Architecture Driver Initialized. [ 0.405486] clocksource: Switched to clocksource arch_sys_counter [ 0.412061] VFS: Disk quotas dquot_6.6.0 [ 0.416180] VFS: Dquot-cache hash table entries: 512 (order 0, 4096 bytes) [ 0.429767] Carveout Heap: Exported 32 MiB at 0x00000000b1e20000 [ 0.436073] NET: Registered protocol family 2 [ 0.440802] IP idents hash table entries: 32768 (order: 6, 262144 bytes, linear) [ 0.449917] tcp_listen_portaddr_hash hash table entries: 1024 (order: 2, 16384 bytes, linear) [ 0.458699] TCP established hash table entries: 16384 (order: 5, 131072 bytes, linear) [ 0.466936] TCP bind hash table entries: 16384 (order: 6, 262144 bytes, linear) [ 0.474687] TCP: Hash tables configured (established 16384 bind 16384) [ 0.481635] UDP hash table entries: 1024 (order: 3, 32768 bytes, linear) [ 0.488542] UDP-Lite hash table entries: 1024 (order: 3, 32768 bytes, linear) [ 0.496038] NET: Registered protocol family 1 [ 0.501128] RPC: Registered named UNIX socket transport module. [ 0.507223] RPC: Registered udp transport module. [ 0.512068] RPC: Registered tcp transport module. [ 0.516878] RPC: Registered tcp NFSv4.1 backchannel transport module. [ 0.523470] NET: Registered protocol family 44 [ 0.528035] PCI: CLS 0 bytes, default 64 [ 0.532872] hw perfevents: enabled with armv8_cortex_a53 PMU driver, 7 counters available [ 0.545705] Initialise system trusted keyrings [ 0.550526] workingset: timestamp_bits=46 max_order=19 bucket_order=0 [ 0.561728] squashfs: version 4.0 (2009/01/31) Phillip Lougher [ 0.568430] NFS: Registering the id_resolver key type [ 0.573666] Key type id_resolver registered [ 0.577952] Key type id_legacy registered [ 0.582133] nfs4filelayout_init: NFSv4 File Layout Driver Registering... [ 0.588983] nfs4flexfilelayout_init: NFSv4 Flexfile Layout Driver Registering... [ 0.596788] 9p: Installing v9fs 9p2000 file system support [ 0.646869] Key type asymmetric registered [ 0.651083] Asymmetric key parser 'x509' registered [ 0.656128] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 243) [ 0.663696] io scheduler mq-deadline registered [ 0.668327] io scheduler kyber registered [ 0.674693] pinctrl-single 4084000.pinctrl: 33 pins, size 132 [ 0.681113] pinctrl-single f4000.pinctrl: 180 pins, size 720 [ 0.688054] pinctrl-single a40000.timesync-router: 512 pins, size 2048 [ 0.703892] Serial: 8250/16550 driver, 10 ports, IRQ sharing enabled [ 0.726293] brd: module loaded [ 0.737801] loop: module loaded [ 0.742311] megasas: 07.714.04.00-rc1 [ 0.748794] libphy: num_reset_gpios=-2 [ 0.754221] tun: Universal TUN/TAP device driver, 1.6 [ 0.760055] igbvf: Intel(R) Gigabit Virtual Function Network Driver [ 0.766503] igbvf: Copyright (c) 2009 - 2012 Intel Corporation. [ 0.772627] sky2: driver version 1.30 [ 0.777680] VFIO - User Level meta-driver version: 0.3 [ 0.784141] i2c /dev entries driver [ 0.788865] sdhci: Secure Digital Host Controller Interface driver [ 0.795218] sdhci: Copyright(c) Pierre Ossman [ 0.800360] sdhci-pltfm: SDHCI platform and OF driver helper [ 0.807420] ledtrig-cpu: registered to indicate activity on CPUs [ 0.814031] SMCCC: SOC_ID: ARCH_SOC_ID not implemented, skipping .... [ 0.822344] optee: probing for conduit method. I/TC: Reserved shared memory is enabled I/TC: Dynamic shared memory is enabled I/TC: Normal World virtualization support is disabled I/TC: Asynchronous notifications are disabled [ 0.826938] optee: revision 3.20 (8e74d476) [ 0.843574] optee: dynamic shared memory is enabled [ 0.853314] optee: initialized driver [ 0.859536] NET: Registered protocol family 17 [ 0.864316] 9pnet: Installing 9P2000 support [ 0.868784] Key type dns_resolver registered [ 0.873658] Loading compiled-in X.509 certificates [ 0.893598] ti-sci 44043000.dmsc: lpm region is required for suspend but not provided. [ 0.901779] ti-sci 44043000.dmsc: ABI: 3.1 (firmware rev 0x0008 '8.6.4--v08.06.04 (Chill Capybar') [ 0.949401] ti-sci-intr bus@f4000:bus@4000000:interrupt-controller1: Interrupt Router 5 domain created [ 0.959254] ti-sci-intr bus@f4000:interrupt-controller0: Interrupt Router 3 domain created [ 0.968093] ti-sci-inta 48000000.interrupt-controller: Interrupt Aggregator domain 28 created [ 0.984499] ti-udma 485c0100.dma-controller: Number of rings: 68 [ 0.992200] ti-udma 485c0100.dma-controller: Channels: 24 (bchan: 12, tchan: 6, rchan: 6) [ 1.002569] ti-udma 485c0000.dma-controller: Number of rings: 288 [ 1.018107] ti-udma 485c0000.dma-controller: Channels: 44 (tchan: 29, rchan: 15) [ 1.029104] printk: console [ttyS2] disabled [ 1.033630] 2800000.serial: ttyS2 at MMIO 0x2800000 (irq = 16, base_baud = 3000000) is a 8250 [ 1.042398] printk: console [ttyS2] enabled [ 1.042398] printk: console [ttyS2] enabled [ 1.050841] printk: bootconsole [ns16550a0] disabled [ 1.050841] printk: bootconsole [ns16550a0] disabled [ 1.062593] 2810000.serial: ttyS3 at MMIO 0x2810000 (irq = 17, base_baud = 3000000) is a 8250 [ 1.082714] davinci_mdio 8000f00.mdio: Configuring MDIO in manual mode [ 1.089710] libphy: num_reset_gpios=2 [ 1.093385] mdio_bus 8000f00.mdio: mii_bus 8000f00.mdio couldn't get reset GPIO [ 1.101139] am65-cpsw-nuss 8000000.ethernet: initializing am65 cpsw nuss version 0x6BA00903, cpsw version 0x6BA80903 Ports: 3 quirks:00000006 [ 1.114119] am65-cpsw-nuss 8000000.ethernet: Use random MAC address [ 1.120400] am65-cpsw-nuss 8000000.ethernet: initialized cpsw ale version 1.4 [ 1.127531] am65-cpsw-nuss 8000000.ethernet: ALE Table size 512 [ 1.134226] pps pps0: new PPS source ptp0 [ 1.138734] am65-cpsw-nuss 8000000.ethernet: CPTS ver 0x4e8a010c, freq:500000000, add_val:1 pps:1 [ 1.149323] am65-cpsw-nuss 8000000.ethernet: set new flow-id-base 16 [ 1.160294] am65-cpts 39000000.cpts: CPTS ver 0x4e8a010c, freq:500000000, add_val:1 pps:0 [ 1.171711] mmc0: CQHCI version 5.10 [ 1.176217] mmc1: CQHCI version 5.10 [ 1.187968] davinci_mdio 8000f00.mdio: Configuring MDIO in manual mode [ 1.194975] libphy: num_reset_gpios=2 [ 1.198688] libphy: reset_delay_us2 [ 1.202174] libphy: reset_post_delay_us2 [ 1.206117] libphy: reset_delay_us2 [ 1.209602] libphy: reset_post_delay_us2 [ 1.216887] mmc0: SDHCI controller on fa10000.mmc [fa10000.mmc] using ADMA 64-bit [ 1.253502] davinci_mdio 8000f00.mdio: davinci mdio revision 9.7, bus freq 1000000 [ 1.264241] davinci_mdio 8000f00.mdio: phy[0]: device 8000f00.mdio:00, driver TI DP83867 [ 1.272364] davinci_mdio 8000f00.mdio: phy[1]: device 8000f00.mdio:01, driver TI DP83867 [ 1.282750] debugfs: Directory 'pd:114' with parent 'pm_genpd' already present! [ 1.300098] ALSA device list: [ 1.303185] No soundcards found. [ 1.316571] mmc0: Command Queue Engine enabled [ 1.321065] mmc0: new HS200 MMC card at address 0001 [ 1.326829] mmcblk0: mmc0:0001 G1M15L 29.6 GiB [ 1.331597] mmcblk0boot0: mmc0:0001 G1M15L partition 1 31.5 MiB [ 1.337703] mmcblk0boot1: mmc0:0001 G1M15L partition 2 31.5 MiB [ 1.343881] mmcblk0rpmb: mmc0:0001 G1M15L partition 3 4.00 MiB, chardev (237:0) [ 1.352403] mmcblk0: p1 [ 2.695549] sdhci-am654 fa00000.mmc: Power on failed [ 2.731192] mmc1: SDHCI controller on fa00000.mmc [fa00000.mmc] using ADMA 64-bit [ 3.074587] EXT4-fs (mmcblk0p1): recovery complete [ 3.079907] EXT4-fs (mmcblk0p1): mounted filesystem with ordered data mode. Opts: (null) [ 3.088091] VFS: Mounted root (ext4 filesystem) on device 179:1. [ 3.094634] devtmpfs: mounted [ 3.099000] Freeing unused kernel memory: 1856K [ 3.103663] Run /sbin/init as init process [ 3.192193] systemd[1]: System time before build time, advancing clock. [ 3.232944] NET: Registered protocol family 10 [ 3.238761] Segment Routing with IPv6 [ 3.261399] systemd[1]: systemd 244.5+ running in system mode. (+PAM -AUDIT -SELINUX +IMA -APPARMOR -SMACK +SYSVINIT +UTMP -LIBCRYPTSETUP -GCRYPT -GNUTLS +ACL +XZ -LZ4 -SECCOMP +BLKID -ELFUTILS +KMOD -IDN2 -IDN -PCRE2 default-hierarchy=hybrid) [ 3.283587] systemd[1]: Detected architecture arm64. Welcome to Arago 2021.09! [ 3.322238] systemd[1]: Set hostname to <am64xx-evm>. [ 3.626372] systemd[1]: /lib/systemd/system/startwlansta.service:7: Unknown key name 'After' in section 'Service', ignoring. [ 3.638948] systemd[1]: /lib/systemd/system/startwlanap.service:7: Unknown key name 'After' in section 'Service', ignoring. [ 3.676218] systemd[1]: /lib/systemd/system/irqbalanced.service:6: Unknown key name 'ConditionCPUs' in section 'Unit', ignoring. [ 3.714221] systemd[1]: /lib/systemd/system/docker.socket:6: ListenStream= references a path below legacy directory /var/run/, updating /var/run/docker.sock → /run/docker.sock; please update the unit file accordingly. [ 3.850793] random: systemd: uninitialized urandom read (16 bytes read) [ 3.862210] systemd[1]: Created slice system-getty.slice. [ OK ] Created slice system-getty.slice. [ 3.885744] random: systemd: uninitialized urandom read (16 bytes read) [ 3.894800] systemd[1]: Created slice system-serial\x2dgetty.slice. [ OK ] Created slice system-serial\x2dgetty.slice. [ 3.917753] random: systemd: uninitialized urandom read (16 bytes read) [ 3.926739] systemd[1]: Created slice system-syslog\x2dng.slice. [ OK ] Created slice system-syslog\x2dng.slice. [ 3.951919] systemd[1]: Created slice User and Session Slice. [ OK ] Created slice User and Session Slice. [ 3.974163] systemd[1]: Started Dispatch Password Requests to Console Directory Watch. [ OK ] Started Dispatch Password …ts to Console Directory Watch. [ 3.998071] systemd[1]: Started Forward Password Requests to Wall Directory Watch. [ OK ] Started Forward Password R…uests to Wall Directory Watch. [ 4.022040] systemd[1]: Reached target Paths. [ OK ] Reached target Paths. [ 4.037812] systemd[1]: Reached target Remote File Systems. [ OK ] Reached target Remote File Systems. [ 4.057795] systemd[1]: Reached target Slices. [ OK ] Reached target Slices. [ 4.073828] systemd[1]: Reached target Swap. [ OK ] Reached target Swap. [ 4.109576] systemd[1]: Listening on RPCbind Server Activation Socket. [ OK ] Listening on RPCbind Server Activation Socket. [ 4.133920] systemd[1]: Reached target RPC Port Mapper. [ OK ] Reached target RPC Port Mapper. [ 4.159492] systemd[1]: Listening on Process Core Dump Socket. [ OK ] Listening on Process Core Dump Socket. [ 4.182206] systemd[1]: Listening on initctl Compatibility Named Pipe. [ OK ] Listening on initctl Compatibility Named Pipe. [ 4.209971] systemd[1]: Condition check resulted in Journal Audit Socket being skipped. [ 4.219009] systemd[1]: Listening on Journal Socket (/dev/log). [ OK ] Listening on Journal Socket (/dev/log). [ 4.242600] systemd[1]: Listening on Journal Socket. [ OK ] Listening on Journal Socket. [ 4.258788] systemd[1]: Listening on Network Service Netlink Socket. [ OK ] Listening on Network Service Netlink Socket. [ 4.282577] systemd[1]: Listening on udev Control Socket. [ OK ] Listening on udev Control Socket. [ 4.306320] systemd[1]: Listening on udev Kernel Socket. [ OK ] Listening on udev Kernel Socket. [ 4.335960] systemd[1]: Mounting Huge Pages File System... Mounting Huge Pages File System... [ 4.359593] systemd[1]: Mounting POSIX Message Queue File System... Mounting POSIX Message Queue File System... [ 4.387659] systemd[1]: Mounting Kernel Debug File System... Mounting Kernel Debug File System... [ 4.416008] systemd[1]: Mounting Temporary Directory (/tmp)... Mounting Temporary Directory (/tmp)... [ 4.440806] systemd[1]: Starting Create list of static device nodes for the current kernel... Starting Create list of st…odes for the current kernel... [ 4.471651] systemd[1]: Starting RPC Bind... Starting RPC Bind... [ 4.494202] systemd[1]: Condition check resulted in File System Check on Root Device being skipped. [ 4.512223] systemd[1]: Starting Journal Service... Starting Journal Service... [ 4.546366] systemd[1]: Starting Load Kernel Modules... Starting Load Kernel Modules... [ 4.575592] systemd[1]: Starting Remount Root and Kernel File Systems... Starting Remount Root and Kernel File Systems... [ 4.591548] cryptodev: loading out-of-tree module taints kernel. [ 4.608299] systemd[1]: Starting udev Coldplug all Devices... Starting udev Coldplug all Devices...[ 4.620209] cryptodev: driver 1.10 loaded. [ 4.635840] EXT4-fs (mmcblk0p1): re-mounted. Opts: (null) [ 4.651819] systemd[1]: Started RPC Bind. [ OK ] Started RPC Bind. [ 4.670617] systemd[1]: Started Journal Service. [ OK ] Started Journal Service. [ OK ] Mounted Huge Pages File System. [ OK ] Mounted POSIX Message Queue File System. [ OK ] Mounted Kernel Debug File System. [ OK ] Mounted Temporary Directory (/tmp). [ OK ] Started Create list of sta… nodes for the current kernel. [ OK ] Started Load Kernel Modules. [ OK ] Started Remount Root and Kernel File Systems. Mounting Kernel Configuration File System... Starting Flush Journal to Persistent Storage 4.860970] random: systemd-journal: uninitialized urandom read (16 bytes read) 0m... [ 4.882067] random: systemd: uninitialized urandom read (16 bytes read) [ 4.889747] systemd-journald[173]: Received client request to flush runtime journal. Starting Apply Kernel Variables...[ 4.907960] random: systemd-journal: uninitialized urandom read (16 bytes read) Starting Create Static Device Nodes in /dev... [ OK ] Mounted Kernel Configuration File System. [ OK ] Started Flush Journal to Persistent Storage. [ OK ] Started Apply Kernel Variables. [ OK ] Started Create Static Device Nodes in /dev. [ OK ] Reached target Local File Systems (Pre). Mounting /media/ram... Mounting /var/volatile... Starting udev Kernel Device Manager... [ OK ] Mounted /media/ram. [ OK ] Started udev Coldplug all Devices. [ OK ] Mounted /var/volatile. Starting udev Wait for Complete Device Initialization... Starting Load/Save Random Seed... [ OK ] Reached target Local File Systems. Starting Create Volatile Files and Directories... [ OK ] Started udev Kernel Device Manager. [ OK ] Started Create Volatile Files and Directories. Starting Network Time Synchronization... Starting Update UTMP about System Boot/Shutdown... [ OK ] Started Update UTMP about System Boot/Shutdown. [ OK ] Started Network Time Synchronization. [ OK ] Reached target System Time Set. [ OK ] Reached target System Time Synchronized. [ 5.939969] random: systemd: uninitialized urandom read (16 bytes read) [ 6.125867] random: crng init done [ 6.129290] random: 64 urandom warning(s) missed due to ratelimiting [ OK ] Started Load/Save Random Seed. [ 6.290324] davinci_mdio 30032400.mdio: Configuring MDIO in manual mode [ 6.331922] libphy: num_reset_gpios=1 [ 6.351870] libphy: reset_delay_us2 [ 6.355517] libphy: reset_post_delay_us2 [ 6.365821] platform 78000000.r5f: configured R5F for remoteproc mode [ 6.385675] platform 78000000.r5f: assigned reserved memory node r5f-dma-memory@a0000000 [ 6.419107] davinci_mdio 30032400.mdio: davinci mdio revision 1.7, bus freq 1000000 [ 6.443051] davinci_mdio 30032400.mdio: phy[3]: device 30032400.mdio:03, driver TI DP83620 10/100 Mbps PHY [ 6.458780] remoteproc remoteproc0: 78000000.r5f is available [ 6.484617] remoteproc remoteproc0: powering up 78000000.r5f [ 6.490549] remoteproc remoteproc0: Booting fw image am64-main-r5f0_0-fw, size 2220032 [ 6.519598] k3_r5_rproc bus@f4000:r5fss@78400000: MCU cluster requires both R5F cores to be enabled but num_cores is set to = 1 [ 6.545804] Unable to handle kernel paging request at virtual address ffff80001321f368 [ 6.553886] Mem abort info: [ 6.556709] ESR = 0x96000007 [ 6.564881] EC = 0x25: DABT (current EL), IL = 32 bits [ 6.570366] SET = 0, FnV = 0 [ 6.573604] EA = 0, S1PTW = 0 [ 6.576866] Data abort info: [ 6.585585] ISV = 0, ISS = 0x00000007 [ 6.589438] CM = 0, WnR = 0 [ 6.592602] swapper pgtable: 4k pages, 48-bit VAs, pgdp=0000000082f39000 [ 6.605580] [ffff80001321f368] pgd=00000000fffff003, p4d=00000000fffff003, pud=00000000ffffe003, pmd=000000008649f003, pte=0000000000000000 [ 6.618380] Internal error: Oops: 96000007 [#1] PREEMPT SMP [ 6.623960] Modules linked in: rti_wdt ti_k3_r5_remoteproc virtio_rpmsg_bus sa2ul sha512_generic authenc pruss optee_rng rng_core sch_fq_codel cryptodev(O) ipv6 [ 6.638352] CPU: 0 PID: 145 Comm: kworker/0:2 Tainted: G O 5.10.168-g2c23e6c538 #6 [ 6.647214] Hardware name: Texas Instruments AM642 EVM (DT) [ 6.652805] Workqueue: events request_firmware_work_func [ 6.658122] pstate: 60000005 (nZCv daif -PAN -UAO -TCO BTYPE=--) [ 6.664134] pc : find_table.isra.0+0x158/0x1f8 [ 6.668584] lr : rproc_elf_load_rsc_table+0x34/0xa0 [ 6.673460] sp : ffff800012293c50 [ 6.676775] x29: ffff800012293c50 x28: ffff800011117000 [ 6.682090] x27: ffff8000113ebcc8 x26: 0000000000000001 [ 6.687405] x25: ffff000005d6d900 x24: ffff0000046bcb38 [ 6.692718] x23: 000000000000001d x22: ffff80001321eef8 [ 6.698030] x21: 000000000021e000 x20: ffff800013001000 [ 6.703341] x19: ffff800013001000 x18: 0000000000000000 [ 6.708650] x17: 0000000000000000 x16: 0000000000000000 [ 6.713963] x15: 00000048c72121f0 x14: 0000000000000145 [ 6.719275] x13: 0000000000000000 x12: 0000000000000001 [ 6.724588] x11: 0000000002b9ef6b x10: 00000000000009f0 [ 6.729898] x9 : ffff8000122939d0 x8 : ffff00007fc4de40 [ 6.735210] x7 : 0100000000000400 x6 : 0000000000000001 [ 6.740524] x5 : ffff00007fc4de68 x4 : 000000000021def8 [ 6.745835] x3 : 0000000000000000 x2 : ffff800013001000 [ 6.751147] x1 : ffff80001321f358 x0 : 0000000000000028 [ 6.756461] Call trace: [ 6.758915] find_table.isra.0+0x158/0x1f8 [ 6.763017] rproc_elf_load_rsc_table+0x34/0xa0 [ 6.767552] rproc_boot+0x4d0/0x690 [ 6.771049] rproc_auto_boot_callback+0x1c/0x38 [ 6.775586] request_firmware_work_func+0x4c/0x90 [ 6.780298] process_one_work+0x1a0/0x348 [ 6.784313] worker_thread+0x4c/0x440 [ 6.787983] kthread+0x140/0x160 [ 6.791221] ret_from_fork+0x10/0x30 [ 6.794805] Code: 8b040056 f90033e0 d37d4821 8b0102c1 (b9401038) [ 6.800901] ---[ end trace db34652282872a61 ]--- [ 6.914148] remoteproc remoteproc1: 30034000.pru is available [ 6.966425] remoteproc remoteproc2: 30004000.rtu is available [ 7.034545] remoteproc remoteproc3: 3000a000.txpru is available [ 7.115733] remoteproc remoteproc4: 30038000.pru is available [ 7.178155] remoteproc remoteproc5: 30006000.rtu is available [ 7.222067] remoteproc remoteproc6: 3000c000.txpru is available [ 7.239726] remoteproc remoteproc7: 300b4000.pru is available [ 7.278549] remoteproc remoteproc8: 30084000.rtu is available [ 7.323758] remoteproc remoteproc9: 3008a000.txpru is available [ 7.370352] remoteproc remoteproc10: 300b8000.pru is available [ 7.408939] remoteproc remoteproc11: 30086000.rtu is available [ 7.449259] remoteproc remoteproc12: 3008c000.txpru is available [ 8.545371] usbcore: registered new interface driver usbfs [ 8.551521] usbcore: registered new interface driver hub [ 8.559531] usbcore: registered new device driver usb [ 8.606516] xhci-hcd xhci-hcd.0.auto: xHCI Host Controller [ 8.612188] xhci-hcd xhci-hcd.0.auto: new USB bus registered, assigned bus number 1 [ 8.620271] xhci-hcd xhci-hcd.0.auto: hcc params 0x200073c9 hci version 0x100 quirks 0x0000002000010010 [ 8.629819] xhci-hcd xhci-hcd.0.auto: irq 523, io mem 0x0f410000 [ 8.636112] xhci-hcd xhci-hcd.0.auto: xHCI Host Controller [ 8.641689] xhci-hcd xhci-hcd.0.auto: new USB bus registered, assigned bus number 2 [ 8.649390] xhci-hcd xhci-hcd.0.auto: Host supports USB 3.0 SuperSpeed [ 8.656162] usb usb1: New USB device found, idVendor=1d6b, idProduct=0002, bcdDevice= 5.10 [ 8.664488] usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1 [ 8.671824] usb usb1: Product: xHCI Host Controller [ 8.676719] usb usb1: Manufacturer: Linux 5.10.168-g2c23e6c538 xhci-hcd [ 8.683367] usb usb1: SerialNumber: xhci-hcd.0.auto [ 8.689127] hub 1-0:1.0: USB hub found [ 8.693069] hub 1-0:1.0: 1 port detected [ 8.697740] usb usb2: We don't know the algorithms for LPM for this host, disabling LPM. [ 8.706035] usb usb2: New USB device found, idVendor=1d6b, idProduct=0003, bcdDevice= 5.10 [ 8.714336] usb usb2: New USB device strings: Mfr=3, Product=2, SerialNumber=1 [ 8.721622] usb usb2: Product: xHCI Host Controller [ 8.726522] usb usb2: Manufacturer: Linux 5.10.168-g2c23e6c538 xhci-hcd [ 8.733167] usb usb2: SerialNumber: xhci-hcd.0.auto [ 8.738889] hub 2-0:1.0: USB hub found [ 8.742775] hub 2-0:1.0: 1 port detected [ OK ] Started udev Wait for Complete Device Initialization. [ OK ] Started Hardware RNG Entropy Gatherer Daemon. [ OK ] Reached target System Initialization. [ OK ] Started Daily rotation of log files. [ OK ] Started Timer service to update the IP on OLED each 10s. [ OK ] Started Daily Cleanup of Temporary Directories. [ OK ] Reached target Timers. [ OK ] Listening on Avahi mDNS/DNS-SD Stack Activation Socket. [ OK ] Listening on D-Bus System Message Bus Socket. Starting Docker Socket for the API. [ OK ] Listening on dropbear.socket. Starting Reboot and dump vmcore via kexec... [ OK ] Listening on Docker Socket for the API. [ OK ] Reached target Sockets. [ OK ] Reached target Basic System. [ OK ] Started Job spooling tools. [ OK ] Started Periodic Command Scheduler. [ OK ] Started D-Bus System Message Bus. Starting Ethernet Bridge Filtering Tables... Starting Print notice about GPLv3 packages... Starting IPv6 Packet Filtering Framework... Starting IPv4 Packet Filtering Framework... [ OK ] Started irqbalance daemon. Starting Matrix GUI... Starting startwlanap... Starting startwlansta... Starting System Logger Daemon "default" instance... Starting Login Service... [ OK ] Started TEE Supplicant. Starting telnetd.service... [ OK ] Started Reboot and dump vmcore via kexec. [ OK ] Started Ethernet Bridge Filtering Tables. [ OK ] Started IPv6 Packet Filtering Framework. [ OK ] Started IPv4 Packet Filtering Framework. [ OK ] Started startwlansta. [ OK ] Started startwlanap. [ OK ] Reached target Network (Pre). Starting Network Service... [ 9.307885] startwlansta.sh[480]: mount: /media/mmcblk1p1: special device /dev/mmcblk1p1 does not exist. [ OK ] Started Matrix GUI. [ OK ] Started telnetd.service. Starting LSB: Expand Rootfs of boot device... Starting syslog.service... [ OK ] Listening on Load/Save RF …itch Status /dev/rfkill Watch. [ 9.688614] cfg80211: Loading compiled-in X.509 certificates for regulatory database [ 9.747186] cfg80211: Loaded X.509 cert 'sforshee: 00b28ddf47aef9cea7' [ OK ] Started syslog.service. [FAILED] Failed to start System Logger Daemon "default" instance. See 'systemctl status syslog-ng@default.service' for details. [ OK ] Stopped System Logger Daemon "default" instance. Starting System Logger Daemon "default" instance... [ OK ] Started Network Service. Starting Wait for Network to be Configured... Starting Network Name Resolution... [ 10.130029] am65-cpsw-nuss 8000000.ethernet eth1: PHY [8000f00.mdio:00] driver [TI DP83867] (irq=POLL) [ 10.165631] am65-cpsw-nuss 8000000.ethernet eth1: configuring for phy/rgmii-rxid link mode [FAILED] Failed to start System Logger Daemon "default" instance. See 'systemctl status syslog-ng@default.service' for details. [ OK ] Stopped System Logger Daemon "default" instance. Starting System Logger Daemon "default" instance... [FAILED] Failed to start System Logger Daemon "default" instance. See 'systemctl status syslog-ng@default.service' for details. [ OK ] Stopped System Logger Daemon "default" instance. Starting System Logger Daemon "default" instance... [ 11.015538] startwlansta.sh[475]: Wi-Fi user configuration file missing, exit [FAILED] Failed to start System Logger Daemon "default" instance. See 'systemctl status syslog-ng@default.service' for details. [ OK ] Stopped System Logger Daemon "default" instance. Starting System Logger Daemon "default" instance... [FAILED] Failed to start System Logger Daemon "default" instance. See 'systemctl status syslog-ng@default.service' for details. [ OK ] Stopped System Logger Daemon "default" instance. [FAILED] Failed to start System Logger Daemon "default" instance. See 'systemctl status syslog-ng@default.service' for details. *************************************************************** *************************************************************** NOTICE: This file system contains the following GPLv3 packages: autoconf bash bc binutils cifs-utils coreutils-stdbuf coreutils cpio cpp-symlinks cpp dosfstools elfutils g++-symlinks g++ gawk gcc-symlinks gcc gdb gdbserver gettext gstreamer1.0-libav gzip hidapi less libasm1 libbfd libdw1 libelf1 libgdbm-compat4 libgdbm6 libgettextlib libgettextsrc libgmp10 libidn2-0 libmpc3 libmpfr6 libreadline8 libunistring2 m4 make nettle parted tar which If you do not wish to distribute GPLv3 components please remove the above packages prior to distribution. This can be done using the opkg remove command. i.e.: opkg remove <package> Where <package> is the name printed in the list above NOTE: If the package is a dependency of another package you will be notified of the dependent packages. You should use the --force-removal-of-dependent-packages option to also remove the dependent packages as well *************************************************************** *************************************************************** [ OK ] Started Print notice about GPLv3 packages. [FAILED] Failed to start LSB: Expand Rootfs of boot device. See 'systemctl status resize_rootfs.service' for details. [FAILED] Failed to start Login Service. See 'systemctl status systemd-logind.service' for details. [FAILED] Failed to start Network Name Resolution. See 'systemctl status systemd-resolved.service' for details. [ OK ] Stopped Login Service. Starting Login Service... [ OK ] Stopped Network Name Resolution. [ **] (2 of 2) A start job is running for…be Configured (9min 4s / no limit)