This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM625: AM625: weston-keyboard alternative

Part Number: AM625

Tool/software:

Hello TI support,

I'm trying to set up a local server on Chromium version 111 running on a customized Kirkstone Linux for the AM625 platform.

Weston Keyboard: When clicking on an input field, the Weston keyboard appears, but when I click outside the input field and return to it, the backspace key on the keyboard stops functioning for old entry.

Mallit Keyboard: I'm encountering an error that says the Mallit keyboard cannot be used because some process is blocking it i.e it's already in use.

Chrome Virtual Keyboard Extension: When I click on an input field, the Chrome virtual keyboard doesn't appear at all.

What can be done to resolve these issues? Is there an alternative way to achieve full keyboard support on my customized Kirkstone Linux for the AM625 platform with Chromium version 111?

- NP