Other Parts Discussed in Thread: OMAPL138, SYSBIOS
I am a sys bios beginner.when I create a project use the task demo in ccsv4.step into Task_sleep(10) function is not return . program is dead.
i cannot find the issue. i am use the omapl138 chip.it is running in arm .
/*
* ======== main.c ========
*/
#include <xdc/std.h>
#include <xdc/runtime/Error.h>
#include <xdc/runtime/System.h>
#include <ti/sysbios/BIOS.h>
#include <ti/sysbios/knl/Task.h>
/*
* ======== taskFxn ========
*/
Void taskFxn(UArg a0, UArg a1)
{
System_printf("enter taskFxn()\n");
Task_sleep(10);
System_printf("exit taskFxn()\n");
}
/*
* ======== main ========
*/
Void main()
{
Task_Handle task;
Error_Block eb;
System_printf("enter main()\n");
Error_init(&eb);
task = Task_create(taskFxn, NULL, &eb);
if (task == NULL) {
System_printf("Task_create() failed!\n");
BIOS_exit(0);
}
BIOS_start(); /* enable interrupts and start SYS/BIOS */
}