Tool/software:
Hello TI Team,
we are facing an issue on a custom board based on a TI am6442 SoC.
Roughly once every 300 reboots, the U-Boot SPL hangs while attempting to start the k3_system_manager
after loading the SYSFW via rproc
.
The error happen at:
static void k3_start_system_controller(int rproc_id, bool rproc_loaded, ulong addr, ulong size)
---------------------------------------------------------------------------------------------------------------------------------------------------------
U-Boot SPL 2021.01-sickpca-08470-g4578b21c59 (May 18 2023 - 23:32:05 +0200) k3_system_controller sysctrler: k3_sysctrler_start: Boot Notification response failed. ret = -110 Firmware init failed on rproc (-110)resetting ...
---------------------------------------------------------------------------------------------------------------------------------------------------------
So far, we haven’t observed any anomalies on the Power Good signals during these occurrences.
Do you have any suggestions on what might cause this behavior? Are there any specific registers or debug mechanisms we can use to verify whether the k3_system_manager
is running correctly or has encountered a failure?
Any guidance or pointers would be greatly appreciated.
HW/SW:
am6442
eMMC raw boot
sysfw: v08.05.03 (Chill Capybar')
u-boot: 2021.01
Br
Stefan