This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BTSEL[2:0] DM368

Hi all,

I've got an personnal PCB and when I turn on the switch BTSEL[2:0] I've got 0,1V and not 3V ?

I've use the same shematic as DM368EVM

Where can come form the mater ? Is the device DM368 damaged?  The mater can come from RBL?

Thanks

Maxime