This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCSTUDIO: F28379D Launchpad Failure for CCSv20.2 (C2000Ware v5.5)

Part Number: CCSTUDIO
Other Parts Discussed in Thread: SYSCONFIG, C2000WARE

Tool/software:

This is not so much a question as it is a bug report for CCSv20.2 (C2000Ware v5.5).  CCS total fails even when the correct board is selected in sysconfig.  What I mean is that it will compile, but chip is totally unresponsive during debug.  This occurred with libraries I had written for this device, which worked with previous versions of CCS.  After some experimentation, this failure appears to be due to a missing predefined symbol.

Under Properties>Build>Tools>C2000 Compiler>Predefined Symbols, add _LAUNCHXL_F28379D under the "Pre-define NAME" and everything appears to work.