This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA4AEN-Q1: Display Support via SN65

Part Number: TDA4AEN-Q1
Other Parts Discussed in Thread: SN65DSI86

Tool/software:

Hello!

We are using TDA4AEN SDK to version 11.0 on a custom board that is similar to the J722S EVM.  We want to use the DSI -> SN65 to output to a mini-display-port connector, ideally so that it can be used in an vision application.

There are some references to the SN65 in vision_apps under utils/dss/src/app_dss_soc.c, but they are not used for this SOC.  Is this supported by the SDK? Is there an example/test application? It seems like the SN65DSI86  is not part of the Linux device tree for J722S.  If not already supported in the SDK,  what steps do we need to follow to make it work. 

After that, will there be any additional modifications in needed to get `app_single_cam.sh` to output a camera's video stream to the display via the SN65?