Part Number: AM623
Other Parts Discussed in Thread: SK-AM62B-P1, AM625
Tool/software:
Hi
We designed a new board, referring to the EVM of SK-AM62B-P1 (DDR4 also uses the same components)
Currently using MMC1 boot, but the console keeps stopping at the following. (Our SD card can boot normally in EVM, but the CPU we use is AM6234)
"U-Boot SPL 2025.01-00406-gcd91d7360181 (Mar 25 2025 - 16:14:37 +0000)
SYSFW ABI: 4.0 (firmware rev 0x000b '11.0.7--v11.00.07 (Fancy Rat)')
Changed A53 CPU frequency to 1250000000Hz (T grade) in DT
SPL initial stack usage: 13424 bytes"
We searched for some E2E information and saw someone saying that the console stops here because of a problem with DDR initialization. Is this information correct?
In addition, regarding the DDR4 part, the hardware has confirmed that the power supply and reset signals are normal.
May I ask what other possible problem directions we can look for? Whether it is software or hardware.