Other Parts Discussed in Thread: OMAP-L138
Dear E2E forum:
Thank you for your help.
I need to use I2C1 SCL on OMAP-L138 as a free running clock.
Can I2C1 SCL be a free running (non stop) clock?
Thank you,
Boris Ruvinsky
802-877-4978
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: OMAP-L138
Dear E2E forum:
Thank you for your help.
I need to use I2C1 SCL on OMAP-L138 as a free running clock.
Can I2C1 SCL be a free running (non stop) clock?
Thank you,
Boris Ruvinsky
802-877-4978
Hello Paul.
Thank you for your respond.
I am trying to use I2C1 SCL for the system self test and need to generate low frequency clock of ~4KHz.
I don't really need "the free running" clock as "all the time running clock".
I need to be able to run the clock from some point ("Start Condition") until I decided to stop the clock ("stop condition").
I have only one master (OMAP-L138) and only one slave.
I looked through the I2C documentation in User Guide (SPRUH77).
If I set ICMDR Register as following:
1. MST =1 for I2C master
2. TRX = 1 for Transmitter mode
3. RM = 1 for continuous I2C transmission
4. FDF = 1 for "free data format"
5. BC = "0h" for 8-bit data word.
I will set all the divider registers as required with "reset bit" IRS=0.
After that I will set IRS = 1 and generate "start condition" by setting STT = 1.
I expect the SCL to start after I set STT=1 and run continuously until "stop condition" is generated by setting STP=1 or "reset conditon" by setting IRS=0.
Will SCL look as continuous CLOCK in this time interval - from STT=1 to IRS=0?
Did I understand the I2C interface correctly or I am missing something?
Thank you for your help,
Boris Ruvinsky
802-877-4978
508-740-5002
Hello Paul.
Reading OMAP-L138 I2C documentation - I found DLB bit in ICMDR register.
If I set:
1. DLB=1 for Digital Loopback
2. FDF=0 - FDF=1 is not supported in DLB mode.
3. MST=1
4. TRX=1
5. BC=0
6. RM = 0
6. ICDC="0" for 65536 data words
According to Figure 23-23 on page982 (SPRUH77) - the SCL (of 4KHz for example) can last for ~65536*8/4000 = ~130Sec. That in case if EDMA provides the sufficient data for TX.
Is this correct?
As I understood - the external ACK is not required in DLB mode. Is it correct?
Thank you for your help,
Boris Ruvinsky
The best way would be to just set up the peripheral as a master transmitter and max out the ICCNT register. There will be 9 clocks per byte transmitted (the extra coming from the ACK cycle). You should also set the IGNACK bit of the ICEMDR register if the slave doesn't plan on sending ACKs back.
Jeff
Hello Jeff.
Thank you very much for your respond and information.
I have just one question:
1. If I2C Pin Function Register set to GPIO mode - the outputs are still Open Drain as in I2C mode?
Thank you,
Boris Ruvinsky
The chip does not use open drain buffers, even in I2C mode. It uses the same buffers as the other IOs except instead of driving high, it automatically configures the IO as an input.
You can mimic the open drain functionality yourself if you are going to bit-bang the interface. In other words, set the GPIO output to 0, and to drive low set it as an output, and for a 1 set it as an input letting the external resistors pull it up.
Jeff
Hello Jeff.
Thank you for your help.
For some reason I can't get the I2C1_SCL running.
I use the following settings:
1. ICCNT = 0 for 65536 data count
2. ICMDR[10]=1 for the "Master"
3. ICMDR[9] = 1 for Transmit
4. ICEMDR[1] = 1 for "Ignore NACK"
5. ICPSC = 0x9 for I2C clock frequency = 80/10=8MHz (SYSCLK4=80MHz)
6. I2C is enabled through the PSC1_11. PSC1_11 status register retunes 0x1E03 which means I2C1 is ON.
7. PINMUX4 = 0x22442244 - UART_TX/RX, I2C1_SDA/SCL, I2C0_SCL/SDA, GP1[6:7].
I2C0 works OK.
But I2C1 does not generate the SCL - looks dead.
Can you give me an idea what is going wrong?
Thank you for your help,
Boris Ruvinsky
I just noticed that Boris started a new thread asking the same question that I responded to above. It would be better to use that thread instead.