Other Parts Discussed in Thread: AM67, AM67A
Parts Discussed in Thread: AM62x, AM62Ax, AM62Dx, AM62Px, AM67, AM67A
The primary role of the Device Management (DM) R5F core is to run the DM task. However, there may be other non-DM code running on the DM R5F, alongside the DM task. The firmware running on the DM R5F core is initialized during boot time, either during SPL boot or SBL boot.
For more information about SPL boot and SBL boot, refer to the processor academy > Multicore > Boot flows: SBL vs SBL
AM62x || AM62Ax || AM62Px
We suggest one of these methods to check the binary:
- Find the DM R5F binary that is built into tispl.bin (For SPL boot flow) or loaded by the SBL (for SBL boot flow)
- During Linux runtime: Test if the ipc_rpmsg_echo_linux firmware is running on the DM R5F