Tool/software:
HI TI :
I want to use the dss1 lvds to display. How should the DTS be modified !
BR
dongcan
Tool/software:
HI TI :
I want to use the dss1 lvds to display. How should the DTS be modified !
BR
dongcan
Please refer: https://www.ti.com/lit/pdf/sprads3
Hi Divyansh :
I followed this guide to modify my dts. tidss panel-simple probe ok , but I couldn't measure the clock of dss1 old1 on the oscilloscope.
BR
dongcan
/* dss1 oldi1 dts */
&max9277_gmsl {
status = "okay";
ports {
port@0 {
lcd_in0: endpoint {
remote-endpoint = <&oldi1_dss1_out>;
};
};
};
};
&dss1 {
status = "okay";
assigned-clocks = <&k3_clks 235 7>,
<&k3_clks 241 0>;
assigned-clock-parents = <&k3_clks 235 9>, /* OLDI TX1 driven by PLL18 and DSS1 VP0 */
<&k3_clks 241 1>; /* PLL18 for DSS1 VP0 */
};
&oldi1_dss1 {
status = "okay";
};
&oldi1_dss1_ports {
#address-cells = <1>;
#size-cells = <0>;
port@0 {
reg = <0>;
oldi1_dss1_in: endpoint {
remote-endpoint = <&dss1_dpi0_out1>;
};
};
port@1 {
reg = <1>;
oldi1_dss1_out: endpoint {
remote-endpoint = <&lcd_in0>;
};
};
};
&dss1_ports {
/* VP1: Output to OLDI */
port@0 {
reg = <0>;
#address-cells = <1>;
#size-cells = <0>;
dss1_dpi0_out1: endpoint@0 {
reg = <0>;
remote-endpoint = <&oldi1_dss1_in>;
};
};
};
/* panel-simple.ko */
static struct panel_desc gmsl_max9277 = {
.timings = &gmsl_max9277_mode,
.num_timings = 1,
.bpc = 8,
.size = {
.width = 800,
.height = 545,
},
.bus_format = MEDIA_BUS_FMT_RGB888_1X7X4_SPWG,
.bus_flags = DRM_BUS_FLAG_DE_HIGH,
.connector_type = DRM_MODE_CONNECTOR_LVDS,
};
Hi divyansh Mittal:
I have updated the sdk to 11.01.05.03 , but this problem still exists.
uname -r
6.12.35-ge3e551586dfa-dirty
BR
dong can
Please share the following:
devmem2 0x3020a160 kmsprint --device=/dev/dri/by-path/platform-30200000.dss-card kmsprint --device=/dev/dri/by-path/platform-30220000.dss-card kmstest --device=/dev/dri/by-path/platform-30200000.dss-card #Share what you see on display/probe kmstest --device=/dev/dri/by-path/platform-30220000.dss-card #Share what you see on display/probe
diff --git a/arch/arm64/boot/dts/ti/k3-am62p5-sk.dts b/arch/arm64/boot/dts/ti/k3-am62p5-sk.dts index ddcbdee85..9075f7ace 100644 --- a/arch/arm64/boot/dts/ti/k3-am62p5-sk.dts +++ b/arch/arm64/boot/dts/ti/k3-am62p5-sk.dts @@ -218,16 +218,6 @@ sound_master: simple-audio-card,codec { }; }; - hdmi0: connector-hdmi { - compatible = "hdmi-connector"; - label = "hdmi"; - type = "a"; - port { - hdmi_connector_in: endpoint { - remote-endpoint = <&sii9022_out>; - }; - }; - }; }; &main_gpio0 { @@ -561,40 +551,6 @@ exp2: gpio@23 { "GPIO_eMMC_RSTn", "SoC_WLAN_SDIO_RST"; }; - sii9022: bridge-hdmi@3b { - compatible = "sil,sii9022"; - reg = <0x3b>; - interrupt-parent = <&exp1>; - interrupts = <16 IRQ_TYPE_EDGE_FALLING>; - #sound-dai-cells = <0>; - sil,i2s-data-lanes = < 0 >; - - hdmi_tx_ports: ports { - #address-cells = <1>; - #size-cells = <0>; - - /* - * HDMI can be serviced with 3 potential VPs - - * (DSS0 VP1 / DSS1 VP0 / DSS1 VP1). - * For now, we will service it with DSS0 VP1. - */ - port@0 { - reg = <0>; - - sii9022_in: endpoint { - remote-endpoint = <&dss0_dpi1_out>; - }; - }; - - port@1 { - reg = <1>; - - sii9022_out: endpoint { - remote-endpoint = <&hdmi_connector_in>; - }; - }; - }; - }; }; &main_i2c2 { @@ -841,6 +797,13 @@ AM62PX_MCU_IOPAD(0x028, PIN_OUTPUT, 0) /* (D7) WKUP_UART0_TXD */ >; bootph-all; }; + mcu_uart0_pins_default: mcu-uart0-default-pins { + pinctrl-single,pins = < + AM62PX_MCU_IOPAD(0x0014, PIN_INPUT, 0) /* (B6) /* MCU_UART0_RXD */ + AM62PX_MCU_IOPAD(0x0018, PIN_OUTPUT, 0) /* (C8) /* MCU_UART0_TXD */ + >; + bootph-all; + }; }; &wkup_uart0 { @@ -851,6 +814,13 @@ &wkup_uart0 { bootph-all; }; +&mcu_uart0 { + pinctrl-names = "default"; + pinctrl-0 = <&mcu_uart0_pins_default>; + status = "okay"; + bootph-all; +}; + /* mcu_gpio0 and mcu_gpio_intr are reserved for mcu firmware usage */ &mcu_gpio0 { status = "reserved"; @@ -863,7 +833,67 @@ &mcu_gpio_intr { &dss_oldi_io_ctrl { bootph-all; }; +&max9277_gmsl { + status = "okay"; + ports { + port@0 { + lcd_in0: endpoint { + remote-endpoint = <&oldi1_dss1_out>; + }; + }; + }; +}; + + +&dss1 { + status = "okay"; + assigned-clocks = <&k3_clks 235 7>, + <&k3_clks 241 0>; + assigned-clock-parents = <&k3_clks 235 9>, /* OLDI TX1 driven by PLL18 and DSS1 VP0 */ + <&k3_clks 241 1>; /* PLL18 for DSS1 VP0 */ +}; + +&oldi1_dss1 { + status = "okay"; +}; + +&oldi1_dss1_ports { + #address-cells = <1>; + #size-cells = <0>; + + port@0 { + reg = <0>; + + oldi1_dss1_in: endpoint { + remote-endpoint = <&dss1_dpi0_out1>; + }; + }; + + port@1 { + reg = <1>; + + oldi1_dss1_out: endpoint { + remote-endpoint = <&lcd_in0>; + }; + }; +}; + +&dss1_ports { + + /* VP1: Output to OLDI */ + port@0 { + reg = <0>; + #address-cells = <1>; + #size-cells = <0>; + + dss1_dpi0_out1: endpoint@0 { + reg = <0>; + remote-endpoint = <&oldi1_dss1_in>; + }; + }; +}; +#if 0 &dss0 { bootph-all; status = "okay"; @@ -881,6 +911,7 @@ dss0_dpi1_out: endpoint { }; }; }; +#endif &epwm0 { /* Pin 24/26 of J4 */ diff --git a/drivers/gpu/drm/panel/panel-simple.c b/drivers/gpu/drm/panel/panel-simple.c index cc05e4367..5b58de2a5 100644 --- a/drivers/gpu/drm/panel/panel-simple.c +++ b/drivers/gpu/drm/panel/panel-simple.c @@ -2923,6 +2923,32 @@ static const struct panel_desc lg_lb070wv8 = { .connector_type = DRM_MODE_CONNECTOR_LVDS, }; +static struct display_timing gmsl_max9277_mode = { + .pixelclock = {26160000,26160000,26160000}, + .hactive = {256,256,256}, + .hfront_porch = {403,403,403}, + .hback_porch = {45,45,45}, + .hsync_len = {96,96,96}, + .vactive = {64,64,64}, + .vfront_porch = {415,415,415}, + .vback_porch = {3,3,3}, + .vsync_len = {63,63,63}, +}; + +static struct panel_desc gmsl_max9277 = { + .timings = &gmsl_max9277_mode, + .num_timings = 1, + .bpc = 8, + .size = { + .width = 800, + .height = 545, + }, + .bus_format = MEDIA_BUS_FMT_RGB888_1X7X4_SPWG, + // .bus_flags = DRM_BUS_FLAG_DE_HIGH | DRM_BUS_FLAG_PIXDATA_SAMPLE_NEGEDGE, + .bus_flags = DRM_BUS_FLAG_DE_HIGH, + .connector_type = DRM_MODE_CONNECTOR_LVDS, +}; + static const struct drm_display_mode lincolntech_lcd185_101ct_mode = { .clock = 155127, .hdisplay = 1920, @@ -4780,7 +4806,12 @@ static const struct of_device_id platform_of_match[] = { }, { .compatible = "edt,etm043080dh6gp", .data = &edt_etm043080dh6gp, - }, { + }, + { + .compatible = "maxim,max9277", + .data = &gmsl_max9277, + }, + { .compatible = "edt,etm0430g0dh6", .data = &edt_etm0430g0dh6, }, {
kmsprint --device=/dev/dri/by-path/platform-30220000.dss-card Connector 0 (41) LVDS-1 (connected) Encoder 0 (40) NONE Crtc 0 (39) 256x64@60.00 26.160 256/403/96/45/? 64/415/63/3/? 60 (60.00) 0x0 0x48
kmstest --device=/dev/dri/by-path/platform-30220000.dss-card Connector 0/@41: LVDS-1 Crtc 0/@39: 256x64@60.00 26.160 256/403/96/45/? 64/415/63/3/? 60 (60.00) 0x0 0x48 Plane 0/@32: 0,0-256x64 Fb 49 256x64-XR24 press enter to exit
devmem2 0x3020a160 /dev/mem opened. [ 667.585644] audit: type=1701 audit(1736660868.476:47): auid=4294967295 uid=0 gid=0 ses=4294967295 subj=kernel pid=7170 comm="devmem2" exe="/usr/bin/devmem2" sig=7 res=1 Memory mapped at address 0xffff83811000. [ 667.610694] audit: type=1334 audit(1736660868.504:48): prog-id=32 op=LOAD [ 667.617570] audit: type=1334 audit(1736660868.508:49): prog-id=33 op=LOAD [ 667.624415] audit: type=1334 audit(1736660868.516:50): prog-id=34 op=LOAD Bus error (core dumped)
What happens when you set status of Dss0 to "okay"
Are you then able to read 0x3020a160?
If you are able to read, does the display work?
Hi,
I just checked on my end. I am able to get signals when configuring only OLDI TX1 and not TX0.
It is weird not reading 3020a160 is giving error to you, this is not the case on my setup.
Can you also read 0x3022a160?
You my try my reference implementation configuring a different panel to see if you are at least seeing data on the lines:
// SPDX-License-Identifier: GPL-2.0-or-later OR MIT /** * Rocktech Panel (single-link lvds) with AM62P-SK EVM in independent mode * * AM62P-SKEVM: https://www.ti.com/tool/SK-AM62P-LP * * Copyright (C) 2024 Texas Instruments Incorporated - http://www.ti.com/ */ /dts-v1/; /plugin/; #include <dt-bindings/gpio/gpio.h> #include <dt-bindings/interrupt-controller/irq.h> &{/} { display0 { compatible = "rocktech,rk101ii01d-ct", "panel-simple"; port { lcd0_in: endpoint { remote-endpoint = <&oldi1_dss1_out>; }; }; }; }; &dss1 { status = "okay"; assigned-clocks = <&k3_clks 235 7>, <&k3_clks 241 0>; assigned-clock-parents = <&k3_clks 235 9>, /* OLDI TX1 driven by PLL18 and DSS1 VP0 */ <&k3_clks 241 1>; /* PLL18 for DSS1 VP0 */ }; &oldi1_dss1 { status = "okay"; }; &oldi1_dss1_ports { #address-cells = <1>; #size-cells = <0>; port@0 { reg = <0>; oldi1_dss1_in: endpoint { remote-endpoint = <&dss1_dpi0_out1>; }; }; port@1 { reg = <1>; oldi1_dss1_out: endpoint { remote-endpoint = <&lcd0_in>; }; }; }; &dss1_ports { #address-cells = <1>; #size-cells = <0>; /* DSS1 VP1: Output to OLDI1 */ port@0 { reg = <0>; dss1_dpi0_out1: endpoint { remote-endpoint = <&oldi1_dss1_in>; }; }; };
[ 100.428365] [drm] Initialized tidss 1.0.0 for 30200000.dss on minor 0
[ 114.512253] [drm] Initialized tidss 1.0.0 for 30220000.dss on minor 1
When I set status of Dss0 to "okay", I still can't read 0x3020a160
DTS config
&max9277_gmsl { status = "okay"; ports { port@0 { lcd_in0: endpoint { remote-endpoint = <&oldi1_dss1_out>; }; }; }; }; &dss1 { status = "okay"; assigned-clocks = <&k3_clks 235 7>, <&k3_clks 241 0>; assigned-clock-parents = <&k3_clks 235 9>, /* OLDI TX1 driven by PLL18 and DSS1 VP0 */ <&k3_clks 241 1>; /* PLL18 for DSS1 VP0 */ }; &dss0 { bootph-all; status = "okay"; pinctrl-names = "default"; pinctrl-0 = <&main_dpi_pins_default>; }; &oldi1_dss1 { status = "okay"; }; &oldi1_dss1_ports { #address-cells = <1>; #size-cells = <0>; port@0 { reg = <0>; oldi1_dss1_in: endpoint { remote-endpoint = <&dss1_dpi0_out1>; }; }; port@1 { reg = <1>; oldi1_dss1_out: endpoint { remote-endpoint = <&lcd_in0>; }; }; }; &dss1_ports { /* VP1: Output to OLDI */ port@0 { reg = <0>; #address-cells = <1>; #size-cells = <0>; dss1_dpi0_out1: endpoint@0 { reg = <0>; remote-endpoint = <&oldi1_dss1_in>; }; }; };
Not able to read that register is very weird to me. Is there some kind of firewall you've setup to prevent read in your software application?
If you have TI EVM, would recommend checking if the panel works there with our dts.
Since devmem2 is not working, can you try reading that register through another core via CCS?
If I use dss0 odli0 alone, the registers"0x3020a160" can be read, after my days off I will try it on the ti evm board, thanks a lot bro!
With the same dts,
1. Can you read 0x3020a160 and 0x3022a160?
2. What happens when you replace 'rocktech' panel compatible with your panel compatible?
Hi Divyansh:
1、yes, I can read with EVM
2、clk was measured
Perhaps there is a problem with the hardware of the dss1 module of my custom board. By the way , how to enbale dss0 dual output synchronously with dpi and lvds? I used the dpi and lvds functions of dss0 respectively, and they worked normally. Here is another question of mine . SK-AM62P-LP: how to enbale dss0 dual output synchronously with dpi and lvds? - Processors forum - Processors - TI E2E support forums
Thanks
Dong Can
Yes, this most likely depicts issue on your custom board, especially since you are not able to access those registers.
Will respond to the other thread.