Part Number: AM69A
Tool/software:
On the AM69x series For the high speed serial interfaces, this product has an MCU CPSW2G,MAIN CPSW2G,and CPSW9G. Can all processors/cores can access these every interface when the chip is fully booted?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: AM69A
Tool/software:
On the AM69x series For the high speed serial interfaces, this product has an MCU CPSW2G,MAIN CPSW2G,and CPSW9G. Can all processors/cores can access these every interface when the chip is fully booted?
Hi,
Sorry for the delay in response on this.
Can all processors/cores can access these every interface when the chip is fully booted?
Yes,
Any core can configure any of the CPSW instances.
It is a good idea to limit the control of one instance from one core. But that core can be any core in any domain, no limitations on that.
Also note that by interface I am assuming you are referring to the hardware MAC. If you mean the software interfaces created for the CPSW, then the answer is no. In that case, you need to use Ethfw serves and client drivers on the cores you need to have access from.
See ethfw user guide for more details on this.
Regards,
Tanmay