Part Number: TDA4VL-Q1
Other Parts Discussed in Thread: TDA4VL, AM68, SK-AM68, J721S2XSOMXEVM, SN65DSI86
Tool/software:
Hi,
Hardware: TDA4VL custom board
Software:
- ti-processor-sdk-linux-edgeai-j721s2-evm-10_01_00_04-Linux-x86-Install.bin
- tisdk-edgeai-image-j721s2-evm.wic.xz
The low-level drivers have been modified, and the system boots to the filesystem. However, no display output appears on the DP-connected monitor. The logs show the following error:
[FAILED] Failed to start Weston, a Wayland compositor, as a system service.
See 'systemctl status weston.service' for details.
When testing with ‘kmsprint’ and ‘modetest -M tidss’, it appears that DRM and DSS are not initialized:
root@am68-sk:/opt/edgeai-gst-apps# kmsprint
terminate called after throwing an instance of 'std::runtime_error'
what(): failed to find DRM cards
Aborted (core dumped)
root@am68-sk:/opt/edgeai-gst-apps# modetest -M tidss
failed to open device 'tidss': No such file or directory
The defconfig uses the default settings (unmodified), with DRM and TI DSS configured as modules (=m) and compiled into .ko files. The full system logs are attached for reference.
Could your please review the logs and provide further debugging suggestions? Thank you!
The log:
U-Boot SPL 2024.04-ti-dirty (Jul 23 2025 - 09:25:40 +0000)
SYSFW ABI: 4.0 (firmware rev 0x000a '10.1.6--v10.01.06 (Fiery Fox)')
EEPROM not available at 0x50, trying to read at 0x51
Reading on-board EEPROM at 0x51 failed -121
SPL initial stack usage: 13456 bytes
Trying to boot from MMC2
Warning: Detected image signing certificate on GP device. Skipping certificate to prevent boot failure. This will fail if the image was also encrypted
Warning: Detected image signing certificate on GP device. Skipping certificate to prevent boot failure. This will fail if the image was also encrypted
Warning: Detected image signing certificate on GP device. Skipping certificate to prevent boot failure. This will fail if the image was also encrypted
Warning: Detected image signing certificate on GP device. Skipping certificate to prevent boot failure. This will fail if the image was also encrypted
Warning: Detected image signing certificate on GP device. Skipping certificate to prevent boot failure. This will fail if the image was also encrypted
Loading Environment from nowhere... OK
Starting ATF on ARM64 core...
NOTICE: BL31: v2.11.0(release):v2.11.0-906-g58b25570c9-dirty
NOTICE: BL31: Built : 04:20:32, Nov 1 2024
I/TC:
I/TC: OP-TEE version: 4.4.0-dev (gcc version 13.3.0 (GCC)) #1 Fri Oct 18 17:45:27 UTC 2024 aarch64
I/TC: WARNING: This OP-TEE configuration might be insecure!
I/TC: WARNING: Please check https://urldefense.com/v3/__https://optee.readthedocs.io/en/latest/architecture/porting_guidelines.html__;!!G3vK!TzkSzxLuFIHqsRAdaMwW87_nC4NHRrAYeghV6DaC6bqKIw47KznE2ox1HFNqu6LbAwWzcmhEaBb2OqrH$
I/TC: Primary CPU initializing
I/TC: GIC redistributor base address not provided
I/TC: Assuming default GIC group status and modifier
I/TC: SYSFW ABI: 4.0 (firmware rev 0x000a '10.1.6--v10.01.06 (Fiery Fox)')
I/TC: Activated SA2UL device
I/TC: Fixing SA2UL firewall owner for GP device
I/TC: Enabled firewalls for SA2UL TRNG device
I/TC: SA2UL TRNG initialized
I/TC: SA2UL Drivers initialized
I/TC: HUK Initialized
I/TC: Primary CPU switching to normal world boot
U-Boot SPL 2024.04-ti-dirty (Jul 23 2025 - 09:25:21 +0000)
SYSFW ABI: 4.0 (firmware rev 0x000a '10.1.6--v10.01.06 (Fiery Fox)')
i2c_omap i2c@42120000: pinctrl_select_state_full: uclass_get_device_by_phandle_id: err=-19
EEPROM not available at 0x50, trying to read at 0x51
Reading on-board EEPROM at 0x51 failed -121
Trying to boot from MMC2
Warning: Detected image signing certificate on GP device. Skipping certificate to prevent boot failure. This will fail if the image was also encrypted
Warning: Detected image signing certificate on GP device. Skipping certificate to prevent boot failure. This will fail if the image was also encrypted
U-Boot 2024.04-ti-dirty (Jul 23 2025 - 09:25:21 +0000)
SoC: J721S2 SR1.0 GP
Model: Texas Instruments J721S2 EVM
i2c_omap i2c@42120000: pinctrl_select_state_full: uclass_get_device_by_phandle_id: err=-19
EEPROM not available at 0x50, trying to read at 0x51
Reading on-board EEPROM at 0x51 failed -121
Board: J721S2X-PM1-SOM rev E1
DRAM: 2 GiB (effective 16 GiB)
Core: 117 devices, 33 uclasses, devicetree: separate
Flash: 0 Bytes
MMC: mmc@4f80000: 0, mmc@4fb0000: 1
Loading Environment from nowhere... OK
In: serial@2880000
Out: serial@2880000
Err: serial@2880000
am65_cpsw_nuss ethernet@46000000: K3 CPSW: nuss_ver: 0x6BA02102 cpsw_ver: 0x6BA82102 ale_ver: 0x00293904 Ports:1
EEPROM not available at 0x50, trying to read at 0x51
Reading on-board EEPROM at 0x51 failed -121
Net: Could not get PHY for mdio@f00: addr 0
am65_cpsw_nuss_port ethernet@46000000port@1: phy_connect() failed
No ethernet found.
Hit any key to stop autoboot: 0
i2c_write: error waiting for data ACK (status=0x116)
pca953x gpio@22: Error reading output register
switch to partitions #0, OK
mmc1 is current device
i2c_write: error waiting for data ACK (status=0x116)
pca953x gpio@22: Error reading output register
SD/MMC found on device 1
941 bytes read in 54 ms (16.6 KiB/s)
Loaded env from uEnv.txt
Importing environment from mmc1 ...
Running uenvcmd ...
k3_r5f_rproc r5f@41000000: Core 1 is already in use. No rproc commands work
k3_r5f_rproc r5f@41400000: Core 2 is already in use. No rproc commands work
495020 bytes read in 139 ms (3.4 MiB/s)
Load Remote Processor 2 with data@addr=0x82000000 495020 bytes: Success!
335060 bytes read in 133 ms (2.4 MiB/s)
Load Remote Processor 3 with data@addr=0x82000000 335060 bytes: Success!
Failed to load '/lib/firmware/j721s2-main-r5f1_0-fw'
Failed to load '/lib/firmware/j721s2-main-r5f1_1-fw'
14020752 bytes read in 695 ms (19.2 MiB/s)
Load Remote Processor 6 with data@addr=0x82000000 14020752 bytes: Success!
9703384 bytes read in 519 ms (17.8 MiB/s)
Load Remote Processor 7 with data@addr=0x82000000 9703384 bytes: Success!
21029376 bytes read in 920 ms (21.8 MiB/s)
112215 bytes read in 61 ms (1.8 MiB/s)
Working FDT set to 88000000
10307 bytes read in 56 ms (179.7 KiB/s)
## Flattened Device Tree blob at 88000000
Booting using the fdt blob at 0x88000000
Working FDT set to 88000000
ERROR: reserving fdt memory region failed (addr=880000000 size=2c000000 flags=4)
Loading Device Tree to 000000008fee1000, end 000000008fffffff ... OK
Working FDT set to 8fee1000
Starting kernel ...
[ 0.000000] Booting Linux on physical CPU 0x0000000000 [0x411fd080]
[ 0.000000] Linux version 6.6.44-ti-g541c20281af7-dirty (tisdk@WHETRON-SZ-TAO) (aarch64-oe-linux-gcc (GCC) 13.3.0, GNU ld (GNU Binutils) 2.42.0.20240723) #1 SMP PREEMPT Wed Jul 23 09:32:41 UTC 2025
[ 0.000000] KASLR disabled due to lack of seed
[ 0.000000] Machine model: Texas Instruments J721S2 EVM
[ 0.000000] earlycon: ns16550a0 at MMIO32 0x0000000002880000 (options '')
[ 0.000000] printk: bootconsole [ns16550a0] enabled
[ 0.000000] efi: UEFI not found.
[ 0.000000] OF: reserved mem: 0x000000009e800000..0x000000009fffffff (24576 KiB) nomap non-reusable optee@9e800000
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a0000000, size 1 MiB
[ 0.000000] OF: reserved mem: initialized node vision-apps-r5f-dma-memory@a0000000, compatible id shared-dma-pool
[ 0.000000] OF: reserved mem: 0x00000000a0000000..0x00000000a00fffff (1024 KiB) nomap non-reusable vision-apps-r5f-dma-memory@a0000000
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a0100000, size 15 MiB
[ 0.000000] OF: reserved mem: initialized node vision-apps-r5f-memory@a0100000, compatible id shared-dma-pool
[ 0.000000] OF: reserved mem: 0x00000000a0100000..0x00000000a0ffffff (15360 KiB) nomap non-reusable vision-apps-r5f-memory@a0100000
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a1000000, size 1 MiB
[ 0.000000] OF: reserved mem: initialized node vision-apps-r5f-dma-memory@a1000000, compatible id shared-dma-pool
[ 0.000000] OF: reserved mem: 0x00000000a1000000..0x00000000a10fffff (1024 KiB) nomap non-reusable vision-apps-r5f-dma-memory@a1000000
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a1100000, size 15 MiB
[ 0.000000] OF: reserved mem: initialized node vision-apps-r5f-memory@a1100000, compatible id shared-dma-pool
[ 0.000000] OF: reserved mem: 0x00000000a1100000..0x00000000a1ffffff (15360 KiB) nomap non-reusable vision-apps-r5f-memory@a1100000
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a2000000, size 1 MiB
[ 0.000000] OF: reserved mem: initialized node vision-apps-r5f-dma-memory@a2000000, compatible id shared-dma-pool
[ 0.000000] OF: reserved mem: 0x00000000a2000000..0x00000000a20fffff (1024 KiB) nomap non-reusable vision-apps-r5f-dma-memory@a2000000
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a2100000, size 31 MiB
[ 0.000000] OF: reserved mem: initialized node vision-apps-r5f-memory@a2100000, compatible id shared-dma-pool
[ 0.000000] OF: reserved mem: 0x00000000a2100000..0x00000000a3ffffff (31744 KiB) nomap non-reusable vision-apps-r5f-memory@a2100000
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a4000000, size 1 MiB
[ 0.000000] OF: reserved mem: initialized node vision-apps-r5f-dma-memory@a4000000, compatible id shared-dma-pool
[ 0.000000] OF: reserved mem: 0x00000000a4000000..0x00000000a40fffff (1024 KiB) nomap non-reusable vision-apps-r5f-dma-memory@a4000000
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a4100000, size 31 MiB
[ 0.000000] OF: reserved mem: initialized node vision-apps-r5f-memory@a4100000, compatible id shared-dma-pool
[ 0.000000] OF: reserved mem: 0x00000000a4100000..0x00000000a5ffffff (31744 KiB) nomap non-reusable vision-apps-r5f-memory@a4100000
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a6000000, size 1 MiB
[ 0.000000] OF: reserved mem: initialized node vision-apps-r5f-dma-memory@a6000000, compatible id shared-dma-pool
[ 0.000000] OF: reserved mem: 0x00000000a6000000..0x00000000a60fffff (1024 KiB) nomap non-reusable vision-apps-r5f-dma-memory@a6000000
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a6100000, size 15 MiB
[ 0.000000] OF: reserved mem: initialized node vision-apps-r5f-memory@a6100000, compatible id shared-dma-pool
[ 0.000000] OF: reserved mem: 0x00000000a6100000..0x00000000a6ffffff (15360 KiB) nomap non-reusable vision-apps-r5f-memory@a6100000
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a7000000, size 1 MiB
[ 0.000000] OF: reserved mem: initialized node vision-apps-r5f-dma-memory@a7000000, compatible id shared-dma-pool
[ 0.000000] OF: reserved mem: 0x00000000a7000000..0x00000000a70fffff (1024 KiB) nomap non-reusable vision-apps-r5f-dma-memory@a7000000
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a7100000, size 15 MiB
[ 0.000000] OF: reserved mem: initialized node vision-apps-r5f-memory@a7100000, compatible id shared-dma-pool
[ 0.000000] OF: reserved mem: 0x00000000a7100000..0x00000000a7ffffff (15360 KiB) nomap non-reusable vision-apps-r5f-memory@a7100000
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a8000000, size 32 MiB
[ 0.000000] OF: reserved mem: initialized node vision-apps-rtos-ipc-memory-region@a8000000, compatible id shared-dma-pool
[ 0.000000] OF: reserved mem: 0x00000000a8000000..0x00000000a9ffffff (32768 KiB) nomap non-reusable vision-apps-rtos-ipc-memory-region@a8000000
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000aa000000, size 96 MiB
[ 0.000000] OF: reserved mem: initialized node vision-apps-dma-memory@aa000000, compatible id shared-dma-pool
[ 0.000000] OF: reserved mem: 0x00000000aa000000..0x00000000afffffff (98304 KiB) nomap non-reusable vision-apps-dma-memory@aa000000
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000b0000000, size 1 MiB
[ 0.000000] OF: reserved mem: initialized node vision-apps-c71-dma-memory@b0000000, compatible id shared-dma-pool
[ 0.000000] OF: reserved mem: 0x00000000b0000000..0x00000000b00fffff (1024 KiB) nomap non-reusable vision-apps-c71-dma-memory@b0000000
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000b0100000, size 95 MiB
[ 0.000000] OF: reserved mem: initialized node vision-apps-c71_0-memory@b0100000, compatible id shared-dma-pool
[ 0.000000] OF: reserved mem: 0x00000000b0100000..0x00000000b5ffffff (97280 KiB) nomap non-reusable vision-apps-c71_0-memory@b0100000
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000b6000000, size 1 MiB
[ 0.000000] OF: reserved mem: initialized node vision-apps-c71_1-dma-memory@b6000000, compatible id shared-dma-pool
[ 0.000000] OF: reserved mem: 0x00000000b6000000..0x00000000b60fffff (1024 KiB) nomap non-reusable vision-apps-c71_1-dma-memory@b6000000
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000b6100000, size 31 MiB
[ 0.000000] OF: reserved mem: initialized node vision-apps-c71_1-memory@b6100000, compatible id shared-dma-pool
[ 0.000000] OF: reserved mem: 0x00000000b6100000..0x00000000b7ffffff (31744 KiB) nomap non-reusable vision-apps-c71_1-memory@b6100000
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000b8000000, size 64 MiB
[ 0.000000] OF: reserved mem: initialized node vision-apps-core-heap-memory-lo@b8000000, compatible id shared-dma-pool
[ 0.000000] OF: reserved mem: 0x00000000b8000000..0x00000000bbffffff (65536 KiB) nomap non-reusable vision-apps-core-heap-memory-lo@b8000000
[ 0.000000] Reserved memory: created DMA memory pool at 0x0000000880000000, size 704 MiB
[ 0.000000] OF: reserved mem: initialized node vision-apps-core-heap-memory-hi@880000000, compatible id shared-dma-pool
[ 0.000000] OF: reserved mem: 0x0000000880000000..0x00000008abffffff (720896 KiB) nomap non-reusable vision-apps-core-heap-memory-hi@880000000
[ 0.000000] OF: reserved mem: initialized node vision_apps_shared-memories, compatible id dma-heap-carveout
[ 0.000000] OF: reserved mem: 0x0000000900000000..0x000000091fffffff (524288 KiB) map non-reusable vision_apps_shared-memories
[ 0.000000] Reserved memory: created CMA memory pool at 0x0000000980000000, size 896 MiB
[ 0.000000] OF: reserved mem: initialized node linux-cma-buffers@980000000, compatible id shared-dma-pool
[ 0.000000] OF: reserved mem: 0x0000000980000000..0x00000009b7ffffff (917504 KiB) map reusable linux-cma-buffers@980000000
[ 0.000000] Zone ranges:
[ 0.000000] DMA [mem 0x0000000080000000-0x00000000ffffffff]
[ 0.000000] DMA32 empty
[ 0.000000] Normal [mem 0x0000000100000000-0x0000000bffffffff]
[ 0.000000] Movable zone start for each node
[ 0.000000] Early memory node ranges
[ 0.000000] node 0: [mem 0x0000000080000000-0x000000009e7fffff]
[ 0.000000] node 0: [mem 0x000000009e800000-0x00000000bbffffff]
[ 0.000000] node 0: [mem 0x00000000bc000000-0x00000000ffffffff]
[ 0.000000] node 0: [mem 0x0000000880000000-0x00000008abffffff]
[ 0.000000] node 0: [mem 0x00000008ac000000-0x0000000bffffffff]
[ 0.000000] Initmem setup node 0 [mem 0x0000000080000000-0x0000000bffffffff]
[ 0.000000] psci: probing for conduit method from DT.
[ 0.000000] psci: PSCIv1.1 detected in firmware.
[ 0.000000] psci: Using standard PSCI v0.2 function IDs
[ 0.000000] psci: Trusted OS migration not required
[ 0.000000] psci: SMC Calling Convention v1.5
[ 0.000000] percpu: Embedded 20 pages/cpu s43176 r8192 d30552 u81920
[ 0.000000] Detected PIPT I-cache on CPU0
[ 0.000000] CPU features: detected: GIC system register CPU interface
[ 0.000000] CPU features: detected: Spectre-v3a
[ 0.000000] CPU features: detected: Spectre-BHB
[ 0.000000] CPU features: detected: ARM erratum 1742098
[ 0.000000] CPU features: detected: ARM errata 1165522, 1319367, or 1530923
[ 0.000000] alternatives: applying boot alternatives
[ 0.000000] Kernel command line: console=ttyS2,115200n8 earlycon=ns16550a,mmio32,0x02880000 mtdparts=47040000.spi.0:512k(ospi.tiboot3),2m(ospi.tispl),4m(ospi.u-boot),256k(ospi.env),256k(ospi.env.backup),57088k@8m(ospi.rootfs),256k(ospi.phypattern);spi-nand0:512k(ospi_nand.tiboot3),2m(ospi_nand.tispl),4m(ospi_nand.u-boot),256k(ospi_nand.env),256k(ospi_nand.env.backup),98048k@32m(ospi_nand.rootfs),256k@130816k(ospi_nand.phypattern) root=PARTUUID=84abfbf3-02 rw rootfstype=ext4 rootwait
[ 0.000000] Dentry cache hash table entries: 2097152 (order: 12, 16777216 bytes, linear)
[ 0.000000] Inode-cache hash table entries: 1048576 (order: 11, 8388608 bytes, linear)
[ 0.000000] Built 1 zonelists, mobility grouping on. Total pages: 4128768
[ 0.000000] mem auto-init: stack:all(zero), heap alloc:off, heap free:off
[ 0.000000] software IO TLB: area num 2.
[ 0.000000] software IO TLB: mapped [mem 0x00000000fbfff000-0x00000000fffff000] (64MB)
[ 0.000000] Memory: 13725772K/16777216K available (12480K kernel code, 1272K rwdata, 4184K rodata, 2496K init, 528K bss, 2133940K reserved, 917504K cma-reserved)
[ 0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=2, Nodes=1
[ 0.000000] rcu: Preemptible hierarchical RCU implementation.
[ 0.000000] rcu: RCU event tracing is enabled.
[ 0.000000] rcu: RCU restricting CPUs from NR_CPUS=256 to nr_cpu_ids=2.
[ 0.000000] Trampoline variant of Tasks RCU enabled.
[ 0.000000] Tracing variant of Tasks RCU enabled.
[ 0.000000] rcu: RCU calculated value of scheduler-enlistment delay is 25 jiffies.
[ 0.000000] rcu: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=2
[ 0.000000] NR_IRQS: 64, nr_irqs: 64, preallocated irqs: 0
[ 0.000000] GICv3: GIC: Using split EOI/Deactivate mode
[ 0.000000] GICv3: 960 SPIs implemented
[ 0.000000] GICv3: 0 Extended SPIs implemented
[ 0.000000] Root IRQ handler: gic_handle_irq
[ 0.000000] GICv3: GICv3 features: 16 PPIs
[ 0.000000] GICv3: CPU0: found redistributor 0 region 0:0x0000000001900000
[ 0.000000] ITS [mem 0x01820000-0x0182ffff]
[ 0.000000] GIC: enabling workaround for ITS: Socionext Synquacer pre-ITS
[ 0.000000] ITS@0x0000000001820000: Devices Table too large, reduce ids 20->19
[ 0.000000] ITS@0x0000000001820000: allocated 524288 Devices @8ac800000 (flat, esz 8, psz 64K, shr 0)
[ 0.000000] ITS: using cache flushing for cmd queue
[ 0.000000] GICv3: using LPI property table @0x00000008ac040000
[ 0.000000] GIC: using cache flushing for LPI property table
[ 0.000000] GICv3: CPU0: using allocated LPI pending table @0x00000008ac050000
[ 0.000000] rcu: srcu_init: Setting srcu_struct sizes based on contention.
[ 0.000000] arch_timer: cp15 timer(s) running at 200.00MHz (phys).
[ 0.000000] clocksource: arch_sys_counter: mask: 0x3ffffffffffffff max_cycles: 0x2e2049d3e8, max_idle_ns: 440795210634 ns
[ 0.000000] sched_clock: 58 bits at 200MHz, resolution 5ns, wraps every 4398046511102ns
[ 0.008439] Console: colour dummy device 80x25
[ 0.013012] Calibrating delay loop (skipped), value calculated using timer frequency.. 400.00 BogoMIPS (lpj=800000)
[ 0.023684] pid_max: default: 32768 minimum: 301
[ 0.028442] LSM: initializing lsm=capability,selinux,integrity
[ 0.034418] SELinux: Initializing.
[ 0.038074] Mount-cache hash table entries: 32768 (order: 6, 262144 bytes, linear)
[ 0.045851] Mountpoint-cache hash table entries: 32768 (order: 6, 262144 bytes, linear)
[ 0.055015] RCU Tasks: Setting shift to 1 and lim to 1 rcu_task_cb_adjust=1.
[ 0.062284] RCU Tasks Trace: Setting shift to 1 and lim to 1 rcu_task_cb_adjust=1.
[ 0.070142] rcu: Hierarchical SRCU implementation.
[ 0.075041] rcu: Max phase no-delay instances is 1000.
[ 0.080569] Platform MSI: msi-controller@1820000 domain created
[ 0.086805] PCI/MSI: /bus@100000/interrupt-controller@1800000/msi-controller@1820000 domain created
[ 0.096265] EFI services will not be available.
[ 0.101027] smp: Bringing up secondary CPUs ...
I/TC: Secondary CPU 1 initializing
I/TC: Secondary CPU 1 switching to normal world boot
[ 0.114125] Detected PIPT I-cache on CPU1
[ 0.114176] GICv3: CPU1: found redistributor 1 region 0:0x0000000001920000
[ 0.114190] GICv3: CPU1: using allocated LPI pending table @0x00000008ac060000
[ 0.114224] CPU1: Booted secondary processor 0x0000000001 [0x411fd080]
[ 0.114287] smp: Brought up 1 node, 2 CPUs
[ 0.143638] SMP: Total of 2 processors activated.
[ 0.148442] CPU features: detected: 32-bit EL0 Support
[ 0.153697] CPU features: detected: CRC32 instructions
[ 0.158977] CPU: All CPU(s) started at EL2
[ 0.163160] alternatives: applying system-wide alternatives
[ 0.169808] devtmpfs: initialized
[ 0.181990] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 7645041785100000 ns
[ 0.191971] futex hash table entries: 512 (order: 3, 32768 bytes, linear)
[ 0.209640] pinctrl core: initialized pinctrl subsystem
[ 0.215317] DMI not present or invalid.
[ 0.219682] NET: Registered PF_NETLINK/PF_ROUTE protocol family
[ 0.226416] DMA: preallocated 2048 KiB GFP_KERNEL pool for atomic allocations
[ 0.234068] DMA: preallocated 2048 KiB GFP_KERNEL|GFP_DMA pool for atomic allocations
[ 0.242407] DMA: preallocated 2048 KiB GFP_KERNEL|GFP_DMA32 pool for atomic allocations
[ 0.250624] audit: initializing netlink subsys (disabled)
[ 0.256248] audit: type=2000 audit(0.164:1): state=initialized audit_enabled=0 res=1
[ 0.256477] thermal_sys: Registered thermal governor 'step_wise'
[ 0.264172] thermal_sys: Registered thermal governor 'power_allocator'
[ 0.270334] cpuidle: using governor menu
[ 0.281095] hw-breakpoint: found 6 breakpoint and 4 watchpoint registers.
[ 0.288063] ASID allocator initialised with 65536 entries
[ 0.303324] platform a000000.dp-bridge: Fixed dependency cycle(s) with /bus@100000/dss@4a00000
[ 0.312291] platform 4800000.dsi: Fixed dependency cycle(s) with /bus@100000/dss@4a00000
[ 0.320594] platform 4800000.dsi: Fixed dependency cycle(s) with /bus@100000/i2c@2040000/dsi-edp-bridge@2c
[ 0.330552] platform a40000.pinctrl: Fixed dependency cycle(s) with /bus@100000/pinctrl@a40000/mcu-cpsw-cpts
[ 0.340813] platform 4800000.dsi: Fixed dependency cycle(s) with /bus@100000/dss@4a00000
[ 0.349121] platform a000000.dp-bridge: Fixed dependency cycle(s) with /bus@100000/dss@4a00000
[ 0.357957] platform 4a00000.dss: Fixed dependency cycle(s) with /bus@100000/dsi@4800000
[ 0.366251] platform 4a00000.dss: Fixed dependency cycle(s) with /bus@100000/dp-bridge@a000000
[ 0.376883] platform a000000.dp-bridge: Fixed dependency cycle(s) with /dp0-connector
[ 0.384941] platform dp0-connector: Fixed dependency cycle(s) with /bus@100000/dp-bridge@a000000
[ 0.394239] Modules: 27488 pages in range for non-PLT usage
[ 0.394243] Modules: 519008 pages in range for PLT usage
[ 0.400452] HugeTLB: registered 1.00 GiB page size, pre-allocated 0 pages
[ 0.412817] HugeTLB: 0 KiB vmemmap can be freed for a 1.00 GiB page
[ 0.419218] HugeTLB: registered 32.0 MiB page size, pre-allocated 0 pages
[ 0.426153] HugeTLB: 0 KiB vmemmap can be freed for a 32.0 MiB page
[ 0.432554] HugeTLB: registered 2.00 MiB page size, pre-allocated 0 pages
[ 0.439487] HugeTLB: 0 KiB vmemmap can be freed for a 2.00 MiB page
[ 0.445888] HugeTLB: registered 64.0 KiB page size, pre-allocated 0 pages
[ 0.452822] HugeTLB: 0 KiB vmemmap can be freed for a 64.0 KiB page
[ 0.460065] k3-chipinfo 43000014.chipid: Family:J721S2 rev:SR1.0 JTAGID[0x0bb7502f] Detected
[ 0.469248] iommu: Default domain type: Translated
[ 0.474167] iommu: DMA domain TLB invalidation policy: strict mode
[ 0.480631] SCSI subsystem initialized
[ 0.484661] usbcore: registered new interface driver usbfs
[ 0.490284] usbcore: registered new interface driver hub
[ 0.495730] usbcore: registered new device driver usb
[ 0.501194] pps_core: LinuxPPS API ver. 1 registered
[ 0.506269] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
[ 0.515608] PTP clock support registered
[ 0.519728] EDAC MC: Ver: 3.0.0
[ 0.523220] scmi_core: SCMI protocol bus registered
[ 0.528377] FPGA manager framework
[ 0.531894] Advanced Linux Sound Architecture Driver Initialized.
[ 0.538591] vgaarb: loaded
[ 0.541536] clocksource: Switched to clocksource arch_sys_counter
[ 0.547919] VFS: Disk quotas dquot_6.6.0
[ 0.551953] VFS: Dquot-cache hash table entries: 512 (order 0, 4096 bytes)
[ 0.562581] Carveout Heap: Exported 512 MiB at 0x0000000900000000
[ 0.568881] NET: Registered PF_INET protocol family
[ 0.574203] IP idents hash table entries: 262144 (order: 9, 2097152 bytes, linear)
[ 0.587149] tcp_listen_portaddr_hash hash table entries: 8192 (order: 5, 131072 bytes, linear)
[ 0.596059] Table-perturb hash table entries: 65536 (order: 6, 262144 bytes, linear)
[ 0.603996] TCP established hash table entries: 131072 (order: 8, 1048576 bytes, linear)
[ 0.612677] TCP bind hash table entries: 65536 (order: 9, 2097152 bytes, linear)
[ 0.621287] TCP: Hash tables configured (established 131072 bind 65536)
[ 0.628181] UDP hash table entries: 8192 (order: 6, 262144 bytes, linear)
[ 0.635322] UDP-Lite hash table entries: 8192 (order: 6, 262144 bytes, linear)
[ 0.642987] NET: Registered PF_UNIX/PF_LOCAL protocol family
[ 0.649134] RPC: Registered named UNIX socket transport module.
[ 0.655198] RPC: Registered udp transport module.
[ 0.660001] RPC: Registered tcp transport module.
[ 0.664804] RPC: Registered tcp-with-tls transport module.
[ 0.670405] RPC: Registered tcp NFSv4.1 backchannel transport module.
[ 0.676989] NET: Registered PF_XDP protocol family
[ 0.681894] PCI: CLS 0 bytes, default 64
[ 0.686634] Initialise system trusted keyrings
[ 0.691327] workingset: timestamp_bits=46 max_order=22 bucket_order=0
[ 0.698107] squashfs: version 4.0 (2009/01/31) Phillip Lougher
[ 0.704233] NFS: Registering the id_resolver key type
[ 0.709420] Key type id_resolver registered
[ 0.713695] Key type id_legacy registered
[ 0.717800] nfs4filelayout_init: NFSv4 File Layout Driver Registering...
[ 0.724649] nfs4flexfilelayout_init: NFSv4 Flexfile Layout Driver Registering...
[ 0.745967] Key type asymmetric registered
[ 0.750160] Asymmetric key parser 'x509' registered
[ 0.755178] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 244)
[ 0.762832] io scheduler mq-deadline registered
[ 0.767466] io scheduler kyber registered
[ 0.771583] io scheduler bfq registered
[ 0.777525] pinctrl-single 4301c000.pinctrl: 13 pins, size 52
[ 0.783537] pinctrl-single 4301c038.pinctrl: 11 pins, size 44
[ 0.789548] pinctrl-single 4301c068.pinctrl: 72 pins, size 288
[ 0.795857] pinctrl-single 4301c190.pinctrl: 1 pins, size 4
[ 0.801691] pinctrl-single 11c000.pinctrl: 72 pins, size 288
[ 0.807824] pinctrl-single 104200.pinctrl: 20 pins, size 80
[ 0.813591] pinctrl-single 104280.pinctrl: 8 pins, size 32
[ 0.819591] pinctrl-single a40000.pinctrl: 512 pins, size 2048
[ 0.829620] Serial: 8250/16550 driver, 12 ports, IRQ sharing enabled
[ 0.841764] loop: module loaded
[ 0.845654] megasas: 07.725.01.00-rc1
[ 0.851381] tun: Universal TUN/TAP device driver, 1.6
[ 0.857189] VFIO - User Level meta-driver version: 0.3
[ 0.863131] usbcore: registered new interface driver usb-storage
[ 0.869664] i2c_dev: i2c /dev entries driver
[ 0.874743] sdhci: Secure Digital Host Controller Interface driver
[ 0.881074] sdhci: Copyright(c) Pierre Ossman
[ 0.885665] sdhci-pltfm: SDHCI platform and OF driver helper
[ 0.891805] ledtrig-cpu: registered to indicate activity on CPUs
[ 0.898133] SMCCC: SOC_ID: ARCH_SOC_ID not implemented, skipping ....
[ 0.905139] usbcore: registered new interface driver usbhid
[ 0.910837] usbhid: USB HID core driver
[ 0.915527] hw perfevents: enabled with armv8_cortex_a72 PMU driver, 7 counters available
[ 0.924266] optee: probing for conduit method.
I/TC: Reserved shared memory is enabled
I/TC: Dynamic shared memory is enabled
I/TC: Normal World virtualization support is disabled
I/TC: Asynchronous notifications are disabled
[ 0.928826] optee: revision 4.4 (8f645256efc0dc66)
[ 0.945283] optee: dynamic shared memory is enabled
[ 0.955620] random: crng init done
[ 0.959158] optee: initialized driver
[ 0.964396] Initializing XFRM netlink socket
[ 0.968793] NET: Registered PF_PACKET protocol family
[ 0.974001] Key type dns_resolver registered
[ 0.982164] registered taskstats version 1
[ 0.986421] Loading compiled-in X.509 certificates
[ 0.998612] ti-sci 44083000.system-controller: ABI: 4.0 (firmware rev 0x000a '10.1.6--v10.01.06 (Fiery Fox)')
[ 1.068605] omap_i2c 42120000.i2c: bus 0 rev0.12 at 400 kHz
[ 1.075623] platform 4800000.dsi: Fixed dependency cycle(s) with /bus@100000/i2c@2040000/dsi-edp-bridge@2c
[ 1.085555] i2c 1-002c: Fixed dependency cycle(s) with /bus@100000/i2c@2040000/dsi-edp-bridge@2c/aux-bus/panel
[ 1.095804] i2c 1-002c: Fixed dependency cycle(s) with /bus@100000/dsi@4800000
[ 1.103465] pca953x 1-0020: supply vcc not found, using dummy regulator
[ 1.110294] pca953x 1-0020: using no AI
[ 1.137588] pca953x 1-0020: failed writing register
[ 1.142635] pca953x: probe of 1-0020 failed with error -121
[ 1.148402] omap_i2c 2040000.i2c: bus 1 rev0.12 at 400 kHz
[ 1.154311] ti-sci-intr 42200000.interrupt-controller: Interrupt Router 125 domain created
[ 1.162858] ti-sci-intr bus@100000:interrupt-controller@a00000: Interrupt Router 148 domain created
[ 1.172204] ti-sci-intr 310e0000.interrupt-controller: Interrupt Router 227 domain created
[ 1.180823] ti-sci-inta 33d00000.msi-controller: Interrupt Aggregator domain 265 created
[ 1.191091] ------------[ cut here ]------------
[ 1.195816] wiz bus@100000:wiz@5060000: Unable to create SERDES platform device
[ 1.203309] WARNING: CPU: 1 PID: 11 at drivers/phy/ti/phy-j721e-wiz.c:1624 wiz_probe+0xd10/0xe6c
[ 1.212301] Modules linked in:
[ 1.215417] CPU: 1 PID: 11 Comm: kworker/u4:0 Not tainted 6.6.44-ti-g541c20281af7-dirty #1
[ 1.223861] Hardware name: Texas Instruments J721S2 EVM (DT)
[ 1.229640] Workqueue: events_unbound deferred_probe_work_func
[ 1.235606] pstate: 60000005 (nZCv daif -PAN -UAO -TCO -DIT -SSBS BTYPE=--)
[ 1.242718] pc : wiz_probe+0xd10/0xe6c
[ 1.246543] lr : wiz_probe+0xd10/0xe6c
[ 1.250367] sp : ffff80008163ba80
[ 1.253746] x29: ffff80008163bb40 x28: ffff000b7e206218 x27: 0000000000000003
[ 1.261039] x26: ffff800080cb8130 x25: 0000000000000004 x24: 0000000000000004
[ 1.268331] x23: 0000000000000000 x22: ffff00082cd010c8 x21: ffff00082c1cc010
[ 1.275623] x20: ffff00082cd01080 x19: 0000000000000000 x18: 0000000000000006
[ 1.282915] x17: 766564206d726f66 x16: 74616c7020534544 x15: 5245532065746165
[ 1.290207] x14: 7263206f7420656c x13: ffff8000812ef178 x12: 0000000000000378
[ 1.297498] x11: 0000000000000128 x10: ffff800081347178 x9 : ffff8000812ef178
[ 1.304790] x8 : 00000000ffffefff x7 : ffff800081347178 x6 : 80000000fffff000
[ 1.312081] x5 : 0000000000000000 x4 : 0000000000000000 x3 : 0000000000000000
[ 1.319373] x2 : 0000000000000000 x1 : 0000000000000000 x0 : ffff00082c151c80
[ 1.326665] Call trace:
[ 1.329155] wiz_probe+0xd10/0xe6c
[ 1.332625] platform_probe+0x68/0xc4
[ 1.336360] really_probe+0x148/0x2b0
[ 1.340097] __driver_probe_device+0x78/0x12c
[ 1.344545] driver_probe_device+0xd8/0x15c
[ 1.348814] __device_attach_driver+0xb8/0x134
[ 1.353350] bus_for_each_drv+0x88/0xe8
[ 1.357264] __device_attach+0xa0/0x190
[ 1.361178] device_initial_probe+0x14/0x20
[ 1.365448] bus_probe_device+0xac/0xb0
[ 1.369362] deferred_probe_work_func+0x88/0xc0
[ 1.373986] process_one_work+0x138/0x248
[ 1.378081] worker_thread+0x320/0x438
[ 1.381906] kthread+0x110/0x114
[ 1.385200] ret_from_fork+0x10/0x20
[ 1.388849] ---[ end trace 0000000000000000 ]---
[ 1.393688] wiz: probe of bus@100000:wiz@5060000 failed with error -12
[ 1.401605] ti-udma 311a0000.dma-controller: Number of rings: 48
[ 1.408598] ti-udma 311a0000.dma-controller: Channels: 24 (bchan: 0, tchan: 8, rchan: 16)
[ 1.418107] k3-ringacc 2b800000.ringacc: Ring Accelerator probed rings:286, gp-rings[96,20] sci-dev-id:272
[ 1.428005] k3-ringacc 2b800000.ringacc: dma-ring-reset-quirk: disabled
[ 1.434766] k3-ringacc 2b800000.ringacc: RA Proxy rev. 66349100, num_proxies:64
[ 1.444268] k3-ringacc 3c000000.ringacc: Ring Accelerator probed rings:1024, gp-rings[878,128] sci-dev-id:259
[ 1.454438] k3-ringacc 3c000000.ringacc: dma-ring-reset-quirk: disabled
[ 1.461199] k3-ringacc 3c000000.ringacc: RA Proxy rev. 66349100, num_proxies:64
[ 1.469403] 40a00000.serial: ttyS1 at MMIO 0x40a00000 (irq = 229, base_baud = 6000000) is a 8250
[ 1.479158] 2880000.serial: ttyS2 at MMIO 0x2880000 (irq = 230, base_baud = 3000000) is a 8250
[ 1.488085] printk: console [ttyS2] enabled
[ 1.488085] printk: console [ttyS2] enabled
[ 1.496543] printk: bootconsole [ns16550a0] disabled
[ 1.496543] printk: bootconsole [ns16550a0] disabled
[ 1.510210] davinci_mdio 46000f00.mdio: Configuring MDIO in manual mode
[ 1.553539] davinci_mdio 46000f00.mdio: davinci mdio revision 9.7, bus freq 1000000
[ 1.578145] davinci_mdio 46000f00.mdio: phy[0]: device 46000f00.mdio:00, driver unknown
[ 1.586157] am65-cpsw-nuss 46000000.ethernet: initializing am65 cpsw nuss version 0x6BA02102, cpsw version 0x6BA82102 Ports: 2 quirks:00000000
[ 1.599046] am65-cpsw-nuss 46000000.ethernet: initialized cpsw ale version 1.4
[ 1.606257] am65-cpsw-nuss 46000000.ethernet: ALE Table size 64
[ 1.612547] pps pps0: new PPS source ptp0
[ 1.616724] am65-cpsw-nuss 46000000.ethernet: CPTS ver 0x4e8a010b, freq:500000000, add_val:1 pps:1
[ 1.627410] am65-cpts 310d0000.cpts: CPTS ver 0x4e8a010c, freq:200000000, add_val:4 pps:0
[ 1.636311] mmc0: CQHCI version 5.10
[ 1.680158] mmc0: SDHCI controller on 4f80000.mmc [4f80000.mmc] using ADMA 64-bit
[ 1.863265] mmc0: Failed to initialize a non-removable card
[ 1.906206] tps6594-rtc tps6594-rtc.4.auto: registered as rtc0
[ 1.917729] tps6594-rtc tps6594-rtc.4.auto: hctosys: unable to read the hardware clock
[ 2.305718] ti-udma 285c0000.dma-controller: Channels: 26 (tchan: 13, rchan: 13, gp-rflow: 8)
[ 2.316161] ti-udma 31150000.dma-controller: Channels: 60 (tchan: 30, rchan: 30, gp-rflow: 16)
[ 2.326587] davinci_mdio 46000f00.mdio: Configuring MDIO in manual mode
[ 2.369553] davinci_mdio 46000f00.mdio: davinci mdio revision 9.7, bus freq 1000000
[ 2.394108] davinci_mdio 46000f00.mdio: phy[0]: device 46000f00.mdio:00, driver unknown
[ 2.402133] am65-cpsw-nuss 46000000.ethernet: initializing am65 cpsw nuss version 0x6BA02102, cpsw version 0x6BA82102 Ports: 2 quirks:00000000
[ 2.415029] am65-cpsw-nuss 46000000.ethernet: initialized cpsw ale version 1.4
[ 2.422245] am65-cpsw-nuss 46000000.ethernet: ALE Table size 64
[ 2.428482] pps pps0: new PPS source ptp1
[ 2.432665] am65-cpsw-nuss 46000000.ethernet: CPTS ver 0x4e8a010b, freq:500000000, add_val:1 pps:1
[ 2.447691] am65-cpsw-nuss 46000000.ethernet: set new flow-id-base 48
[ 2.458041] mmc1: CQHCI version 5.10
[ 2.461321] clk: Disabling unused clocks
[ 2.473978] ALSA device list:
[ 2.476942] No soundcards found.
[ 2.500121] mmc1: SDHCI controller on 4fb0000.mmc [4fb0000.mmc] using ADMA 64-bit
[ 2.507766] Waiting for root device PARTUUID=84abfbf3-02...
[ 2.583831] mmc1: new ultra high speed SDR104 SDXC card at address aaaa
[ 2.590858] mmcblk1: mmc1:aaaa SD64G 59.5 GiB
[ 2.601898] mmcblk1: p1 p2
[ 2.876005] EXT4-fs (mmcblk1p2): recovery complete
[ 2.881789] EXT4-fs (mmcblk1p2): mounted filesystem 8861bdbd-06e1-4780-a1d9-3f9f378fc842 r/w with ordered data mode. Quota mode: none.
[ 2.893905] VFS: Mounted root (ext4 filesystem) on device 179:2.
[ 2.906247] devtmpfs: mounted
[ 2.910157] Freeing unused kernel memory: 2496K
[ 2.914794] Run /sbin/init as init process
[ 3.081857] systemd[1]: System time before build time, advancing clock.
[ 3.116661] systemd[1]: systemd 255.13^ running in system mode (+PAM -AUDIT -SELINUX -APPARMOR +IMA -SMACK +SECCOMP -GCRYPT -GNUTLS -OPENSSL +ACL +BLKID -CURL -ELFUTILS -FIDO2 -IDN2 -IDN -IPTC +KMOD -LIBCRYPTSETUP +LIBFDISK -PCRE2 -PWQUALITY -P11KIT -QRENCODE -TPM2 -BZIP2 -LZ4 -XZ -ZLIB +ZSTD -BPF_FRAMEWORK -XKBCOMMON +UTMP +SYSVINIT default-hierarchy=unified)
[ 3.148570] systemd[1]: Detected architecture arm64.
Welcome to Arago 2023.10!
[ 3.170185] systemd[1]: Hostname set to <am68-sk>.
[ 3.267777] systemd-sysv-generator[90]: SysV service '/etc/init.d/edgeai-launcher.sh' lacks a native systemd unit file. ~ Automatically generating a unit file for compatibility. Please update package to include a native systemd unit file, in order to make it safe, robust and future-proof. ! This compatibility logic is deprecated, expect removal soon. !
[ 3.395594] systemd[1]: Binding to IPv6 address not available since kernel does not support IPv6.
[ 3.404510] systemd[1]: Binding to IPv6 address not available since kernel does not support IPv6.
[ 3.435733] systemd[1]: /usr/lib/systemd/system/bt-enable.service:9: Standard output type syslog is obsolete, automatically updating to journal. Please update your unit file, and consider removing the setting altogether.
[ 3.504803] systemd[1]: /etc/systemd/system/sync-clocks.service:11: Standard output type syslog is obsolete, automatically updating to journal. Please update your unit file, and consider removing the setting altogether.
[ 3.562361] systemd[1]: Queued start job for default target Graphical Interface.
[ 3.605000] systemd[1]: Created slice Slice /system/getty.
[ OK ] Created slice Slice /system/getty.
[ 3.627007] systemd[1]: Created slice Slice /system/modprobe.
[ OK ] Created slice Slice /system/modprobe.
[ 3.650869] systemd[1]: Created slice Slice /system/serial-getty.
[ OK ] Created slice Slice /system/serial-getty.
[ 3.674546] systemd[1]: Created slice User and Session Slice.
[ OK ] Created slice User and Session Slice.
[ 3.697813] systemd[1]: Started Dispatch Password Requests to Console Directory Watch.
[ OK ] Started Dispatch Password Requests to Console Directory Watch.
[ 3.721725] systemd[1]: Started Forward Password Requests to Wall Directory Watch.
[ OK ] Started Forward Password Requests to Wall Directory Watch.
[ 3.745634] systemd[1]: Expecting device /dev/ttyS2...
Expecting device /dev/ttyS2...
[ 3.765656] systemd[1]: Reached target Path Units.
[ OK ] Reached target Path Units.
[ 3.785596] systemd[1]: Reached target Remote File Systems.
[ OK ] Reached target Remote File Systems.
[ 3.805598] systemd[1]: Reached target Slice Units.
[ OK ] Reached target Slice Units.
[ 3.825603] systemd[1]: Reached target Swaps.
[ OK ] Reached target Swaps.
[ 3.872770] systemd[1]: Listening on RPCbind Server Activation Socket.
[ OK ] Listening on RPCbind Server Activation Socket.
[ 3.897719] systemd[1]: Reached target RPC Port Mapper.
[ OK ] Reached target RPC Port Mapper.
[ 3.926563] systemd[1]: Listening on Process Core Dump Socket.
[ OK ] Listening on Process Core Dump Socket.
[ 3.949849] systemd[1]: Listening on initctl Compatibility Named Pipe.
[ OK ] Listening on initctl Compatibility Named Pipe.
[ 3.974273] systemd[1]: Listening on Journal Audit Socket.
[ OK ] Listening on Journal Audit Socket.
[ 3.998018] systemd[1]: Listening on Journal Socket (/dev/log).
[ OK ] Listening on Journal Socket (/dev/log).
[ 4.021995] systemd[1]: Listening on Journal Socket.
[ OK ] Listening on Journal Socket.
[ 4.042100] systemd[1]: Listening on Network Service Netlink Socket.
[ OK ] Listening on Network Service Netlink Socket.
[ 4.072010] systemd[1]: Listening on udev Control Socket.
[ OK ] Listening on udev Control Socket.
[ 4.093947] systemd[1]: Listening on udev Kernel Socket.
[ OK ] Listening on udev Kernel Socket.
[ 4.113928] systemd[1]: Listening on User Database Manager Socket.
[ OK ] Listening on User Database Manager Socket.
[ 4.161801] systemd[1]: Mounting Huge Pages File System...
Mounting Huge Pages File System...
[ 4.184235] systemd[1]: Mounting POSIX Message Queue File System...
Mounting POSIX Message Queue File System...
[ 4.211105] systemd[1]: Mounting Kernel Debug File System...
Mounting Kernel Debug File System...
[ 4.233958] systemd[1]: Kernel Trace File System was skipped because of an unmet condition check (ConditionPathExists=/sys/kernel/tracing).
[ 4.255321] systemd[1]: Mounting Temporary Directory /tmp...
Mounting Temporary Directory /tmp...
[ 4.269984] systemd[1]: Create List of Static Device Nodes was skipped because of an unmet condition check (ConditionFileNotEmpty=/lib/modules/6.6.44-ti-g541c20281af7-dirty/modules.devname).
[ 4.309835] systemd[1]: Starting Load Kernel Module configfs...
Starting Load Kernel Module configfs...
[ 4.334224] systemd[1]: Starting Load Kernel Module drm...
Starting Load Kernel Module drm...
[ 4.354258] systemd[1]: Starting Load Kernel Module fuse...
Starting Load Kernel Module fuse...
[ 4.394199] systemd[1]: Starting Start psplash boot splash screen...
Starting Start psplash boot splash screen...
[ 4.427502] systemd[1]: Starting RPC Bind...
Starting RPC Bind...
[ 4.437512] systemd[1]: File System Check on Root Device was skipped because of an unmet condition check (ConditionPathIsReadWrite=!/).
[ 4.454736] systemd[1]: Starting Journal Service...
Starting Journal Service...
[ 4.490994] systemd[1]: Starting Load Kernel Modules...
Starting Load Kernel Modules...
[ 4.515150] systemd[1]: Starting Generate network units from Kernel command line...
Starting Generate network units from Kernel command line...
[ 4.546437] systemd-journald[104]: Collecting audit messages is enabled.
[ 4.558102] systemd[1]: Starting Remount Root and Kernel File Systems...
Starting Remount Root and Kernel File Systems...
[ 4.606093] EXT4-fs (mmcblk1p2): re-mounted 8861bdbd-06e1-4780-a1d9-3f9f378fc842 r/w. Quota mode: none.
[ 4.606373] systemd[1]: Starting Create Static Device Nodes in /dev gracefully...
Starting Create Static Device Nodes in /dev gracefully...
[ 4.662385] systemd[1]: Starting Coldplug All udev Devices...
Starting Coldplug All udev Devices...
[ 4.680554] systemd[1]: Started RPC Bind.
[ OK ] Started RPC Bind.
[ 4.694055] systemd[1]: Started Journal Service.
[ OK ] Started Journal Service.
[ OK ] Mounted Huge Pages File System.
[ OK ] Mounted POSIX Message Queue File System.
[ OK ] Mounted Kernel Debug File System.
[ OK ] Mounted Temporary Directory /tmp.
[ OK ] Finished Load Kernel Module configfs.
[ OK ] Finished Load Kernel Module drm.
[ OK ] Finished Load Kernel Module fuse.
[FAILED] Failed to start Start psplash boot splash screen.
See 'systemctl status psplash-start.service' for details.
[DEPEND] Dependency failed for Start psplas…temd progress communication helper.
[ OK ] Finished Load Kernel Modules.
[ OK ] Finished Generate network units from Kernel command line.
[ OK ] Finished Remount Root and Kernel File Systems.
[ OK ] Finished Create Static Device Nodes in /dev gracefully.
Mounting Kernel Configuration File System...
Starting Flush Journal to Persistent Storage...
Starting Apply Kernel Variables...
Starting Create Static Device Nodes in /dev 5.067826] systemd-journald[104]: Received client request to flush runtime journal.
m...
[ OK ] Mounted Kernel Configuration File System.
[ OK ] Finished Flush Journal to Persistent Storage.
[ OK ] Finished Apply Kernel Variables.
[ OK ] Finished Create Static Device Nodes in /dev.
[ OK ] Reached target Preparation for Local File Systems.
Mounting /var/volatile...
[ 5.203303] audit: type=1334 audit(1728487094.116:2): prog-id=6 op=LOAD
[ 5.210310] audit: type=1334 audit(1728487094.124:3): prog-id=7 op=LOAD
Starting Rule-based Manager for Device Events and Files...
[ OK ] Finished Coldplug All udev Devices.
[ OK ] Mounted /var/volatile.
Starting Load/Save OS Random Seed...
[ OK ] Reached target Local File Systems.
Starting Create System Files and Directories...
[ OK ] Finished Load/Save OS Random Seed.
[ OK ] Finished Create System Files and Directories.
[ 5.414914] audit: type=1334 audit(1728487094.328:4): prog-id=8 op=LOAD
Starting Network Name Resolution...
[ 5.456038] audit: type=1334 audit(1728487094.368:5): prog-id=9 op=LOAD
Starting Network Time Synchronization...
Starting Record System Boot/Shutdown in UTMP...
[ 5.535797] audit: type=1334 audit(1728487094.448:6): prog-id=10 op=LOAD
[ 5.543758] audit: type=1334 audit(1728487094.456:7): prog-id=11 op=LOAD
[ 5.550533] audit: type=1334 audit(1728487094.456:8): prog-id=12 op=LOAD
Starting User Database Manager...
[ OK ] Finished Record System Boot/Shutdown in UTMP.
[ OK ] Started User Database Manager.
[ OK ] Started Rule-based Manager for Device Events and Files.
[ OK ] Found device /dev/ttyS2.
[ OK ] Started Network Time Synchronization.
[ OK ] Reached target System Time Set.
[ OK ] Started Network Name Resolution.
[ OK ] Reached target Host and Network Name Lookups.
[ OK ] Reached target System Initialization.
[ OK ] Started Daily rotation of log files.
[ OK ] Started Daily Cleanup of Temporary Directories.
[ OK ] Reached target Timer Units.
[ OK ] Listening on Avahi mDNS/DNS-SD Stack Activation Socket.
[ OK ] Listening on D-Bus System Message Bus Socket.
Starting Docker Socket for the API...
[ OK ] Listening on dropbear.socket.
[ OK ] Listening on PC/SC Smart Card Daemon Activation Socket.
Starting Weston socket...
[ 6.161942] audit: type=1334 audit(1728510629.556:9): prog-id=13 op=LOAD
Starting D-Bus System Message Bus...
Starting Reboot and dump vmcore via kexec...
[ OK ] Listening on Docker Socket for the API.
[ OK ] Listening on Weston socket.
[ OK ] Finished Reboot and dump vmcore via kexec.
[ OK ] Started D-Bus System Message Bus.
[ OK ] Reached target Socket Units.
[ 6.364446] dbus-broker-lau[253]: memfd_create() called without MFD_EXEC or MFD_NOEXEC_SEAL set
[ OK ] Reached target Basic System.
[ OK ] Started Job spooling tools.
Starting Avahi mDNS/DNS-SD Stack...
[ OK ] Started Periodic Command Scheduler.
Starting Print notice about GPLv3 packages...
Starting IPv6 Packet Filtering Framework...
Starting IPv4 Packet Filtering Framework...
[ OK ] Started irqbalance daemon.
Starting Telephony service...
Starting Expand the rootfs partiti…to full size of the boot device....
[ OK ] Started strongSwan IPsec IKEv1/IKEv2 daemon using ipsec.conf.
[ 6.557029] audit: type=1334 audit(1728510629.952:10): prog-id=14 op=LOAD
[ 6.573361] audit: type=1334 audit(1728510629.952:11): prog-id=15 op=LOAD
Starting User Login Management...
[ 6.596487] audit: type=1334 audit(1728510629.952:12): prog-id=16 op=LOAD
Starting Telnet Server...
[ OK ] Finished IPv6 Packet Filtering Framework.
[ OK ] Finished IPv4 Packet Filtering Framework.
[ OK ] Started A[ 6.727450] audit: type=1334 audit(1728510630.124:13): prog-id=17 op=LOAD
vahi mDNS/DNS-SD Stack.
[ OK ] Reached target Preparation for Network.
Starting Network Configuration...
[ OK ] Finished Telnet Server.
[ OK ] Started Telephony service.
[ OK ] Finished Expand the rootfs partition to full size of the boot device..
[ OK ] Started Network Configuration.
[ OK ] Started User Login Management.
[ OK ] Reached target Network.
Starting Enable and configure wl18xx bluetooth stack...
Starting containerd container runtime...
[ 7.147723] am65-cpsw-nuss 46000000.ethernet eth0: validation of with support 00,00000000,00000000,00006000 and advertisement 00,00000000,00000000,00000000 failed: -EINVAL
Starting LLDP daemon...
[ OK ] Started Netperf Benchmark Server.
Starting Simple Network Management Protocol (SNMP) Daemon....
Starting Permit User Sessions...
[ OK ] Finished Enable and configure wl18xx bluetooth stack.
[ OK ] Finished Permit User Sessions.
[ OK ] Started Getty on tty1.
[ OK ] Started Serial Getty on ttyS2.
[ OK ] Reached target Login Prompts.
Starting Synchronize System and HW clocks...
Starting Weston, a Wayland compositor, as a system service...
[ OK ] Started LLDP daemon.
[ OK ] Finished Synchronize System and HW clocks.
[ OK ] Created slice User Slice of UID 1000.
Starting User Runtime Directory /run/user/1000...
[ OK ] Finished User Runtime Directory /run/user/1000.
[ OK ] Created slice Slice /system/tee-supplicant.
[ OK ] Started TEE Supplicant on teepriv0.
Starting User Manager for UID 1000...
Starting Virtual Console Setup...
[ OK ] Finished Virtual Console Setup.
[ OK ] Created slice Slice /system/systemd-fsck.
Expecting device /dev/mmcblk1p1...
[ OK ] Started Simple Network Management Protocol (SNMP) Daemon..
[ OK ] Started User Manager for UID 1000.
[ OK ] Started Session c1 of User weston.
[ OK ] Found device /dev/mmcblk1p1.
Starting File System Check on /dev/mmcblk1p1...
[FAILED] Failed to start Weston, a Wayland compositor, as a system service.
See 'systemctl status weston.service' for details.
Starting EdgeAI OOB demos...
[ OK ] Finished File System Check on /dev/mmcblk1p1.
Mounting /run/media/BOOT-mmcblk1p1...
[ OK ] Mounted /run/media/BOOT-mmcblk1p1.
[ OK ] Created slice Slice /system/systemd-coredump.
[ OK ] Started Process Core Dump (PID 567/UID 0).
[ OK ] Started containerd container runtime.
[ OK ] Started EdgeAI OOB demos.
[ OK ] Started Process Core Dump (PID 670/UID 0).
[ 10.685933] kauditd_printk_skb: 17 callbacks suppressed
[ 10.685940] audit: type=1334 audit(1728510634.084:27): prog-id=23 op=UNLOAD
[ 10.699021] audit: type=1334 audit(1728510634.084:28): prog-id=22 op=UNLOAD
[ 10.706977] audit: type=1334 audit(1728510634.084:29): prog-id=21 op=UNLOAD
[ 10.940755] audit: type=1701 audit(1728510634.336:30): auid=4294967295 uid=0 gid=0 ses=4294967295 subj=kernel pid=823 comm="kmsprint" exe="/usr/bin/kmsprint" sig=6 res=1
[ 10.963952] audit: type=1334 audit(1728510634.360:31): prog-id=24 op=LOAD
[ 10.972716] audit: type=1334 audit(1728510634.360:32): prog-id=25 op=LOAD
[ 10.980047] audit: type=1334 audit(1728510634.360:33): prog-id=26 op=LOAD
[ OK ] Started Process Core Dump (PID 830/UID 0).
[ 11.202052] audit: type=1334 audit(1728510634.600:34): prog-id=26 op=UNLOAD
[ 11.211709] audit: type=1334 audit(1728510634.600:35): prog-id=25 op=UNLOAD
[ 11.220278] audit: type=1334 audit(1728510634.600:36): prog-id=24 op=UNLOAD
***************************************************************
***************************************************************
NOTICE: This file system contains the following GPL-3.0 packages:
adwaita-icon-theme-symbolic
autoconf
bash-dev
bash
bc
binutils
cifs-utils
coreutils-stdbuf
coreutils
cpio
cpp-symlinks
cpp
dosfstools
elfutils-dev
elfutils
findutils
g++-symlinks
g++
gawk
gcc-symlinks
gcc
gdb
gdbserver
gettext
glmark2
gnu-config
grub-common
grub-editenv
grub-efi
gzip
hidapi
kbd-dev
kbd-keymaps-pine
less
libasm1
libatomic-dev
libatomic1
libbfd
libdebuginfod1
libdw1
libelf1
libgcc-s-dev
libgcc1
libgdbm-compat4
libgdbm-dev
libgdbm6
libgettextlib
libgettextsrc
libgmp-dev
libgmp10
libgmpxx4
libgnutls-dev
libgnutls-openssl27
libidn2-0
libidn2-dev
libmpc3
libmpfr6
libopcodes
libqt5charts-examples
libqt5charts-plugins
libqt5charts-qmlplugins
libqt5charts5
libqt5serialport-examples
libqt5serialport-plugins
libqt5serialport-qmlplugins
libqt5serialport5
libqt5svg-examples
libqt5svg-plugins
libqt5svg-qmlplugins
libqt5svg5
libqt5virtualkeyboard-plugins
libqt5virtualkeyboard-qmlplugins
libqt5virtualkeyboard5
libreadline-dev
libreadline8
libstdc++-dev
libstdc++6
libtasn1-dev
libunistring-dev
libunistring5
m4
make
nettle-dev
nettle
parted
piglit
qt3d-plugins
qt3d-qmlplugins
qt3d
qtbase-examples
qtbase-plugins
qtbase-qmlplugins
qtbase
qtconnectivity-plugins
qtconnectivity-qmlplugins
qtconnectivity
qtdeclarative-plugins
qtdeclarative-qmlplugins
qtdeclarative-tools
qtdeclarative
qtgraphicaleffects-qmlplugins
qtlocation-examples
qtlocation-plugins
qtlocation-qmlplugins
qtlocation
qtmultimedia-examples
qtmultimedia-plugins
qtmultimedia-qmlplugins
qtmultimedia
qtquick3d-plugins
qtquick3d-qmlplugins
qtquick3d
qtquics-qmlplugins.control
qtquics2-plugins.control
qtquics2-qmlplugins.control
qtquics2.control
qtscript-examples
qtscript-plugins
qtscript-qmlplugins
qtscript
qtwayland-examples
qtwayland-plugins
qtwayland-qmlplugins
qtwayland
tar
which
If you do not wish to distribute GPL-3.0 components please remove
the above packages prior to distribution. This can be done using
the opkg remove command. i.e.:
opkg remove <package>
Where <package> is the name printed in the list above
NOTE: If the package is a dependency of another package you
will be notified of the dependent packages. You should
use the --force-removal-of-dependent-packages option to
also remove the dependent packages as well
***************************************************************
***************************************************************
[ OK ] Finished Print notice about GPLv3 packages.
[ OK ] Reached target Multi-User System.
[ OK ] Reached target Graphical Interface.
Starting Record Runlevel Change in UTMP...
[ OK ] Finished Record Runlevel Change in UTMP.
[ 12.702310] platform 2030000.i2c: deferred probe pending
[ 12.707643] platform fixedregulator-dp0-prw: deferred probe pending
[ 12.713902] platform regulator-dp1-prw: deferred probe pending
_____ _____ _ _
| _ |___ ___ ___ ___ | _ |___ ___ |_|___ ___| |_
| | _| .'| . | . | | __| _| . | | | -_| _| _|
|__|__|_| |__,|_ |___| |__| |_| |___|_| |___|___|_|
|___| |___|
Arago Project am68-sk ttyS2
Arago 2023.10 am68-sk ttyS2
am68-sk login: root
[ 15.940964] audit: type=1006 audit(1728510639.336:37): pid=1189 uid=0 subj=kernel old-auid=4294967295 auid=0 tty=(none) old-ses=4294967295 ses=3 res=1
[ 15.954959] audit: type=1300 audit(1728510639.336:37): arch=c00000b7 syscall=64 success=yes exit=1 a0=8 a1=ffffe7195148 a2=1 a3=1 items=0 ppid=1 pid=1189 auid=0 uid=0 gid=0 euid=0 suid=0 fsuid=0 egid=0 sgid=0 fsgid=0 tty=(none) ses=3 comm="(systemd)" exe="/usr/lib/systemd/systemd-executor" subj=kernel key=(null)
[ 15.983008] audit: type=1327 audit(1728510639.336:37): proctitle="(systemd)"
[ 15.990262] audit: type=1334 audit(1728510639.352:38): prog-id=27 op=LOAD
[ 15.997128] audit: type=1300 audit(1728510639.352:38): arch=c00000b7 syscall=280 success=yes exit=8 a0=5 a1=ffffddc1f318 a2=90 a3=0 items=0 ppid=1 pid=1189 auid=0 uid=0 gid=0 euid=0 suid=0 fsuid=0 egid=0 sgid=0 fsgid=0 tty=(none) ses=3 comm="systemd" exe="/usr/lib/systemd/systemd" subj=kernel key=(null)
[ 16.023982] audit: type=1327 audit(1728510639.352:38): proctitle="(systemd)"
[ 16.031479] audit: type=1334 audit(1728510639.380:39): prog-id=27 op=UNLOAD
[ 16.038796] audit: type=1300 audit(1728510639.380:39): arch=c00000b7 syscall=57 success=yes exit=0 a0=8 a1=1 a2=0 a3=ffffacf55c60 items=0 ppid=1 pid=1189 auid=0 uid=0 gid=0 euid=0 suid=0 fsuid=0 egid=0 sgid=0 fsgid=0 tty=(none) ses=3 comm="systemd" exe="/usr/lib/systemd/systemd" subj=kernel key=(null)
[ 16.065837] audit: type=1327 audit(1728510639.380:39): proctitle="(systemd)"
[ 16.073165] audit: type=1334 audit(1728510639.380:40): prog-id=28 op=LOAD
terminate called after throwing an instance of 'std::runtime_error'
what(): failed to find DRM cards
root@am68-sk:/opt/edgeai-gst-apps# kmsprint
terminate called after throwing an instance of 'std::runtime_error'
what(): failed to find DRM cards
Aborted (core dumped)
root@am68-sk:/opt/edgeai-gst-apps# modetest -M tidss
failed to open device 'tidss': No such file or directory
root@am68-sk:/opt/edgeai-gst-apps#