This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

XDM_FLUSH crash

Hi,

I use RDK 01.08.00.15 to do dynamic resolution change for H.264 video stream, but the program will crash on XDM_FLUSH, even I update the decoder patch to 01.00.00.06.

Thanks.

  • Jack,

    Do you observe crash during the control call with "XDM_FLUSH" command id or in the very first process call after XDM_FLUSH control call?

    -Ramakrishna.

     

  •  [m3video]  67900: DECODE: CH0: Decoder flush needed (error = 1048833)!!!
    [m3video] 67900: DECODE: CH0: Decoder Flushing !!!
    [m3vpss ] SWMS: *** UPDATING RT Params ***
    [m3vpss ] 68883: SWMS : ******* Configuring clock 30 secs...
    [m3vpss ]
    [m3vpss ] *** [SWMS0] Mosaic Parameters ***
    [m3vpss ]
    [m3vpss ] Win | Ch | Input | Input | Input | Input | Output | Output | Output | Output | Low Cost | SWMS | Data |
    [m3vpss ] Num | Num | Start X, Y | Width x Height | Pitch Y / C | Memory Type | Start X, Y | Width x Height | Pitch Y / C | Memory Type | ON / OFF | Inst | Format|
    [m3vpss ]
  • Dear Jack

    This information is not providing much things to analyze. Can you please see if there is way to get more details by increasing/configuring the debug trace level. Some how it doesn't look like codec issue.

    -Ramakrishna.