Tool/software:
Hi TI Experts,
We followed the official instructions to build SDK with Yocto (SDK Linux for J721s2 r10.1)
The purpose is to generate the roots "tisdk-adas-image-j721s2-evm.tar.xz" which is used in SDK RTOS.
git clone https://git.ti.com/git/arago-project/oe-layersetup.git yocto-build cd yocto-build ./oe-layertool-setup.sh -f configs/processor-sdk-analytics/processor-sdk-analytics-10.01.00-config.txt cd build . conf/setenv echo 'ARAGO_BRAND = "adas"' >> conf/local.conf TOOLCHAIN_BASE=/opt/tda4 MACHINE="j721s2-evm" bitbake -k tisdk-adas-image
But encountered the following error during the build process:
Parsing of 7036 .bb files complete (0 cached, 7036 parsed). 11095 targets, 1643 skipped, 0 masked, 0 errors.
ERROR: Nothing PROVIDES 'tisdk-adas-image'. Close matches:
tisdk-base-image
tisdk-default-image
tisdk-edgeai-image
$ MACHINE="j721s2-evm" bitbake -k tisdk-adas-image WARNING: Duplicate inclusion for /home/user-ai/sdc/iAVM/ti-processor-sdk-linux-adas-j721s2-evm-10_01_00_04/yocto-build/sources/meta-arago/meta-arago-distro/conf/distro/include/branding-core.inc in /home/jet-ai/sdc/iAVM/ti-processor-sdk-linux-adas-j721s2-evm-10_01_00_04/yocto-build/sources/meta-arago/meta-arago-distro/conf/distro/arago.conf WARNING: Duplicate inclusion for /home/user-ai/sdc/iAVM/ti-processor-sdk-linux-adas-j721s2-evm-10_01_00_04/yocto-build/sources/meta-arago/meta-arago-distro/conf/distro/include/branding-core.inc in /home/jet-ai/sdc/iAVM/ti-processor-sdk-linux-adas-j721s2-evm-10_01_00_04/yocto-build/sources/meta-arago/meta-arago-distro/conf/distro/arago.conf NOTE: Started PRServer with DBfile: /mnt/sdc/iAVM/ti-processor-sdk-linux-adas-j721s2-evm-10_01_00_04/yocto-build/build/cache/prserv.sqlite3, Address: 127.0.0.1:43269, PID: 2008227 Loading cache: 100% | | ETA: --:--:-- Loaded 0 entries from dependency cache. Parsing recipes: 100% |#############################################################################| Time: 0:00:57 Parsing of 7036 .bb files complete (0 cached, 7036 parsed). 11095 targets, 1643 skipped, 0 masked, 0 errors. ERROR: Nothing PROVIDES 'tisdk-adas-image'. Close matches: tisdk-base-image tisdk-default-image tisdk-edgeai-image NOTE: Resolving any missing task queue dependencies NOTE: Resolving any missing task queue dependencies NOTE: Resolving any missing task queue dependencies NOTE: Resolving any missing task queue dependencies Build Configuration (mc:default): BB_VERSION = "2.8.0" BUILD_SYS = "x86_64-linux" NATIVELSBSTRING = "ubuntu-22.04" TARGET_SYS = "aarch64-oe-linux" MACHINE = "j721s2-evm" DISTRO = "arago" DISTRO_VERSION = "2023.10" TUNE_FEATURES = "aarch64" TARGET_FPU = "" meta-arago-distro meta-arago-extras meta-arago-demos meta-arago-test = "HEAD:b6349e47760397add572cc27468e0f30b40474c1" meta-qt5 = "scarthgap:554fc20c326a9b205169331644f0cb471619e63c" meta-virtualization = "HEAD:450941a1b6df96285691e8c23d4f332d3c88a994" meta-networking meta-python meta-oe meta-gnome meta-filesystems meta-multimedia = "HEAD:b8d1a14f7f3b76457c36752202ea7ae5881b6654" meta-ti-extras meta-ti-bsp = "HEAD:f06324bc1649e4f437686560cbd66f973ba920f5" meta-arm meta-arm-toolchain = "HEAD:7088279c0ab00c7dabefdd4544951b4746b48476" meta-clang = "HEAD:9fbfa9db33131abdf3870a94f00199eb53e276e5" meta = "HEAD:92cb4641ff4ec8c1f681bca21cfeaf2ba6923ab7" meta-tisdk = "HEAD:fcd7661087b0dd5b5b57d30ba0d45f2698e962f8" meta-edgeai = "HEAD:41499d7bcc8d37862b93c0d56cf782f9182d0be1" Build Configuration: BB_VERSION = "2.8.0" BUILD_SYS = "x86_64-linux" NATIVELSBSTRING = "ubuntu-22.04" TARGET_SYS = "arm-oe-eabi" MACHINE = "j721s2-evm-k3r5" DISTRO = "arago" DISTRO_VERSION = "2023.10" TUNE_FEATURES = "arm armv7a vfp thumb callconvention-hard" TARGET_FPU = "hard" meta-arago-distro meta-arago-extras meta-arago-demos meta-arago-test = "HEAD:b6349e47760397add572cc27468e0f30b40474c1" meta-qt5 = "scarthgap:554fc20c326a9b205169331644f0cb471619e63c" meta-virtualization = "HEAD:450941a1b6df96285691e8c23d4f332d3c88a994" meta-networking meta-python meta-oe meta-gnome meta-filesystems meta-multimedia = "HEAD:b8d1a14f7f3b76457c36752202ea7ae5881b6654" meta-ti-extras meta-ti-bsp = "HEAD:f06324bc1649e4f437686560cbd66f973ba920f5" meta-arm meta-arm-toolchain = "HEAD:7088279c0ab00c7dabefdd4544951b4746b48476" meta-clang = "HEAD:9fbfa9db33131abdf3870a94f00199eb53e276e5" meta = "HEAD:92cb4641ff4ec8c1f681bca21cfeaf2ba6923ab7" meta-tisdk = "HEAD:fcd7661087b0dd5b5b57d30ba0d45f2698e962f8" meta-edgeai = "HEAD:41499d7bcc8d37862b93c0d56cf782f9182d0be1" NOTE: Writing buildhistory NOTE: Writing buildhistory took: 5 seconds NOTE: Writing buildhistory NOTE: Writing buildhistory took: 5 seconds Summary: There were 2 WARNING messages. Summary: There was 1 ERROR message, returning a non-zero exit code.
It seems the build target "tisdk-adas-image" is not found when running bitbake.
I would appreciate it if you could guide me through the process of building tisdk-adas-image-j721s2-evm.tar.xz for use with Vision Apps.
Regards,
Christopher