This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

J721S2XSOMXEVM: J721S2: TDA4VE-Q1: GESI: Getting started with enet_loopback example in PDK

Part Number: J721S2XSOMXEVM


Tool/software:

Hi,

I am trying to understand how the enet_loopback works, as per my understanding if I set testPhyLoopback to BTRUE, it should use PHY to do the loopback test and not MAC; but in my case, even if I set testPhyLoopback to BTRUE, the loopback test prints everything is fine and that the test runs successfully even when no cables are connected to any of the RJ45 ports on GESI or CPB.

I would like to know, if I miss something or if there is some issue with the default config.

Thanks in advance

Best,
Moses

  • Hi,

    I am trying to understand how the enet_loopback works, as per my understanding if I set testPhyLoopback to BTRUE, it should use PHY to do the loopback test and not MAC; but in my case, even if I set testPhyLoopback to BTRUE, the loopback test prints everything is fine and that the test runs successfully even when no cables are connected to any of the RJ45 ports on GESI or CPB.

    No need to connect the cable, the movent PHY is configured in loopback mode, you get Link Up.

    I would like to know, if I miss something or if there is some issue with the default config.

    No, it will work even if the RJ45 cable is not connected.

    Best Regards,
    Sudheer