Part Number: AM623
Tool/software:
Hello,
We have been working on getting an HS part to boot, but without much success. This forum post is exactly the issue we have been experiencing.
AM620-Q1: Issue with Loading tispl.bin on AM62x(HS-FS) Custom Board Using SDK 8.06
Running on custom hardware, GP part of same type has been tested on the exact same hardware and is programmed just fine through UART.
Loading tiboot3.bin_hs works fine, but then hangs on the loading tispl.bin_hs on the Arm trusted firmware binary. This is only an issue with the HS part, the GP part on the exact same hardware runs fine.
Binaries were loaded through minicom with xModem for tiboot3.bin_hs and yModem for tispl.bin_hs
Build scripts are taken from this website and images are signed with default keys provided by TI. software-dl.ti.com/.../UG-General-Info.html
Here are the bootlogs:
02000000011a0000616d3632780000000000000048534653010001000100010002a6000000000000d68ecb2c055dff11ade95bd927e837d2a53bc23b0a2800cebce4f106bcf309df2213912d77a157C U-Boot SPL 2021.01-00001-ga347ec164e-dirty (Jul 30 2025 - 15:12:57 -0600) SYSFW ABI: 3.1 (firmware rev 0x0008 '8.6.4--v08.06.04 (Chill Capybar') SPL initial stack usage: 13424 bytes Trying to boot from UART CCxyzModem - CRC mode, 7219(SOH)/0(STX)/0(CAN) packets, 7 retries Loaded 923672 bytes init_env from device 7 not supported! ## No elf image at address 0x89000000 Starting ATF on ARM64 core...
Thank you in advance,
Nikolay