This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Adding multiple serializers into DM8148 McASP0



Hi,

I am trying to add use multiple serializers (4 TX and 4 RX) in DM8148 McASP0. I am using the PSP release linux-2.6.37-psp04.01.00.05.patch1 that has code for 1 TX and 1 RX usage. This framework uses ASoC to playback and capture stream using McASP0.

I have gotten 1 TX and 1 RX working in my board using DM5148 McASP. But when I add 3 more channels, nothing is working. Following are the modifications I made to the default architecture.

1. In arch/arm/mach-omap2/devices.c I have defined that I am using McASP0 as given below.

static struct resource ti81xx_mcasp_resource[] = {
{
.name = "mcasp",
.start = TI81XX_ASP0_BASE,
.end = TI81XX_ASP0_BASE + (SZ_1K * 12) - 1,
.flags = IORESOURCE_MEM,
},
/* TX event */
{
.start = TI81XX_DMA_MCASP0_AXEVT,
.end = TI81XX_DMA_MCASP0_AXEVT,
.flags = IORESOURCE_DMA,
},
/* RX event */
{
.start = TI81XX_DMA_MCASP0_AREVT,
.end = TI81XX_DMA_MCASP0_AREVT,
.flags = IORESOURCE_DMA,
},
};
2. I have defined the serializers I will be using in arch/arm/mach-omap2/board-ti8148evm.c as given below.
static u8 ti8148_iis_serializer_direction_mcasp0[] = {
TX_MODE, TX_MODE, TX_MODE, TX_MODE,
RX_MODE, RX_MODE, RX_MODE, RX_MODE,
INACTIVE_MODE, INACTIVE_MODE, INACTIVE_MODE, INACTIVE_MODE,
INACTIVE_MODE, INACTIVE_MODE, INACTIVE_MODE, INACTIVE_MODE,
};
static struct snd_platform_data ti8148_evm_snd_data = {
.tx_dma_offset = 0x46000000,
.rx_dma_offset = 0x46000000,
.op_mode = DAVINCI_MCASP_IIS_MODE,
.num_serializer = ARRAY_SIZE(ti8148_iis_serializer_direction_mcasp0),
.tdm_slots = 1,
.serial_dir = ti8148_iis_serializer_direction_mcasp0,
.asp_chan_q = EVENTQ_2,
.version = MCASP_VERSION_2,
.txnumevt = 4,
.rxnumevt = 4,
};
3. I have mentioned that I will use 4 dai's in McASP0 in sound/soc/davinci/davinci-evm.c as given below.
static struct snd_soc_dai_link grg_dai[] = {
{
.name = "PCM3501E.0", /* Codec name */
.stream_name = "PCM3501EStream.0", /* Stream name */
.cpu_dai_name = "davinci-mcasp.0", /* McASP instance to be Used */
.codec_dai_name = "pcm3501e-hifi",
.codec_name = "pcm3501e-codec.0", /* for multi-codec */
.platform_name = "davinci-pcm-audio", /* for multi-platform */
.init = NULL, /* codec/machine specific init - e.g. add machine controls */
.ops = &grg_snd_soc_ops, /* machine stream operations */
},
{
.name = "PCM3501E.1", /* Codec name */
.stream_name = "PCM3501EStream.1", /* Stream name */
.cpu_dai_name = "davinci-mcasp.0", /* McASP instance to be Used */
.codec_dai_name = "pcm3501e-hifi",
.codec_name = "pcm3501e-codec.1", /* for multi-codec */
.platform_name = "davinci-pcm-audio", /* for multi-platform */
.init = NULL, /* codec/machine specific init - e.g. add machine controls */
.ops = &grg_snd_soc_ops, /* machine stream operations */
},
{
.name = "PCM3501E.2", /* Codec name */
.stream_name = "PCM3501EStream.2", /* Stream name */
.cpu_dai_name = "davinci-mcasp.0", /* McASP instance to be Used */
.codec_dai_name = "pcm3501e-hifi",
.codec_name = "pcm3501e-codec.2", /* for multi-codec */
.platform_name = "davinci-pcm-audio", /* for multi-platform */
.init = NULL, /* codec/machine specific init - e.g. add machine controls */
.ops = &grg_snd_soc_ops, /* machine stream operations */
},
        {
                .name           = "PCM3501E.3",             /* Codec name */
.stream_name = "PCM3501EStream.3", /* Stream name */
.cpu_dai_name = "davinci-mcasp.0", /* McASP instance to be Used */
.codec_dai_name = "pcm3501e-hifi",
.codec_name = "pcm3501e-codec.3", /* for multi-codec */
.platform_name = "davinci-pcm-audio", /* for multi-platform */
.init = NULL, /* codec/machine specific init - e.g. add machine controls */
.ops = &grg_snd_soc_ops, /* machine stream operations */
},
};
Note - The codec I am using is PCM3501e and in its driver I have defined 4 codec dais to correspond to this definition.
4. When the board boots up, I can see that 4 pcm nodes come up as given below.
controlC0  pcmC0D0p   pcmC0D1p   pcmC0D2p   pcmC0D3p
pcmC0D0c pcmC0D1c pcmC0D2c pcmC0D3c timer
5. Also enabling the debug messages I am seeing that each of the codec dai's are getting DMA allocated. See the dump at the end of the post.
6. When I try to playback a file using aplay, I see that no DMA IRQs are getting generated. The dump is given below.
Kindly tell me what I am missing.
===========================================================================================================
Register dump with first channel accessed.
aplay -D"hw:0,0" -r16000 -traw -fS16_LE -c1  sine.wav.raw
...
Reg Value (0x0) : 44307302
Reg Value (0x10) : 0
Reg Value (0x14) : b400000f
Reg Value (0x18) : 0
Reg Value (0x1c) : 7c000090
Reg Value (0x20) : 0
Reg Value (0x44) : 1f00
Reg Value (0x48) : 0
Reg Value (0x4c) : 0
Reg Value (0x50) : 0
Reg Value (0x60) : 1f00
Reg Value (0x64) : ffff
Reg Value (0x68) : 74
Reg Value (0x6c) : 2
Reg Value (0x70) : 18009f
Reg Value (0x74) : 8000
Reg Value (0x78) : 0
Reg Value (0x7c) : 0
Reg Value (0x80) : 104
Reg Value (0x84) : 0
Reg Value (0x88) : 0
Reg Value (0x8c) : 0
Reg Value (0xa0) : 1f00
Reg Value (0xa4) : ffff
Reg Value (0xa8) : 18074
Reg Value (0xac) : 82
Reg Value (0xb0) : bf
Reg Value (0xb4) : 0
Reg Value (0xb8) : 1
Reg Value (0xbc) : 0
Reg Value (0xc0) : 175
Reg Value (0xc4) : 0
Reg Value (0xc8) : 85000000
Reg Value (0xcc) : 0
Reg Value (0x100) : 0
Reg Value (0x104) : 0
Reg Value (0x108) : 0
Reg Value (0x10c) : 0
Reg Value (0x110) : 0
Reg Value (0x114) : 0
Reg Value (0x118) : 0
Reg Value (0x11c) : 0
Reg Value (0x120) : 0
Reg Value (0x124) : 0
Reg Value (0x128) : 0
Reg Value (0x12c) : 0
Reg Value (0x130) : 0
Reg Value (0x134) : 0
Reg Value (0x138) : 0
Reg Value (0x13c) : 0
Reg Value (0x140) : 0
Reg Value (0x144) : 0
Reg Value (0x148) : 0
Reg Value (0x14c) : 0
Reg Value (0x150) : 0
Reg Value (0x154) : 0
Reg Value (0x158) : 0
Reg Value (0x15c) : 0
Reg Value (0x180) : 11
Reg Value (0x184) : 11
Reg Value (0x188) : 11
Reg Value (0x190) : 2
Reg Value (0x194) : 2
Reg Value (0x200) : 0
Reg Value (0x204) : 0
Reg Value (0x208) : 0
Reg Value (0x20c) : 0
Reg Value (0x210) : 0
Reg Value (0x214) : 0
Reg Value (0x280) : 0
Reg Value (0x284) : 0
Reg Value (0x288) : 0
Reg Value (0x28c) : 0
Reg Value (0x290) : 0
Reg Value (0x294) : 0
Reg Value (0x1000) : 11004
Reg Value (0x1004) : 0
Reg Value (0x1008) : 1004
Reg Value (0x100c) : 0
===========================================================================
debug prints when the playback is happening

Enter McASP : davinci_mcasp_startup +953
EDMA: EER0 00000000
asoc: pcm3501e-hifi <-> davinci-mcasp.0 info:
asoc: rate mask 0x8
asoc: min ch 1 max ch 2
asoc: min rate 16000 max rate 16000
Enter McASP : davinci_mcasp_set_dai_fmt +518
Exit : grg_snd_soc_hw_params +65
Enter: sound/soc/codecs/pcm3501e.c +38
Enter McASP : davinci_mcasp_hw_params +865
Enter McASP : davinci_hw_common_param +705
Enter McASP : davinci_hw_param +766
Enter McASP : davinci_config_channel_size +621
davinci_pcm: audio_set_dma_params_play channel = 191 dma_ptr = 872a0000 period_size=fa0
davinci_pcm: audio_set_dma_params_play channel = 191 dma_ptr = 872a0fa0 period_size=fa0
EDMA: ER0 00000000
EDMA: EER0 00000100
pcm3501e-codec pcm3501e-codec.0: Setting standby bias
pcm3501e-codec pcm3501e-codec.0: Setting bias prepare
pcm3501e-codec pcm3501e-codec.0: Setting full bias
Enter McASP : davinci_mcasp_trigger +915
Enter McASP : davinci_mcasp_start +463
Enter McASP : mcasp_start_tx +416
ALSA sound/core/pcm_lib.c:1765: playback write error (DMA or IRQ trouble?)
ALSA sound/core/pcm_lib.c:1765: playback write error (DMA or IRQ trouble?)
Enter McASP : davinci_mcasp_trigger +915
Enter McASP : davinci_mcasp_stop +498
Enter McASP : mcasp_stop_tx +489
EDMA: EER0 00000000
pop wq checking: PCM3501E Playback status: inactive waiting: yes
pcm3501e-codec pcm3501e-codec.0: Setting bias prepare
pcm3501e-codec pcm3501e-codec.0: Setting standby bias
  • Hi,

    As mentioned in the other thread, currently multiple-serializers are not supported. Here's some pointers to get started...

    You'll need to make changes to the McASP/PCM driver to make use of multiple serializers. Changes need to be for the EDMA setup portion so that it transfer length is for multiple serializers. You'll also need to ensure that the McASP hw config is for the required serializers. The TRM has a step by step description of what needs to be done for the McASP. You can use that as starting point.

    Regards,

    Vaibhav

  • HI Vaibhav

    whether  the function of multiple-serializers are supported on DM81xx platform or not ? 

    could you give a patch if  it have been supported.