when running kernel,the board will stop ,How to make the kernel normal start?
Serial print information is as follows:
reading uImage
2362144 bytes read
## Booting kernel from Legacy Image at 81000000 ...
Image Name: Arago/2.6.37-psp04.00.00.10/dm81
Image Type: ARM Linux Kernel Image (uncompressed)
Data Size: 2362080 Bytes = 2.3 MiB
Load Address: 80008000
Entry Point: 80008000
Verifying Checksum ... OK
Loading Kernel Image ... OK
OK
Starting kernel ...