Other Parts Discussed in Thread: TDA4VM
Tool/software:
Dear TI
After patched the
[FAQ] TDA4VM: How to enable MCU R5F cores running in split mode in SPL boot flow.
u-boot_patches_to_enable_MCU_R5F_SplitMode.zip
Linux_patches_to_enable_MCU_R5F_SplitMode.zip
u-boot load /lib/firmware/j721s2-mcu-r5f0_1-fw fail
It cause by the size of vx_app_rtos_linux_mcu1_1.out is 0 , right ?
Is there any suggestion for this, thanks
a) u-boot command
=> load mmc 0:5 0x82000000 /lib/firmware/j721s2-mcu-r5f0_1-fw
Failed to load '/lib/firmware/j721s2-mcu-r5f0_1-fw'
=> load mmc 0:5 0x82000000 /lib/firmware/j721s2-main-r5f0_1-fw
335028 bytes read in 120 ms (2.7 MiB/s)
b)root@j721s2-evm:/lib/firmware# ls -la
lrwxrwxrwx 1 root root 62 Mar 9 2018 j721s2-mcu-r5f0_1-fw -> /usr/lib/firmware/vision_apps_evm/vx_app_rtos_linux_mcu1_1.out
lrwxrwxrwx 1 root root 79 Mar 9 2018 j721s2-mcu-r5f0_1-fw-sec -> /usr/lib/firmware/ti-ipc/j721s2/ipc_echo_test_mcu1_1_release_strip.xer5f.signed
lrwxrwxrwx 1 root root 62 Mar 9 2018 j721s2-main-r5f0_1-fw -> /usr/lib/firmware/vision_apps_evm/vx_app_rtos_linux_mcu2_1.out
lrwxrwxrwx 1 root root 69 Mar 9 2018 j721s2-main-r5f0_1-fw-sec -> /usr/lib/firmware/vision_apps_evm/vx_app_rtos_linux_mcu2_1.out.signed
c)
root@j721s2-evm:~# ls -la /usr/lib/firmware/vision_apps_evm/vx_app_rtos_linux_mcu1_1.out
-rw-r--r-- 1 root root 0 Mar 9 2018 /usr/lib/firmware/vision_apps_evm/vx_app_rtos_linux_mcu1_1.out
root@j721s2-evm:~#
root@j721s2-evm:~# ls -la /usr/lib/firmware/vision_apps_evm/vx_app_rtos_linux_mcu2_0.out
-rw-r--r-- 1 root root 1203596 Mar 9 2018 /usr/lib/firmware/vision_apps_evm/vx_app_rtos_linux_mcu2_0.out
root@j721s2-evm:~#
d) uart log
Best Regards
Jiahao