Other Parts Discussed in Thread: TPS40400, AM3894
Hello, I did 5 model board with the DM8168,The 1V_AVS power using TPS40400 chip, output 0.99V.Currently both the power supply board or the power requirements of the order are in line DM8168, but when power up the board, my SD card on the board sometimes start, sometimes it will not start, USART port does not print any information, and when it is seted to NandFlash start up first, is the samesituation! I have the power to fly to the EVM board of Ti, EVM board each time you open all the normal, very stable! Power problems should be excluded. I Would like to ask, if there are any factors affecting the chip enable those which that i need to pay attention? Which aspects of this large number? Thanks