Tool/software:
Hello,
as below show, from D-note, should add a 22R at the output of MCASP1_ACLKX near to the SOC, but i do not find the resistor in the schematic of "PROC164E1-1_SCH_With_Design-Updates..Notes_V1.0", how to understand this?
thanks!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Hello,
as below show, from D-note, should add a 22R at the output of MCASP1_ACLKX near to the SOC, but i do not find the resistor in the schematic of "PROC164E1-1_SCH_With_Design-Updates..Notes_V1.0", how to understand this?
thanks!
Hello Liujian,
The D-Note is not pointing to an existing resistor but rather recommends reserving a 0Ω resistor at the output of MCASP1_ACLKX near to the SOC and if you face EMI testing issues to swap the 0Ω with a 22Ω resistor.
The resistor is mainly for smoothing the edge off the rising edge if it fails EMI testing.
Let me know if this helps!
Regards,
Karam