This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

uart

hai i am using usbstk5535 ezdsp and when i run the the uart example no data is transfered through the hyper terminal .no data exchange is happening the sw3 is also enable for uart via j2   what configuration i want to do or i want to check the EBSR value for the uart port .if so help me on this module

 

 

with regards

seeni

 

  • Hi,

    I confirmed that csl_uart_dma_example works. EBSR value is 0x5000. SW3 pin 2 should be ON position (allows virtual comm port enable).

    Also you make sure your hyperterminal setting matches uart_example settings.

    Regards,

    Hyun