Tool/software:
Im using in my product the TMS320DM8148CCYE2. Is it possible to use the TMS320DM8148SCYE2 instead.
What are the differences? Are the two chips pin compatible?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Im using in my product the TMS320DM8148CCYE2. Is it possible to use the TMS320DM8148SCYE2 instead.
What are the differences? Are the two chips pin compatible?
Hi,
These are two variants of Davinci processor.
You can find these details in the datasheet of the DaVinci processor. Please refer to it from the following link.

Regards,
Betsy Varughese
Hi,
Hi, I have checked the datasheet before posting the question, which states the "S" version is "Video Security". No other information is available in the DS.
Yes, exactly. both are same silicon revision.
"S" includes video security features.
The question is can I use the TMS320DM8148SCYE2 instead of TMS320DM8148CCYE2.
I’ll need to confirm this internally and will get back to you as soon as possible.
Regards,
Betsy Varughese
Hi,
Thanks for the patience. Will update you shortly.
Regards,
Betsy Varughese
Hi Yigal,
The TMS320DM8148SCYE2 part should be identical to the TMS320DM8148CCYE2.
TI recommends you buy/build a handful of systems (say ~5) as a sanity check before moving forward with building in higher quantities.
Regards,
Kyle