Part Number: PROCESSOR-SDK-AM62X
Tool/software:
Hi All,
I use the same kernel and device tree, on SD card boot, the CAN driver is able to load normally, but when booted via Emmc, the driver fails to load, even after boot using insmod manually loading the driver shows that the load is successful but the ifconfig command cannot see the CAN device.
Attached are logs from the SD card and Emmc boot_from_SDcard.log5315.boot_from_emmc.log