Part Number: AM62P-Q1
Other Parts Discussed in Thread: AM62P5
Tool/software:
SoC: AM62P5
SDK: Linux 10.0
Boot mode: SPL from eMMC
Reference URL: https://dev.ti.com/tirex/explore/node?node=A__AXEeWNLEW2jak3KzsCN3BA__AM62P-ACADEMY__fp5YxRM__LATEST
Dear Technical Supporter,
While we are able to successfully boot the SPL from the SD card, switching to booting it from eMMC has failed. We have done:
1. Changed to root=/dev/mmcblk0p2, in the k3-am62p5-sk.dts
2. Changed to mmcdev=0 and bootpart=0:2 in the am62px.env
3. Configured boot switches to eMMC mode
4. Copied boot binaries to mmcblk0boot0; copied rootfs to mmcblk0p1.
After reboot, system log shows
U-Boot SPL 2024.04 (Aug 04 2025 - 16:00:23 +0800) SYSFW ABI: 4.0 (firmware rev 0x000a '10.1.8--v10.01.08 (Fiery Fox)') SPL initial stack usage: 17056 bytes Trying to boot from MMC1 Authentication passed Authentication passed Authentication passed Authentication passed Authentication passed Starting ATF on ARM64 core... NOTICE: BL31: v2.11.0(release):v2.11.0-906-g58b25570c9-dirty NOTICE: BL31: Built : 04:20:32, Nov 1 2024 U-Boot SPL 2024.04 (Aug 04 2025 - 16:01:31 +0800) SYSFW ABI: 4.0 (firmware rev 0x000a '10.1.8--v10.01.08 (Fiery Fox)') SPL initial stack usage: 1776 bytes MMC: no card present ** Bad device specification mmc 1 ** Couldn't find partition mmc 1:1 Error: could not access storage. Trying to boot from MMC1 Authentication passed Authentication passed U-Boot 2024.04 (Aug 04 2025 - 16:01:31 +0800) SoC: AM62PX SR1.0 HS-FS Model: Texas Instruments AM62P5 SK DRAM: 1 GiB Core: 65 devices, 27 uclasses, devicetree: separate MMC: mmc@fa10000: 0, mmc@fa00000: 1 Loading Environment from nowhere... OK In: serial Out: serial Err: serial Net: am65_cpsw_nuss_port ethernet@8000000port@1: Invalid PHY mode, port 1 am65_cpsw_nuss_port ethernet@8000000port@2: Invalid PHY mode, port 2 No ethernet found. Hit any key to stop autoboot: 0 switch to partitions #0, OK mmc0(part 0) is current device SD/MMC found on device 0 Can't set block device ** Invalid partition 2 ** ** Invalid partition 2 ** Couldn't find partition mmc 0:2 Can't set block device ** Invalid partition 2 ** Couldn't find partition mmc 0:2 Can't set block device libfdt fdt_check_header(): FDT_ERR_BADMAGIC No FDT memory address configured. Please configure the FDT address via "fdt addr <address>" command. Aborting! Bad Linux ARM64 Image magic! Scanning for bootflows in all bootdevs Seq Method State Uclass Part Name Filename --- ----------- ------ -------- ---- ------------------------ ---------------- Scanning global bootmeth 'efi_mgr': MMC: no card present No EFI system partition No EFI system partition Failed to persist EFI variables No EFI system partition Failed to persist EFI variables No EFI system partition Failed to persist EFI variables am65_cpsw_nuss_port ethernet@8000000ethernet@800000: Invalid PHY mode, port 1 am65_cpsw_nuss_port ethernet@8000000ethernet@800000: Invalid PHY mode, port 1 0 efi_mgr ready (none) 0 <NULL> ** Booting bootflow '<NULL>' with efi_mgr Loading Boot0000 'mmc 0' failed EFI boot manager: Cannot load any image Boot failed (err=-14) Scanning bootdev 'mmc@fa10000.bootdev': Scanning bootdev 'mmc@fa00000.bootdev': MMC: no card present MMC: no card present MMC: no card present MMC: no card present No more bootdevs --- ----------- ------ -------- ---- ------------------------ ---------------- (1 bootflow, 1 valid) =>
The following settings were obtained from printenv:
addr_fit=0x90000000
arch=arm
args_all=setenv optargs ${optargs} earlycon=ns16550a,mmio32,0x02800000 ${mtdparts}
args_mmc=run finduuid;setenv bootargs console=${console} ${optargs} root=PARTUUID=${uuid} rw rootfstype=${mmcrootfstype}
baudrate=115200
board=am62px
board_name=am62px
boot=mmc
boot_fdt=try
boot_fit=0
boot_rprocs=if test ${dorprocboot} -eq 1 && test ${boot} = mmc; then rproc init; run boot_rprocs_mmc; fi;
boot_rprocs_mmc=env set rproc_id; env set rproc_fw; env set secure_suffix; if test ${secure_rprocs} -eq 1; then env set secure_suffix -sec; fi; for i in ${rproc_fw_binaries} ; do if test -z "${rproc_id}" ; then env set rproc_id $i; else env set rproc_fw $i${secure_suffix}; run rproc_load_and_boot_one; env set rproc_id; env set rproc_fw; fi; done
boot_targets=mmc0 mmc1
bootcmd=run envboot; run bootcmd_ti_mmc; bootflow scan -lb
bootcmd_ti_mmc=run init_${boot}; run update_do_main_cpsw0_qsgmii_phyinit; if test ${do_main_cpsw0_qsgmii_phyinit} -eq 1; then run main_cpsw0_qsgmii_phyinit; fi; run boot_rprocs; if test ${boot_fit} -eq 1; then run get_fit_${boot}; run get_fit_overlaystring; run run_fit; else; run get_kern_${boot}; run get_fdt_${boot}; run get_overlay_${boot}; run run_kern; fi;
bootdelay=2
bootdir=/boot
bootenvfile=uEnv.txt
bootm_size=0x10000000
bootpart=0:2
bootscript=echo Running bootscript from mmc${mmcdev} ...; source ${loadaddr}
console=ttyS2,115200n8
cpu=armv8
dfu_alt_info_emmc=rawemmc raw 0 0x800000 mmcpart 1; rootfs part 0 1; tiboot3.bin.raw raw 0x0 0x400 mmcpart 1; tispl.bin.raw raw 0x400 0x1000 mmcpart 1; u-boot.img.raw raw 0x1400 0x2000 mmcpart 1; u-env.raw raw 0x3400 0x100 mmcpart 1; sysfw.itb.raw raw 0x3600 0x800 mmcpart 1
dfu_alt_info_mmc=boot part 1 1; rootfs part 1 2; tiboot3.bin fat 1 1; tispl.bin fat 1 1; u-boot.img fat 1 1; uEnv.txt fat 1 1; sysfw.itb fat 1 1
dfu_alt_info_nand=NAND.tiboot3 part 0 1; NAND.tispl part 0 2; NAND.tiboot3.backup part 0 3; NAND.u-boot part 0 4; NAND.u-boot-env part 0 5; NAND.u-boot-env.backup part 0 6; NAND.file-system part 0 7
dfu_alt_info_ospi=tiboot3.bin raw 0x0 0x080000; tispl.bin raw 0x080000 0x200000; u-boot.img raw 0x280000 0x400000; u-boot-env raw 0x680000 0x020000; sysfw.itb raw 0x6c0000 0x100000; rootfs raw 0x800000 0x3800000
dfu_alt_info_ospi_nand=ospi_nand.tiboot3 part 1; ospi_nand.tispl part 2; ospi_nand.u-boot part 3; ospi_nand.env part 4; ospi_nand.env.backup part 5; ospi_nand.rootfs part 6; ospi_nand.phypattern part 7
dfu_alt_info_ram=tispl.bin ram 0x80080000 0x200000; u-boot.img ram 0x81000000 0x400000
dorprocboot=0
dtboaddr=0x89000000
envboot=if mmc dev ${mmcdev}; then if mmc rescan; then echo SD/MMC found on device ${mmcdev}; if test -n "${loadbootscript}" && run loadbootscript; then run bootscript; else if run loadbootenv; then echo Loaded env from ${bootenvfile}; run importbootenv; fi; if test -n $uenvcmd; then echo Running uenvcmd ...; run uenvcmd; fi; fi; fi; fi;
fdt_addr_r=0x88000000
fdtaddr=0x88000000
fdtcontroladdr=bde98660
fdtfile=ti/k3-am62p5-sk.dtb
fdtoverlay_addr_r=0x89500000
findfdt=echo WARN: fdtfile already set. Stop using findfdt in script
finduuid=part uuid ${boot} ${bootpart} uuid
get_fdt_mmc=load mmc ${bootpart} ${fdtaddr} ${bootdir}/dtb/${fdtfile}
get_fit_config=setexpr name_fit_config gsub / _ conf-${fdtfile}
get_fit_mmc=load mmc ${bootpart} ${addr_fit} ${bootdir}/${name_fit}
get_fit_overlaystring=for overlay in $name_overlays; do; setexpr name_fit_overlay gsub / _ conf-${overlay}; setenv overlaystring ${overlaystring}'#'${name_fit_overlay}; done;
get_kern_mmc=load mmc ${bootpart} ${loadaddr} ${bootdir}/${name_kern}
get_overlay_mmc=fdt address ${fdtaddr}; fdt resize 0x100000; for overlay in $name_overlays; do; load mmc ${bootpart} ${dtboaddr} ${bootdir}/dtb/${overlay} && fdt apply ${dtboaddr}; done;
importbootenv=echo Importing environment from mmc${mmcdev} ...; env import -t ${loadaddr} ${filesize}
init_mmc=run args_all args_mmc
kernel_addr_r=0x82000000
loadaddr=0x82000000
loadbootenv=fatload mmc ${mmcdev} ${loadaddr} ${bootenvfile}
loadfdt=load ${devtype} ${bootpart} ${fdtaddr} ${bootdir}/dtb/${fdtfile}
loadimage=load ${devtype} ${bootpart} ${loadaddr} ${bootdir}/${bootfile}
mmcboot=if mmc dev ${mmcdev}; then devnum=${mmcdev}; devtype=mmc; if mmc rescan; then echo SD/MMC found on device ${mmcdev}; if run loadimage; then run args_mmc; if test ${boot_fit} -eq 1; then run run_fit; else run mmcloados; fi; fi; fi; fi;
mmcdev=0
mmcloados=if test ${boot_fdt} = yes || test ${boot_fdt} = try; then if run get_fdt_mmc; then bootz ${loadaddr} - ${fdtaddr}; else if test ${boot_fdt} = try; then bootz; else echo WARN: Cannot load the DT; fi; fi; else bootz; fi;
mmcrootfstype=ext4 rootwait
name_fit=fitImage
name_kern=Image
partitions=name=rootfs,start=0,size=-,uuid=${uuid_gpt_rootfs}
pxefile_addr_r=0x80100000
ramdisk_addr_r=0x88080000
rd_spec=-
rdaddr=0x88080000
rproc_fw_binaries= 0 /lib/firmware/am62p-mcu-r5f0_0-fw
rproc_load_and_boot_one=if load mmc ${bootpart} $loadaddr ${rproc_fw}; then if rproc load ${rproc_id} ${loadaddr} ${filesize}; then rproc start ${rproc_id}; fi; fi
run_fit=run get_fit_config; bootm ${addr_fit}#${name_fit_config}${overlaystring}
run_kern=booti ${loadaddr} ${rd_spec} ${fdtaddr}
scriptaddr=0x80000000
secure_rprocs=0
soc=k3
splashfile=ti_logo_414x97_32bpp.bmp.gz
splashimage=0x80200000
splashpos=m,m
splashsource=mmc
update_do_main_cpsw0_qsgmii_phyinit=setenv do_main_cpsw0_qsgmii_phyinit 0;
update_to_fit=setenv loadaddr ${addr_fit}; setenv bootfile ${name_fit}
vendor=ti
Environment size: 5481/126972 bytes
Question:
Is it possible that we overlooked some areas that require modification?
Thank you very much.
Wilson