Part Number: PROCESSOR-SDK-AM62X
Tool/software:
Hi,
we are using the AM62x in an automation product with Linux in switch mode (via devlink dev param..). With the tc tool its possible to set a rate-limit for boradcast traffic and/or muliticast traffic.
From our observation the cpsw hw does a pretty simple (strict) rate-limiting. Is it possible to allow for some kind of burst behavior? The typical topology is a line and with the strict rate-limiting regime it can be very disruptive, especially during the start-up phase. (Automation protocols sometimes do strange things..)
For example when set to 1000pps the cpsw-hw will only allow for one broadcast packet every 1ms.
Thanks,
Jan