This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM8168 nand flash write error, where can i download the flash-writer source files?



Hi, buddys

I have designed a evaluation board with dm8168. Now it can be correctly connect to the emulator, and also can be initialized with defalut gel files which

in the EZSDK(ezsdk_dm816x-evm_5_03_01_15_setuplinux). Next i try to write a pre-build uboot file into the nand flash, the are something wrong with the

wirte operation but it work fine of earasing the nand flash.

There dosn't contains any c file or some other source files. In the host-tools, only 3 pre-build file: nand-flash-writer.out; norflash-writer.out; spi-flash-writer.out.

So i can not modify it.......

see the logs as fallowns:

----------------------
NAND FLASH DETAILS
----------------------
Device ID : 0xf1
Manufacture ID : 0xad
Page Size : 2048 Bytes
Spare Size : 256 Bytes
Pages_Per_Block : 64
Number_of_Blocks : 1024
Device_width : 1 Byte
DeviceSize : 128 MB


Performing Global Nand Erase
... done

NAND flashing successful!
================================================================
----------------------
NAND FLASH DETAILS
----------------------
Device ID : 0xf1
Manufacture ID : 0xad
Page Size : 2048 Bytes
Spare Size : 256 Bytes
Pages_Per_Block : 64
Number_of_Blocks : 1024
Device_width : 1 Byte
DeviceSize : 128 MB

Setting the ECC scheme
Set the BCH 8 bit ECC scheme .... done
Preparing to Flash image ....
Opening image ... done.
Erasing Required Blocks [start = 0, count = 2]...Done
Flashing image ...
Number of blocks needed for header and data: 0x2
Attempting to start write in block number 0x0.
Writing image data to Block 0 Page0x0
Verify failed. Attempting to clear page
Attempting to start write in block number 0x1.
Writing image data to Block 1 Page0x0
Verify failed. Attempting to clear page
Attempting to start write in block number 0x2.
Writing image data to Block 2 Page0x0
Verify failed. Attempting to clear page
Attempting to start write in block number 0x3.
Writing image data to Block 3 Page0x0
Verify failed. Attempting to clear page
Attempting to start write in block number 0x4.