Tool/software:
Hello
During development I often got errors from SYSFW that I was not able to interpret. That is the reason why I want to be able to use the debug trace feature. I tried enabling it with this patch
diff --git a/board/ti/am64x/board-cfg.yaml b/board/ti/am64x/board-cfg.yaml index 8981b75caa27..ca1aa22d8965 100644 --- a/board/ti/am64x/board-cfg.yaml +++ b/board/ti/am64x/board-cfg.yaml @@ -27,10 +27,10 @@ board-cfg: subhdr: magic: 0xA5C3 size: 5 - msmc_cache_size: 0x0 + msmc_cache_size: 0x1C debug_cfg: subhdr: magic: 0x020C size: 8 - trace_dst_enables: 0x00 - trace_src_enables: 0x00 + trace_dst_enables: 0x0D + trace_src_enables: 0x3F
I made sure the corresponding UART is enabled and should work however there is nothing coming on the UART. I tried the FAQ tutorial for SBL with MCU+SDK there it works.
What am I missing here?
Best Regards,
Philippe